<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Requirements for minimal installation under Linux in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Requirements-for-minimal-installation-under-Linux/m-p/880945#M3603</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was able to successfully install the Debian package under Linux and run UsbdmScript / UsdbmFlashProgramer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I want to install it on a system without a window server / GUI. Is this possible? What are the minimal requirements?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have installed Eclipse and Eclipse-CDT, libwxgtk3.0-0 and libxerces-c3.1 so far. UsbdmScript is installed, but the error "Illegal Instruction" occurs when executing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a log file where I can see where the error came from?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;During the installation of the Debian package an error message appears:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Installing net.sourceforge.usbdm.cdt.feature.feature.group 5.0.0.201609031021.&lt;BR /&gt;Installation failed.&lt;BR /&gt;Cannot complete the install because some dependencies are not satisfiable&lt;BR /&gt;&amp;nbsp;net.sourceforge.usbdm.usbdm.cdt.feature.feature.group.group [5.0.0.201609031021] cannot be installed in this environment because its filter is not applicable.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Feb 2019 11:13:09 GMT</pubDate>
    <dc:creator>s_hensel</dc:creator>
    <dc:date>2019-02-21T11:13:09Z</dc:date>
    <item>
      <title>Requirements for minimal installation under Linux</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Requirements-for-minimal-installation-under-Linux/m-p/880945#M3603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was able to successfully install the Debian package under Linux and run UsbdmScript / UsdbmFlashProgramer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I want to install it on a system without a window server / GUI. Is this possible? What are the minimal requirements?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have installed Eclipse and Eclipse-CDT, libwxgtk3.0-0 and libxerces-c3.1 so far. UsbdmScript is installed, but the error "Illegal Instruction" occurs when executing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a log file where I can see where the error came from?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;During the installation of the Debian package an error message appears:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Installing net.sourceforge.usbdm.cdt.feature.feature.group 5.0.0.201609031021.&lt;BR /&gt;Installation failed.&lt;BR /&gt;Cannot complete the install because some dependencies are not satisfiable&lt;BR /&gt;&amp;nbsp;net.sourceforge.usbdm.usbdm.cdt.feature.feature.group.group [5.0.0.201609031021] cannot be installed in this environment because its filter is not applicable.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Feb 2019 11:13:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Requirements-for-minimal-installation-under-Linux/m-p/880945#M3603</guid>
      <dc:creator>s_hensel</dc:creator>
      <dc:date>2019-02-21T11:13:09Z</dc:date>
    </item>
    <item>
      <title>Re: Requirements for minimal installation under Linux</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Requirements-for-minimal-installation-under-Linux/m-p/880946#M3604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is the solution: I tried to use&amp;nbsp;UsbdmScript with the latest Release of Raspbian Stretch. With the older Release (&lt;A href="http://downloads.raspberrypi.org/raspbian/images/raspbian-2017-07-05/"&gt;raspbian-2017-07-05&lt;/A&gt;), UsbdmScript is now working without problems. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Feb 2019 15:31:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Requirements-for-minimal-installation-under-Linux/m-p/880946#M3604</guid>
      <dc:creator>s_hensel</dc:creator>
      <dc:date>2019-02-25T15:31:34Z</dc:date>
    </item>
  </channel>
</rss>