<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDML中的主题 UsbdmFlashProgrammer command line</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/UsbdmFlashProgrammer-command-line/m-p/790858#M3586</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with UsbdmFlashProgrammer command line.&lt;/P&gt;&lt;P&gt;I use a HCS08 MC9S08PA32 Cpu and want to program it with the UsbdmFlashProgrammer tool.&lt;/P&gt;&lt;P&gt;If the cpu was not programmed before (clean and fresh one) the UsbdmFlashProgrammer commandline failed with BDM_RC_SYNC_TIMEOUT.&lt;/P&gt;&lt;P&gt;If I use the windows version then a messagebox comes out with ' Cycle power'. If I do this (power off the device and power on again) then the programming works.&lt;/P&gt;&lt;P&gt;Also after this point the UsbdmFlashProgrammer commandline works as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can I do that UsbdmFlashProgrammer commandline works also with fresh and clean cpu's ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Werner&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 07 Jul 2018 09:05:35 GMT</pubDate>
    <dc:creator>wernerdungs</dc:creator>
    <dc:date>2018-07-07T09:05:35Z</dc:date>
    <item>
      <title>UsbdmFlashProgrammer command line</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/UsbdmFlashProgrammer-command-line/m-p/790858#M3586</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with UsbdmFlashProgrammer command line.&lt;/P&gt;&lt;P&gt;I use a HCS08 MC9S08PA32 Cpu and want to program it with the UsbdmFlashProgrammer tool.&lt;/P&gt;&lt;P&gt;If the cpu was not programmed before (clean and fresh one) the UsbdmFlashProgrammer commandline failed with BDM_RC_SYNC_TIMEOUT.&lt;/P&gt;&lt;P&gt;If I use the windows version then a messagebox comes out with ' Cycle power'. If I do this (power off the device and power on again) then the programming works.&lt;/P&gt;&lt;P&gt;Also after this point the UsbdmFlashProgrammer commandline works as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can I do that UsbdmFlashProgrammer commandline works also with fresh and clean cpu's ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Werner&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Jul 2018 09:05:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/UsbdmFlashProgrammer-command-line/m-p/790858#M3586</guid>
      <dc:creator>wernerdungs</dc:creator>
      <dc:date>2018-07-07T09:05:35Z</dc:date>
    </item>
  </channel>
</rss>