<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USBDM driver in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675289#M3530</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo&lt;/P&gt;&lt;P&gt;Not sure of the make - it just says "freescale USBDM" on the case, but it does use a JS16 chip.&lt;/P&gt;&lt;P&gt;The good news is that it is now working. I tried loading the driver using the "Update Driver" from the the device driver window and selected the driver myself rather than the automatic option.&lt;/P&gt;&lt;P&gt;The bad news is that CodeWarrior will not select it as debug hardware. In Debug Settings I select the Connection Type &amp;nbsp;"USBDM HCS Interface" and Preferred BDM as "USBDM-JS16-SWD_SER-0001" I get the message : -&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;Error launching DEO_01_Issue_6_FLASH_PnE U-Multilink&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;There was an error parsing the memory configuration file&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 02 Jul 2017 07:56:05 GMT</pubDate>
    <dc:creator>juliancox</dc:creator>
    <dc:date>2017-07-02T07:56:05Z</dc:date>
    <item>
      <title>USBDM driver</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675286#M3527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have CodeWarrior 10.7, USBDM_4_12_1_180_win and USBDM_Drivers_1_3_0_Win_x64 all on Windows 7 64-bit. With the USBDM connecter the device manager showed "Interface 0 - USBDM' and "USBDM CDC Interface" - both under " Other Devices" and both showed "No Driver Installed". After removing, installing, repairing, reinstalling the driver&amp;nbsp;many times a device eventually appeared under "Debug devices" and&amp;nbsp;it&amp;nbsp;had a driver. I was then able to program my S08SH4 - once. After that - back to square one. Eventually I re-established the device driver and tried to do a firmware upgrade. This worked until I was instructed to "unplug the device, wait a few moments and re-connect the BDM". I then got the message that part 2 of the process had failed. Since then I am unable to load the device driver - so no USBDM.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Jun 2017 15:04:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675286#M3527</guid>
      <dc:creator>juliancox</dc:creator>
      <dc:date>2017-06-27T15:04:16Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM driver</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675287#M3528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Cox,&lt;/P&gt;&lt;P&gt;I just moved your question from &lt;SPAN class=""&gt;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-objectid="2028" data-objecttype="14" href="https://community.nxp.com/community/codewarrior/cw-mcu"&gt;CodeWarrior for MCU space &lt;/A&gt;to &lt;A _jive_internal="true" class="" data-content-finding="Community" data-objectid="2024" data-objecttype="14" href="https://community.nxp.com/community/bdm"&gt;OSBDM and TBDML space&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Thus our USBDM expert would be able to see it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Jennie Zhang.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jun 2017 02:52:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675287#M3528</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2017-06-28T02:52:13Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM driver</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675288#M3529</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Julian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you provide the following information so that I can suggest some things to try:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;What BDM do you actually have?&amp;nbsp; There are a range of USBDM interfaces available and it is unclear which one you are using.&amp;nbsp; In&amp;nbsp; particular, what is the chip the BDM is based on and what interfaces does it support?&amp;nbsp; What did the software identify the BDM as?&amp;nbsp; Post a picture if you are unsure.&lt;/LI&gt;&lt;LI&gt;If it has JS16 chip does the BDM have a boot link? If so it should be possible to load the firmware from scratch if you can identify which hardware it is.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jun 2017 07:46:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675288#M3529</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2017-06-28T07:46:36Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM driver</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675289#M3530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo&lt;/P&gt;&lt;P&gt;Not sure of the make - it just says "freescale USBDM" on the case, but it does use a JS16 chip.&lt;/P&gt;&lt;P&gt;The good news is that it is now working. I tried loading the driver using the "Update Driver" from the the device driver window and selected the driver myself rather than the automatic option.&lt;/P&gt;&lt;P&gt;The bad news is that CodeWarrior will not select it as debug hardware. In Debug Settings I select the Connection Type &amp;nbsp;"USBDM HCS Interface" and Preferred BDM as "USBDM-JS16-SWD_SER-0001" I get the message : -&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;Error launching DEO_01_Issue_6_FLASH_PnE U-Multilink&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;There was an error parsing the memory configuration file&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 02 Jul 2017 07:56:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675289#M3530</guid>
      <dc:creator>juliancox</dc:creator>
      <dc:date>2017-07-02T07:56:05Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM driver</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675290#M3531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Julian,&lt;/P&gt;&lt;P&gt;It should not be necessary to select anything in the debug settings and, in fact, it's quite hard to create a debug setting from scratch since the debugger startup and memory files depend on the target&lt;/P&gt;&lt;P&gt;If you create a new project with the USBDM interface does the launch configuration look correct?&lt;/P&gt;&lt;P&gt;see &lt;A class="link-titled" href="http://usbdm.sourceforge.net/USBDM_V4.12/USBDM_JS16/html/eclipse_v10_1__usage_page.html" title="http://usbdm.sourceforge.net/USBDM_V4.12/USBDM_JS16/html/eclipse_v10_1__usage_page.html"&gt;USBDM: Codewarrior - Eclipse V10.x&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The error message seems to be indicating that it is looking for the wrong kind of interface and/or is missing a memory configuration file which is part of the&amp;nbsp; Target settings&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24656i61EC69A1E175B5C2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you try launching without the USBDM plugged in does it complain about a missing BDM?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jul 2017 03:55:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675290#M3531</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2017-07-04T03:55:47Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM driver</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675291#M3532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just moved onto a different machine with a "clean" windows 7 installation. In the devices window it is shown as "JS16"&lt;/P&gt;&lt;P&gt;I downloaded the driver package&amp;nbsp;"USBDMDrivers_1_3_0_Win_x64.msi"&amp;nbsp;from SourceForge and ran the package.&lt;/P&gt;&lt;P&gt;In Device Manager, under "Hardware Debugging Interfaces" it was listed as "USBDM BDM Interface"&lt;/P&gt;&lt;P&gt;I created a new project&amp;nbsp;named Issue_1_BDM&amp;nbsp;with USBDM Interface. The Connection type is "USBDM HCS08 Interface" under "Connections | Preferred BDM" we have "Any Connected BDM " and under that window it says "Generic BDM"&lt;/P&gt;&lt;P&gt;When I launch Debug The message says "No suitable BDM Module Found"&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also when I launch the HCS08 Programmer it says "No Devices Found"&lt;/P&gt;&lt;P&gt;At no time do I see any Comms activity (the COM light never flashes)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 09:48:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675291#M3532</guid>
      <dc:creator>juliancox</dc:creator>
      <dc:date>2017-07-06T09:48:49Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM driver</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675292#M3533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Julian,&lt;/P&gt;&lt;P&gt;I suspect the device is in in-circuit-programming (ICP) mode.&lt;/P&gt;&lt;P&gt;Try the following please:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Open device manager&lt;/LI&gt;&lt;LI&gt;Right-click on the device and open properties&lt;/LI&gt;&lt;LI&gt;Select Details Tab&lt;/LI&gt;&lt;LI&gt;Select Device instance path&lt;/LI&gt;&lt;LI&gt;If it shows something like &lt;STRONG&gt;&lt;EM&gt;USB\VID_15A2&amp;amp;PID_0038\&lt;/EM&gt;&lt;/STRONG&gt;... it is in ICP mode&lt;/LI&gt;&lt;LI&gt;It should show something like &lt;STRONG&gt;&lt;EM&gt;USB\VID_16D0&amp;amp;PID_0567\USBDM-JS16-SWD-0001 &lt;/EM&gt;&lt;/STRONG&gt;&lt;/LI&gt;&lt;LI&gt;If in ICP mode please reflash the firmware from scratch using the instructions here: &lt;A class="link-titled" href="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_JS16/html/construction_page.html" title="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_JS16/html/construction_page.html"&gt;USBDM: BDM Construction and Firmware&lt;/A&gt; (from the top of the page using the JS16 First stage bootloader)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Bye&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24763iDF9D04877A4D7950/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/24811i2032514130C27A48/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Jul 2017 14:43:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/675292#M3533</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2017-07-08T14:43:28Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM driver</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/1478891#M3716</link>
      <description>&lt;P&gt;Hello pgo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using USBDM for MC9S12GA48 microcontroller for programing and debugging. I am using Windows 10 enterprise. My USBDM is based on JM16 design. USBDM is working fine with codewarrior in Win7. I can see the connection in CW5.2 in Win7.&lt;/P&gt;&lt;P&gt;I have installed latest drivers and USBDM in Win 10. I can program my board with HCS Programmer app available in USBDM. But, in CW5.2, I can not see the USBDM in the connection dialog list.&lt;/P&gt;&lt;P&gt;am I missing something?&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Gavali N. K.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jun 2022 08:33:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-driver/m-p/1478891#M3716</guid>
      <dc:creator>nkgavali1</dc:creator>
      <dc:date>2022-06-23T08:33:53Z</dc:date>
    </item>
  </channel>
</rss>