<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックRe: JS16</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/JS16/m-p/519477#M3377</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dietmar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see the answer to your later posting for a discussion of how USBDM handles the security region in the flash.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="" href="https://community.nxp.com/thread/442705?commentID=868480#comment" title="https://community.nxp.com/message/868480?commentID=868480#comment-868480"&gt;https://community.nxp.com/message/868480?commentID=868480#comment-868480&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately I do not have access to 32-bit Windows&amp;nbsp; machines for testing any longer.&lt;/P&gt;&lt;P&gt;The usual reason for problems is incompatibility with the driver.&amp;nbsp; You should try the XP version as well as the later version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 15 Jan 2017 00:29:03 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2017-01-15T00:29:03Z</dc:date>
    <item>
      <title>JS16</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/JS16/m-p/519476#M3376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I would like to program JS16 devices.&lt;/P&gt;&lt;P&gt;On a 32 bit Windows 7 machine, I have no problems using the JS16_Bootloader.exe from version 4.12.1.80.&lt;/P&gt;&lt;P&gt;On a 64 bit Windows 7 machine, I did not yet have success. I tried USBDM 4.12.1.80 and 90.&lt;/P&gt;&lt;P&gt;The drivers are the latest and from the device manager they seem to be the same revisions on both machines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The s19 file does not define a value for 0xFFBA (Checksumbypass), but even with this set to 00 I always end up in the bootloader, even with BLMS* tied to +5V. Before I switched to 64 bit, I did not have problems on this machine either, but at that time I was using a five years old version.&lt;/P&gt;&lt;P&gt;I assume that the 64 bit version somehow does not write a value to address 0xFFBA. I tried also programming via BDM, but that also did not work on the 64 bit machine, even though a verify was successful.&lt;/P&gt;&lt;P&gt;From an internet search, I know that somwhere there must be a thread "DB:6.94:Usbdm Cant Program Js16 At 0xffba (Checksumbypass)", but I can't find that, due to the switch from Freescale to NXP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas?&lt;/P&gt;&lt;P&gt;P.S.: Programming via BDM also does not work on the 32 bit machine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dietmar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jun 2016 13:40:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/JS16/m-p/519476#M3376</guid>
      <dc:creator>dschwertb1</dc:creator>
      <dc:date>2016-06-13T13:40:24Z</dc:date>
    </item>
    <item>
      <title>Re: JS16</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/JS16/m-p/519477#M3377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dietmar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see the answer to your later posting for a discussion of how USBDM handles the security region in the flash.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="" href="https://community.nxp.com/thread/442705?commentID=868480#comment" title="https://community.nxp.com/message/868480?commentID=868480#comment-868480"&gt;https://community.nxp.com/message/868480?commentID=868480#comment-868480&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately I do not have access to 32-bit Windows&amp;nbsp; machines for testing any longer.&lt;/P&gt;&lt;P&gt;The usual reason for problems is incompatibility with the driver.&amp;nbsp; You should try the XP version as well as the later version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 15 Jan 2017 00:29:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/JS16/m-p/519477#M3377</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2017-01-15T00:29:03Z</dc:date>
    </item>
  </channel>
</rss>