<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MC9S08MP16 board program upload OSBDM in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/MC9S08MP16-board-program-upload-OSBDM/m-p/496557#M3341</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem solved, It was problem with one of resistors in my board which has short circuit. I was using TWR-MCF51CN board as BDM debugger. Thanks for responding!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Dec 2015 14:26:08 GMT</pubDate>
    <dc:creator>pawelniewiadoms</dc:creator>
    <dc:date>2015-12-23T14:26:08Z</dc:date>
    <item>
      <title>MC9S08MP16 board program upload OSBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/MC9S08MP16-board-program-upload-OSBDM/m-p/496555#M3339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have MC9S08MP board and I have problem to upload program on it via BDM. I'm using CodeWarrior 10.6 and when I'm trying debug example program this window appears:&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/35345i10A4C54FB12CFCCE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When I reconnect it nothing happens. After click OK this appears:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/35346i7F91EEEE2A0670B8/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Then it's just error when I click 'Abort'. OSBDM is visible in device manager and all drivers are installed properly.&lt;BR /&gt;Please help me with this problem.&lt;BR /&gt;Greetings,&lt;BR /&gt;Pawel Niewiadomski&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Dec 2015 13:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/MC9S08MP16-board-program-upload-OSBDM/m-p/496555#M3339</guid>
      <dc:creator>pawelniewiadoms</dc:creator>
      <dc:date>2015-12-21T13:29:31Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08MP16 board program upload OSBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/MC9S08MP16-board-program-upload-OSBDM/m-p/496556#M3340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pawel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could I check what actual hardware you have?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also - depending on your hardware, are you ONLY cycling the target power, not the power to the BDM.&amp;nbsp; With some hardware this is difficult to do especially if the BDM in integrated into a board with the target hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should also make sure that the delay after removing the power is sufficient for the target Vdd to drop to a very low level to ensure a power-on-reset of the target.&amp;nbsp; With some low-power devices this can be quite a while.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: you would also get a similar error if there is anything incorrect about the connection between the BDM and target.&amp;nbsp; You could check this.&amp;nbsp; In particular check that the BKGD pin has initial activity when trying to connect and then is held low when the power-cycle dialogue appears.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Finally, you could try an external BDM such as P&amp;amp;E multilink or USBDM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Dec 2015 01:59:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/MC9S08MP16-board-program-upload-OSBDM/m-p/496556#M3340</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2015-12-22T01:59:33Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08MP16 board program upload OSBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/MC9S08MP16-board-program-upload-OSBDM/m-p/496557#M3341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem solved, It was problem with one of resistors in my board which has short circuit. I was using TWR-MCF51CN board as BDM debugger. Thanks for responding!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Dec 2015 14:26:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/MC9S08MP16-board-program-upload-OSBDM/m-p/496557#M3341</guid>
      <dc:creator>pawelniewiadoms</dc:creator>
      <dc:date>2015-12-23T14:26:08Z</dc:date>
    </item>
  </channel>
</rss>