<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックOSJTAG activate the JTAG interface without running debugger</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/OSJTAG-activate-the-JTAG-interface-without-running-debugger/m-p/466089#M3258</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the TWR-K21F120M and the connect a debugger from iSystem for hardware trace and debugging.&lt;/P&gt;&lt;P&gt;When I will use the UART interface from the OSJTAG (on-board MC9S08JM60) it enables his JTAG signal to the target when the USB is connected to a host and the other debugger have problems with the JTAG interface.&lt;/P&gt;&lt;P&gt;Exists a solution for disabling the JTAG from OSJTAG during no debugger is connected to this?&lt;/P&gt;&lt;P&gt;In the hardware must the signal OUT_EN (U200 Pin15) deactivate. At the moment exists no jumper for disable the JTAG from the OSJTAG, so I have only a change with a software change or o firmware which only supports the UART device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bernd&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 May 2016 09:20:02 GMT</pubDate>
    <dc:creator>berndmönnicke</dc:creator>
    <dc:date>2016-05-12T09:20:02Z</dc:date>
    <item>
      <title>OSJTAG activate the JTAG interface without running debugger</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/OSJTAG-activate-the-JTAG-interface-without-running-debugger/m-p/466089#M3258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the TWR-K21F120M and the connect a debugger from iSystem for hardware trace and debugging.&lt;/P&gt;&lt;P&gt;When I will use the UART interface from the OSJTAG (on-board MC9S08JM60) it enables his JTAG signal to the target when the USB is connected to a host and the other debugger have problems with the JTAG interface.&lt;/P&gt;&lt;P&gt;Exists a solution for disabling the JTAG from OSJTAG during no debugger is connected to this?&lt;/P&gt;&lt;P&gt;In the hardware must the signal OUT_EN (U200 Pin15) deactivate. At the moment exists no jumper for disable the JTAG from the OSJTAG, so I have only a change with a software change or o firmware which only supports the UART device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bernd&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 09:20:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/OSJTAG-activate-the-JTAG-interface-without-running-debugger/m-p/466089#M3258</guid>
      <dc:creator>berndmönnicke</dc:creator>
      <dc:date>2016-05-12T09:20:02Z</dc:date>
    </item>
  </channel>
</rss>