<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックRe: USBDM Programming Issue</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Programming-Issue/m-p/445908#M3203</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sunil,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The KV10Z128M7 has not been tested and is not currently supported.&lt;/P&gt;&lt;P&gt;I have added the required entries to the attached file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can try using this file if you wish.&amp;nbsp; You would need to replace the existing file in C:\Program Files (x86)\pgo\USBDM 4.12.1.40\DeviceData&lt;/P&gt;&lt;P&gt;I'm not sure of SDID (part ID) - If you could confirm this (it appears on the Programmer dialogue as shown) after Detecting the chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/51803i9F74DC9CBD89E8D8/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Nov 2015 09:23:25 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2015-11-02T09:23:25Z</dc:date>
    <item>
      <title>USBDM Programming Issue</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Programming-Issue/m-p/445907#M3202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am facing issue to flash Kinetis KV10 using USBDM interface.&lt;/P&gt;&lt;P&gt;I have KV10Z128M7 and When I am trying to detect USBDM is detecting KV10Z16M7 but not able to program it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Seems, There is no support of KV10Z128M7 mcu or may be some other issue.&lt;/P&gt;&lt;P&gt;Can any help me out how Can I ,program this mcu using USBDM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sunil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Oct 2015 15:41:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Programming-Issue/m-p/445907#M3202</guid>
      <dc:creator>sunilkumar_sing</dc:creator>
      <dc:date>2015-10-30T15:41:56Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM Programming Issue</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Programming-Issue/m-p/445908#M3203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sunil,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The KV10Z128M7 has not been tested and is not currently supported.&lt;/P&gt;&lt;P&gt;I have added the required entries to the attached file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can try using this file if you wish.&amp;nbsp; You would need to replace the existing file in C:\Program Files (x86)\pgo\USBDM 4.12.1.40\DeviceData&lt;/P&gt;&lt;P&gt;I'm not sure of SDID (part ID) - If you could confirm this (it appears on the Programmer dialogue as shown) after Detecting the chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/51803i9F74DC9CBD89E8D8/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2015 09:23:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Programming-Issue/m-p/445908#M3203</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2015-11-02T09:23:25Z</dc:date>
    </item>
  </channel>
</rss>