<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックRe: Debugging Problem FXTH87xx02 - CodeWarrior - USBDM</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Debugging-Problem-FXTH87xx02-CodeWarrior-USBDM/m-p/439150#M3167</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo pgo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for your message same probleme in the link &lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2024" data-containertype="14" data-content-finding="Community" data-objectid="460885" data-objecttype="2" href="https://community.nxp.com/message/460885#460885" style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #017bba;"&gt;Fail to program FXTH87xx11 using USBDM&lt;/A&gt;&lt;/P&gt;&lt;P&gt;as in my case!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seem to be that have overwritten the preprogrammed areas of my sensor, too!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my first question there was a mistake i'm using the sensor fxth870502 (so the 1 axis one) not the fxth870511&lt;/P&gt;&lt;P&gt;Is there somebody who can send me an image file&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;a&amp;nbsp; for the one axis Sensor FXTH870502?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Cheers&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Jun 2015 17:18:29 GMT</pubDate>
    <dc:creator>wernermoeck</dc:creator>
    <dc:date>2015-06-09T17:18:29Z</dc:date>
    <item>
      <title>Debugging Problem FXTH87xx02 - CodeWarrior - USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Debugging-Problem-FXTH87xx02-CodeWarrior-USBDM/m-p/439148#M3165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo together, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i try to debug the TPMS Sensor FXTH87xx02 with CodeWarrior and a USBDM Programmer. &lt;/P&gt;&lt;P&gt;Programming of the following example project for the 1 Axis Sensor is working. &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30993iFBA467467E0123F7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If i start to debug the programm in the stepping mode of codewarrior then i get a error in the following line by reading the Voltage.&lt;/P&gt;&lt;P&gt;Temperature- and Pressure- Measurment also gives a error in the same way!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31117i86831C4751C7D060/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31165iCE3C1AC217AFD135/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Someone has an idea what the problem could be?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could it be that the preprogrammed areas of the FXTH870511 were overwritten by mistake?&lt;/P&gt;&lt;P&gt;Therefore the question has somebody a Image File for the one axis Sensor FXTH870511? I can only find one for the two axis sensor!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope someone can help me...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards &lt;/P&gt;&lt;P&gt;Werner &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jun 2015 16:12:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Debugging-Problem-FXTH87xx02-CodeWarrior-USBDM/m-p/439148#M3165</guid>
      <dc:creator>wernermoeck</dc:creator>
      <dc:date>2015-06-08T16:12:40Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Problem FXTH87xx02 - CodeWarrior - USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Debugging-Problem-FXTH87xx02-CodeWarrior-USBDM/m-p/439149#M3166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Werner,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is quite long discussion of using USBDM with this chip here:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/460885"&gt;Fail to program FXTH87xx11 using USBDM&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A brief description of the required set-up for USBDM for programming and debugging is given here:&lt;/P&gt;&lt;P&gt;&lt;A href="http://usbdm.sourceforge.net/USBDM_V4.11/USBDM_JS16/html/_f_x_t_h87xx11.html" title="http://usbdm.sourceforge.net/USBDM_V4.11/USBDM_JS16/html/_f_x_t_h87xx11.html"&gt;USBDM: Programming devices while preserving data&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are two issues:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;It is very easy to accidentally erase the pre-programmed routines that are in the FXTH87.&amp;nbsp; It is necessary to set up selective erase in Codewarrior.&amp;nbsp; See second link above.&amp;nbsp; If you accidentally erase the chip you have to restore the missing code somehow.&lt;/LI&gt;&lt;LI&gt;You don't have the source code for the above flash routines so you cannot "step-into" the routines and expect source-level debugging - Only assembly code which is pretty useless.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope the above helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2015 05:05:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Debugging-Problem-FXTH87xx02-CodeWarrior-USBDM/m-p/439149#M3166</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2015-06-09T05:05:28Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Problem FXTH87xx02 - CodeWarrior - USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Debugging-Problem-FXTH87xx02-CodeWarrior-USBDM/m-p/439150#M3167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo pgo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for your message same probleme in the link &lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" data-containerid="2024" data-containertype="14" data-content-finding="Community" data-objectid="460885" data-objecttype="2" href="https://community.nxp.com/message/460885#460885" style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #017bba;"&gt;Fail to program FXTH87xx11 using USBDM&lt;/A&gt;&lt;/P&gt;&lt;P&gt;as in my case!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seem to be that have overwritten the preprogrammed areas of my sensor, too!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my first question there was a mistake i'm using the sensor fxth870502 (so the 1 axis one) not the fxth870511&lt;/P&gt;&lt;P&gt;Is there somebody who can send me an image file&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;a&amp;nbsp; for the one axis Sensor FXTH870502?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Cheers&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2015 17:18:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Debugging-Problem-FXTH87xx02-CodeWarrior-USBDM/m-p/439150#M3167</guid>
      <dc:creator>wernermoeck</dc:creator>
      <dc:date>2015-06-09T17:18:29Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Problem FXTH87xx02 - CodeWarrior - USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Debugging-Problem-FXTH87xx02-CodeWarrior-USBDM/m-p/439151#M3168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Werner,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are still looking for an image file please see bottom of this updated page:&lt;/P&gt;&lt;P&gt;&lt;A href="http://usbdm.sourceforge.net/USBDM_V4.11/USBDM_JS16/html/_f_x_t_h87xx11.html" title="http://usbdm.sourceforge.net/USBDM_V4.11/USBDM_JS16/html/_f_x_t_h87xx11.html"&gt;USBDM: Programming devices while preserving data&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 11:13:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Debugging-Problem-FXTH87xx02-CodeWarrior-USBDM/m-p/439151#M3168</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2015-06-22T11:13:29Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Problem FXTH87xx02 - CodeWarrior - USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Debugging-Problem-FXTH87xx02-CodeWarrior-USBDM/m-p/439152#M3169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you perfect :-)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2015 21:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Debugging-Problem-FXTH87xx02-CodeWarrior-USBDM/m-p/439152#M3169</guid>
      <dc:creator>wernermoeck</dc:creator>
      <dc:date>2015-06-22T21:33:27Z</dc:date>
    </item>
  </channel>
</rss>