<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックTWR-SENSOR OSBDM problem</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/TWR-SENSOR-OSBDM-problem/m-p/408364#M3089</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to ask for a help with onboard OSBDM in TWR-SENSOR module. I'm using Codewarrior 10.6, it automatically updates OSBDM firmware to the latest version. However TWR-SENSOR is unable to work with this latest version, target MCU is not powered. It seems that the problem is caused by wrong polarity of VTRG_EN signal, it should be active high in correct OSBDM implementation but TWR-SENSOR is wired in such a way that it is active low. Please see TWR-SENSOR schematic (SCH-26439, rev C) around transistor Q1 and some working board for comparison, for example TWR-S08MM128 (SCH-26136, rev D) around U2, described difference is evident here. Please, can someone from FSL confirm this errata? If yes, is there a software fix, that is latest OSBDM firmware with active low VTRG_EN polarity? If the software fix is not available, is there any recommended hardware workaround?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 18 Oct 2015 20:59:05 GMT</pubDate>
    <dc:creator>mst_</dc:creator>
    <dc:date>2015-10-18T20:59:05Z</dc:date>
    <item>
      <title>TWR-SENSOR OSBDM problem</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/TWR-SENSOR-OSBDM-problem/m-p/408364#M3089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to ask for a help with onboard OSBDM in TWR-SENSOR module. I'm using Codewarrior 10.6, it automatically updates OSBDM firmware to the latest version. However TWR-SENSOR is unable to work with this latest version, target MCU is not powered. It seems that the problem is caused by wrong polarity of VTRG_EN signal, it should be active high in correct OSBDM implementation but TWR-SENSOR is wired in such a way that it is active low. Please see TWR-SENSOR schematic (SCH-26439, rev C) around transistor Q1 and some working board for comparison, for example TWR-S08MM128 (SCH-26136, rev D) around U2, described difference is evident here. Please, can someone from FSL confirm this errata? If yes, is there a software fix, that is latest OSBDM firmware with active low VTRG_EN polarity? If the software fix is not available, is there any recommended hardware workaround?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Oct 2015 20:59:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/TWR-SENSOR-OSBDM-problem/m-p/408364#M3089</guid>
      <dc:creator>mst_</dc:creator>
      <dc:date>2015-10-18T20:59:05Z</dc:date>
    </item>
  </channel>
</rss>