<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックProblem installing drivers for USBDM under Win7 64 bit</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Problem-installing-drivers-for-USBDM-under-Win7-64-bit/m-p/393825#M3048</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I installed OpenSDAv1.sx on a FRDM-KL25Z board, and installed the USBDM driver 1.3.0, using USBDM_Drivers_1_3_0_Win_x64.msi installer on my Win7 64 PC. When I plug in the FRDM-KL25Z board, Windows fails to find suitable drivers for it, even if I manually direct it to the "C:\Program Files (x86)\pgo\USBDM Drivers 1.3.0\Drivers" directory. I have noticed that the FRDM-KL25Z firmware identifies as a VID/PID of 16D0/06A5, while the "USBDMSerial.inf" file uses the values 16D0/0567, so I modified the PID to 06A5 and then installing the CDC part of the USB composite driver succeeds. However, the USBDM specific part still fails. Possibly related, I saw that in the file "&lt;STRONG class="final-path" style="color: #000000; font-family: Helvetica, arial, nimbussansl, liberationsans, freesans, clean, sans-serif, 'Segoe UI Emoji', 'Segoe UI Symbol'; font-size: 18px;"&gt;usbdm.rules&lt;/STRONG&gt;" found online as part of USBDM software for Linux specifies that "&lt;SPAN style="color: #333333; font-family: Consolas, 'Liberation Mono', Menlo, Courier, monospace; font-size: 12px;"&gt;Note: HEX numbers must be lower case - yes really!!!!&lt;/SPAN&gt;", yet a line below for adding the 16D0/06A5 combination still uses a capital A for 06A5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea how to proceed with installing drivers for the USBDM on FRDM-KL25Z?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Uri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Oct 2015 16:36:03 GMT</pubDate>
    <dc:creator>uribendelac</dc:creator>
    <dc:date>2015-10-13T16:36:03Z</dc:date>
    <item>
      <title>Problem installing drivers for USBDM under Win7 64 bit</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Problem-installing-drivers-for-USBDM-under-Win7-64-bit/m-p/393825#M3048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I installed OpenSDAv1.sx on a FRDM-KL25Z board, and installed the USBDM driver 1.3.0, using USBDM_Drivers_1_3_0_Win_x64.msi installer on my Win7 64 PC. When I plug in the FRDM-KL25Z board, Windows fails to find suitable drivers for it, even if I manually direct it to the "C:\Program Files (x86)\pgo\USBDM Drivers 1.3.0\Drivers" directory. I have noticed that the FRDM-KL25Z firmware identifies as a VID/PID of 16D0/06A5, while the "USBDMSerial.inf" file uses the values 16D0/0567, so I modified the PID to 06A5 and then installing the CDC part of the USB composite driver succeeds. However, the USBDM specific part still fails. Possibly related, I saw that in the file "&lt;STRONG class="final-path" style="color: #000000; font-family: Helvetica, arial, nimbussansl, liberationsans, freesans, clean, sans-serif, 'Segoe UI Emoji', 'Segoe UI Symbol'; font-size: 18px;"&gt;usbdm.rules&lt;/STRONG&gt;" found online as part of USBDM software for Linux specifies that "&lt;SPAN style="color: #333333; font-family: Consolas, 'Liberation Mono', Menlo, Courier, monospace; font-size: 12px;"&gt;Note: HEX numbers must be lower case - yes really!!!!&lt;/SPAN&gt;", yet a line below for adding the 16D0/06A5 combination still uses a capital A for 06A5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea how to proceed with installing drivers for the USBDM on FRDM-KL25Z?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Uri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Oct 2015 16:36:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Problem-installing-drivers-for-USBDM-under-Win7-64-bit/m-p/393825#M3048</guid>
      <dc:creator>uribendelac</dc:creator>
      <dc:date>2015-10-13T16:36:03Z</dc:date>
    </item>
    <item>
      <title>Re: Problem installing drivers for USBDM under Win7 64 bit</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Problem-installing-drivers-for-USBDM-under-Win7-64-bit/m-p/393826#M3049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Uri,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect you are using old drivers with new firmware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure that you are using the firmware from the latest version (installed in the FlashImages directory with &lt;A class="name" href="http://sourceforge.net/projects/usbdm/files/Version%204.12.1/Software/USBDM_4_12_1_30_Win.msi/download" title="Click to download USBDM_4_12_1_30_Win.msi"&gt;USBDM_4_12_1_30_Win.msi&lt;/A&gt;)&amp;nbsp; with the drivers from the latest version &lt;A class="name" href="http://sourceforge.net/projects/usbdm/files/Version%204.12.1/Drivers/USBDM_Drivers_4_12_1_Win_x64.msi/download" title="Click to download USBDM_Drivers_4_12_1_Win_x64.msi"&gt;USBDM_Drivers_4_12_1_Win_x64.msi&lt;/A&gt;​ .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PID/VID number had to be changed with the signing of the drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this doesn't fix the problem please re-post and I will have another look.&lt;/P&gt;&lt;P&gt;In particular, please post information on&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;What version of USBM (and the firmware being used)&lt;/LI&gt;&lt;LI&gt;What version of driver&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will look at the Linux files but they are obviously not relevant to WIN.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 10:21:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Problem-installing-drivers-for-USBDM-under-Win7-64-bit/m-p/393826#M3049</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2015-10-14T10:21:21Z</dc:date>
    </item>
    <item>
      <title>Re: Problem installing drivers for USBDM under Win7 64 bit</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Problem-installing-drivers-for-USBDM-under-Win7-64-bit/m-p/393827#M3050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi PGO,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your prompt response.&lt;/P&gt;&lt;P&gt;Yes, indeed I was apparently using outdated drivers. It seems to work perfectly well with the correct drivers, thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Uri&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 16:32:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Problem-installing-drivers-for-USBDM-under-Win7-64-bit/m-p/393827#M3050</guid>
      <dc:creator>uribendelac</dc:creator>
      <dc:date>2015-10-14T16:32:50Z</dc:date>
    </item>
  </channel>
</rss>