<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックRe: Using KDS with USBDM</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Using-KDS-with-USBDM/m-p/346098#M2959</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gustavo leal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you tell me the full name of you chip?&lt;/P&gt;&lt;P&gt;What the detail operation system you are using? You can try it in windows 7 system, it can works ok.&lt;/P&gt;&lt;P&gt;You should make sure your USBDM can works in your platform.&lt;/P&gt;&lt;P&gt;About the configuration, you can refer to this link and check it again:&lt;/P&gt;&lt;P&gt;&lt;A href="http://usbdm.sourceforge.net/USBDM_V4.10/Freedom/html/code_sourcery_new_project.html"&gt;USBDM Functions in Eclipse (including Kinetis Design Studio)&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jingjing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Mar 2015 05:09:40 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2015-03-26T05:09:40Z</dc:date>
    <item>
      <title>Using KDS with USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Using-KDS-with-USBDM/m-p/346097#M2958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I've managed to install and run KDS with USBDM and configure it successfully. I'm running a Ubuntu Server installation.&lt;/P&gt;&lt;P&gt;However, when I try to run (or debug) an application, there's an error in the final launch sequence:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="p1"&gt;Error in final launch sequence&lt;/P&gt;&lt;P class="p2"&gt;Failed to execute MI command:&lt;/P&gt;&lt;P class="p3"&gt;monitor reset halt&lt;/P&gt;&lt;P class="p3"&gt;Error message from debugger back end:&lt;/P&gt;&lt;P class="p1"&gt;"monitor" command not supported by this target.&lt;/P&gt;&lt;P class="p1"&gt;Failed to execute MI command:&lt;/P&gt;&lt;P class="p1"&gt;monitor reset halt&lt;/P&gt;&lt;P class="p1"&gt;Error message from debugger back end:&lt;/P&gt;&lt;P class="p1"&gt;"monitor" command not supported by this target.&lt;/P&gt;&lt;P class="p1"&gt;"monitor" command not supported by this target.&lt;/P&gt;&lt;P class="p1"&gt;&lt;/P&gt;&lt;P class="p1"&gt;&lt;/P&gt;&lt;P class="p1"&gt;I have GDB installed on KDS.&lt;/P&gt;&lt;P class="p1"&gt;What could it be?&lt;/P&gt;&lt;P class="p1"&gt;&lt;/P&gt;&lt;P class="p1"&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2015 18:52:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Using-KDS-with-USBDM/m-p/346097#M2958</guid>
      <dc:creator>gustavsl</dc:creator>
      <dc:date>2015-03-24T18:52:49Z</dc:date>
    </item>
    <item>
      <title>Re: Using KDS with USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Using-KDS-with-USBDM/m-p/346098#M2959</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gustavo leal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you tell me the full name of you chip?&lt;/P&gt;&lt;P&gt;What the detail operation system you are using? You can try it in windows 7 system, it can works ok.&lt;/P&gt;&lt;P&gt;You should make sure your USBDM can works in your platform.&lt;/P&gt;&lt;P&gt;About the configuration, you can refer to this link and check it again:&lt;/P&gt;&lt;P&gt;&lt;A href="http://usbdm.sourceforge.net/USBDM_V4.10/Freedom/html/code_sourcery_new_project.html"&gt;USBDM Functions in Eclipse (including Kinetis Design Studio)&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jingjing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 05:09:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Using-KDS-with-USBDM/m-p/346098#M2959</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2015-03-26T05:09:40Z</dc:date>
    </item>
    <item>
      <title>Re: Using KDS with USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Using-KDS-with-USBDM/m-p/346099#M2960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. I'm using the MKL26Z64.&lt;/P&gt;&lt;P&gt;I'm running it on a Ubuntu 14.04 server with XFCE.&lt;/P&gt;&lt;P&gt;I managed to partially solve the problem.&lt;/P&gt;&lt;P&gt;One of the libraries required to launch the USBDM ARM GDB Server (libwx_gtk2u-unnoficial) was missing. I installed this library and tcl-8.5 and the GDB server launched.&lt;/P&gt;&lt;P&gt;Now I can flash the chip using the ARM Flash Programmer application, but I still can't do it from inside KDS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Gustavo.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2015 16:04:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Using-KDS-with-USBDM/m-p/346099#M2960</guid>
      <dc:creator>gustavsl</dc:creator>
      <dc:date>2015-03-26T16:04:43Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Using KDS with USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Using-KDS-with-USBDM/m-p/346100#M2961</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gustavo Leal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; From the kds_user_guide.pdf, it need ubuntu14.04 LTS,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49066i8F335246FCB2C724/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, maybe KDS in your ubuntu 14.04 with XFCE will have problem, you should better working in the operation system which KDS defined.&lt;/P&gt;&lt;P&gt;At least, when I working in Window7 ,USBDM can works ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jingjing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Mar 2015 01:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Using-KDS-with-USBDM/m-p/346100#M2961</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2015-03-27T01:47:28Z</dc:date>
    </item>
    <item>
      <title>Re: Using KDS with USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Using-KDS-with-USBDM/m-p/1290152#M3639</link>
      <description>&lt;P&gt;In my case I get that all the time when I have too many breakpoints enabled.&amp;nbsp; Using KE06 chips that is two, and since you need 1 for main . . .&amp;nbsp; &amp;nbsp; I also get it if one of the breakpoints is not able to be properly set.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jun 2021 18:43:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Using-KDS-with-USBDM/m-p/1290152#M3639</guid>
      <dc:creator>andrewmeyerbti</dc:creator>
      <dc:date>2021-06-09T18:43:09Z</dc:date>
    </item>
  </channel>
</rss>