<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USBDM in KDS 2.0 in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-in-KDS-2-0/m-p/340831#M2931</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not able to see USBDM option in the Debug Configurations in KDS 2.0. I've installed USBDM 4.10.6.250 and USBDM Drivers v1.3.0 that actually run on a FRDM-KL25Z target but cannot start a debug session using USBDM. I also update KDS 2.0 with CDT main and optional features with no success. How can I get the correct plugin?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;gaston&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Feb 2015 13:01:46 GMT</pubDate>
    <dc:creator>gschelotto</dc:creator>
    <dc:date>2015-02-26T13:01:46Z</dc:date>
    <item>
      <title>USBDM in KDS 2.0</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-in-KDS-2-0/m-p/340831#M2931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not able to see USBDM option in the Debug Configurations in KDS 2.0. I've installed USBDM 4.10.6.250 and USBDM Drivers v1.3.0 that actually run on a FRDM-KL25Z target but cannot start a debug session using USBDM. I also update KDS 2.0 with CDT main and optional features with no success. How can I get the correct plugin?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;gaston&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Feb 2015 13:01:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-in-KDS-2-0/m-p/340831#M2931</guid>
      <dc:creator>gschelotto</dc:creator>
      <dc:date>2015-02-26T13:01:46Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM in KDS 2.0</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-in-KDS-2-0/m-p/340832#M2932</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gaston,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;There should be a &lt;STRONG&gt;&lt;EM&gt;usbdm.link&lt;/EM&gt;&lt;/STRONG&gt;&amp;nbsp; file in the &lt;EM&gt;&lt;STRONG&gt;....\KDS_2.0.0\eclipse\dropins &lt;/STRONG&gt;&lt;/EM&gt;directory.&amp;nbsp; If not then the installation failed in some way.&lt;/LI&gt;&lt;LI&gt;If the above file is present then KDS should pick up the USBDM plugins on the next start.&amp;nbsp; This may not occur if the permissions associated with some of the KDS installation are incorrect.&amp;nbsp; This prevents KDS from changing its own configuration.&amp;nbsp; &lt;/LI&gt;&lt;LI&gt;Check if the plugins as loading: &lt;UL&gt;&lt;LI&gt;From the menu select &lt;STRONG&gt;&lt;EM&gt;Help About Kinetis Design Studio&lt;/EM&gt;&lt;/STRONG&gt; &lt;/LI&gt;&lt;LI&gt;Click on &lt;EM&gt;&lt;STRONG&gt;Installation Details&lt;/STRONG&gt;&lt;/EM&gt;&lt;/LI&gt;&lt;LI&gt;Go to the &lt;EM&gt;&lt;STRONG&gt;Plug-ins&lt;/STRONG&gt;&lt;/EM&gt; Tab&lt;/LI&gt;&lt;LI&gt;Click on the top of the &lt;EM&gt;&lt;STRONG&gt;Plug-in Id&lt;/STRONG&gt;&lt;/EM&gt; column to sort by ID&lt;/LI&gt;&lt;LI&gt;You should see something similar to (numbers will vary from shown but should all be the same):&lt;/LI&gt;&lt;LI&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50902i1838FAF8EAE1C7DE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_29.png" alt="pastedImage_29.png" /&gt;&lt;/span&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;If the plug-ins are not present you can try the following:&lt;UL&gt;&lt;LI&gt;Go to the eclipse &lt;EM&gt;&lt;STRONG&gt;....\KDS_2.0.0\eclipse&lt;/STRONG&gt;&lt;/EM&gt; directory and change its permissions so that you have write permission for it and its sub-directories. Restart KDS.&lt;/LI&gt;&lt;LI&gt;If this fails - Right-click on &lt;EM&gt;&lt;STRONG&gt;KDS icon&lt;/STRONG&gt;&lt;/EM&gt; or &lt;STRONG&gt;&lt;EM&gt;kinetis-design-studio.exe&lt;/EM&gt;&lt;/STRONG&gt; and select &lt;EM&gt;&lt;STRONG&gt;Run as administrator&lt;/STRONG&gt;&lt;/EM&gt;&lt;/LI&gt;&lt;LI&gt;If this fails - Go to a command line and run &lt;STRONG&gt;&lt;EM&gt;kinetis-design-studio.exe -initialise&lt;/EM&gt;&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2015 01:15:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-in-KDS-2-0/m-p/340832#M2932</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2015-03-02T01:15:08Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM in KDS 2.0</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-in-KDS-2-0/m-p/340833#M2933</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the installation failed for the USBDSM-KDS files. Now it fixed, thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;gaston&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2015 12:28:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-in-KDS-2-0/m-p/340833#M2933</guid>
      <dc:creator>gschelotto</dc:creator>
      <dc:date>2015-03-02T12:28:43Z</dc:date>
    </item>
  </channel>
</rss>