<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Failed to resume target process. Downloading binary to target... in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Failed-to-resume-target-process-Downloading-binary-to-target/m-p/334848#M2862</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello PGO,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for writing. I have added the 3 lines in the file "C:\Program Files (x86)\pgo\USBDM 4.10.6.200\DeviceData\arm_devices.xml" just below the three lines for KE02 M2 devices but it is not working :-( I have created a new project in a new workspace, and it is still written "DEVICE = '_DEFAULT'" in the console. Do I need to do something to force CodeWarrior taking care of the new configuration ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: I have created a new project with a KE02 M2 device (well, I don't now the difference between the two except the maximum clock speed) and launched the debug of a very simple application with CodeWarrior and it is working. So issue is only for the M4 devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Joel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Oct 2014 17:38:51 GMT</pubDate>
    <dc:creator>Joel69003</dc:creator>
    <dc:date>2014-10-20T17:38:51Z</dc:date>
    <item>
      <title>Failed to resume target process. Downloading binary to target...</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Failed-to-resume-target-process-Downloading-binary-to-target/m-p/334846#M2860</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all, and particularly PGO,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm experimenting issues with CodeWarrior and the USBDM with MKE02Z64M4 device. I have created a project and keep all default options. However, it is not possible to load and debug the application. I get the following error when launching the debugging:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="error.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46928iA331072373AA2378/image-size/large?v=v2&amp;amp;px=999" role="button" title="error.PNG" alt="error.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the console:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="console.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46929i9A27088DE10D7433/image-size/large?v=v2&amp;amp;px=999" role="button" title="console.PNG" alt="console.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My USBDM is "USBDM_SWD_JS16CWJ". Software version is 4.10.6.200, drivers 1.3.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am able to program the target with the ARM programmer provided with the USBDM (it works well) but it is not very convenient to debug the application...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you experimented this kind of issues ? Thanks for your help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Joel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Oct 2014 23:42:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Failed-to-resume-target-process-Downloading-binary-to-target/m-p/334846#M2860</guid>
      <dc:creator>Joel69003</dc:creator>
      <dc:date>2014-10-18T23:42:13Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to resume target process. Downloading binary to target...</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Failed-to-resume-target-process-Downloading-binary-to-target/m-p/334847#M2861</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is not setting the device correctly (Hence the _DEFAULT) in the flash programming log.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This probably means that I have not correctly set an alias for the device.&amp;nbsp; Codewarrior uses different names internally for devices and these are mapped to the usual names by an alias entry in the database.&lt;/P&gt;&lt;P&gt;I probably have missed the one for the device you are using.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will check this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS Confirmed missing entries.&amp;nbsp; This will be corrected in the next version or you can try manually adding the following lines to near the end of &lt;STRONG&gt;&lt;EM&gt;arm_devices.xml&lt;/EM&gt;&lt;/STRONG&gt; (after similar ones for KE02Z16M2):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&amp;lt;device name="KE02Z16M4"&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;alias="MKE02Z16M4"&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;hidden="true"/&amp;gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&amp;lt;device name="KE02Z32M4"&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;alias="MKE02Z32M4"&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;hidden="true"/&amp;gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;&amp;lt;device name="KE02Z64M4"&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;alias="MKE02Z64M4"&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;hidden="true"/&amp;gt;&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt; &lt;/TD&gt;&lt;TD&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Oct 2014 22:33:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Failed-to-resume-target-process-Downloading-binary-to-target/m-p/334847#M2861</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-10-19T22:33:09Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to resume target process. Downloading binary to target...</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Failed-to-resume-target-process-Downloading-binary-to-target/m-p/334848#M2862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello PGO,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for writing. I have added the 3 lines in the file "C:\Program Files (x86)\pgo\USBDM 4.10.6.200\DeviceData\arm_devices.xml" just below the three lines for KE02 M2 devices but it is not working :-( I have created a new project in a new workspace, and it is still written "DEVICE = '_DEFAULT'" in the console. Do I need to do something to force CodeWarrior taking care of the new configuration ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: I have created a new project with a KE02 M2 device (well, I don't now the difference between the two except the maximum clock speed) and launched the debug of a very simple application with CodeWarrior and it is working. So issue is only for the M4 devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Joel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Oct 2014 17:38:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Failed-to-resume-target-process-Downloading-binary-to-target/m-p/334848#M2862</guid>
      <dc:creator>Joel69003</dc:creator>
      <dc:date>2014-10-20T17:38:51Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to resume target process. Downloading binary to target...</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Failed-to-resume-target-process-Downloading-binary-to-target/m-p/334849#M2863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The current version adds these aliases so I would expect it to work now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Oct 2014 20:45:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Failed-to-resume-target-process-Downloading-binary-to-target/m-p/334849#M2863</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-10-27T20:45:41Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to resume target process. Downloading binary to target...</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Failed-to-resume-target-process-Downloading-binary-to-target/m-p/334850#M2864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi PGO,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have installed 4.10.6.210 and the issue is now corrected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Joel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Oct 2014 19:50:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Failed-to-resume-target-process-Downloading-binary-to-target/m-p/334850#M2864</guid>
      <dc:creator>Joel69003</dc:creator>
      <dc:date>2014-10-28T19:50:37Z</dc:date>
    </item>
    <item>
      <title>Re: Failed to resume target process. Downloading binary to target...</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Failed-to-resume-target-process-Downloading-binary-to-target/m-p/334851#M2865</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello PGO&lt;/P&gt;&lt;P&gt;I meet the same problems using the USBDM 4.10.6.250 to Debug the DSC MC56F8345 and MC56F84789 with Codewarrior 10.6.But the information in Console is different.Here is the details:&lt;/P&gt;&lt;P&gt;Executing Initialization File: E:\Codewarrior\84789_BDM/Project_Settings/Debugger/MC56F84789.tcl&lt;/P&gt;&lt;P&gt;radix x &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config hexprefix 0x &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemWidth 16 &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemAccess 16 &lt;/P&gt;&lt;P&gt;cmdwin::eclipse::config MemSwap off &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Starting 3rd party flash programming...&lt;/P&gt;&lt;P&gt;DiMemoryDownload() - DI_DNLD_TERMINATE - Programming memory image...&lt;/P&gt;&lt;P&gt;===========================================================&lt;/P&gt;&lt;P&gt;Programming target&lt;/P&gt;&lt;P&gt;&amp;nbsp; Device = 'MC56F84585'&lt;/P&gt;&lt;P&gt;&amp;nbsp; Trim, F=0, NVA@0000, clock@0000&lt;/P&gt;&lt;P&gt;&amp;nbsp; Ram[0000...3FFF]&lt;/P&gt;&lt;P&gt;&amp;nbsp; Erase=EraseMass&lt;/P&gt;&lt;P&gt;&amp;nbsp; Security=intelligent&lt;/P&gt;&lt;P&gt;&amp;nbsp; Total bytes=35556&lt;/P&gt;&lt;P&gt;&amp;nbsp; doRamWrites=T&lt;/P&gt;&lt;P&gt;Erase Time = 3.48 s, Speed = 9.97 kBytes/s, rc = 0&lt;/P&gt;&lt;P&gt;DiMemoryDownload() - DI_DNLD_TERMINATE - Programming complete, rc = 7&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for your attention,&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Best Regards,&lt;/P&gt;&lt;P style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; yongsheng&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Apr 2015 16:10:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Failed-to-resume-target-process-Downloading-binary-to-target/m-p/334851#M2865</guid>
      <dc:creator>wangyongsheng</dc:creator>
      <dc:date>2015-04-18T16:10:34Z</dc:date>
    </item>
  </channel>
</rss>