<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Fail to program MC9S08PT60 using USBDM in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329741#M2851</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes I cycled power to the board. Yesterday I measured waveforms of BKGD and reset pin and found the BKGD pin voltage level is not correct, I changed the pull-up resistor from 10k ohms to 2kohms. Now the programmer start to detect ID of MCU. However it detected the PT to PA series. I will find out the log and attach them here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Shucheng Zhu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Sep 2014 23:24:03 GMT</pubDate>
    <dc:creator>shuchengzhu</dc:creator>
    <dc:date>2014-09-22T23:24:03Z</dc:date>
    <item>
      <title>Fail to program MC9S08PT60 using USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329736#M2846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to use USBDM commercial products to program the MC9S08PT60, however the programmer can not detect the chip ID. It gave error like: could not launch the BDM, the target MCU may be secured. I don't know how to fix this problem. Does this MCU requires a new version of BDM??? Hope someone can help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Sep 2014 22:59:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329736#M2846</guid>
      <dc:creator>shuchengzhu</dc:creator>
      <dc:date>2014-09-18T22:59:05Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to program MC9S08PT60 using USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329737#M2847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shucheng,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did a quick test with a JS16 based BDM&lt;/P&gt;&lt;P&gt;&lt;A href="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_JS16/html/index.html" title="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_JS16/html/index.html"&gt;http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_JS16/html/index.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and it seemed to work OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is a bit unclear what the problem is from your description.&amp;nbsp; Could you do the following:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Start the stand-alone HCS08 programmer&lt;/LI&gt;&lt;LI&gt;Manually select the device&lt;/LI&gt;&lt;LI&gt;Load a test image&lt;/LI&gt;&lt;LI&gt;Program to target&lt;/LI&gt;&lt;LI&gt;Report exactly what error you get.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;If you want to be more helpful you can repeat the above using the debug version of the HCS08 programmer which is available in the installation directory.&amp;nbsp; Please post the Programmer log file and the usbdm.log.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also provide the following information:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;What programmer you are using.&amp;nbsp; There are several so it is quite unclear which you are using. You can look at this web sit&amp;nbsp; &lt;A href="http://usbdm.sourceforge.net/" title="http://usbdm.sourceforge.net/"&gt;USBDM: USBDM Debugger interface for Freescale RS08,HCS08,HCS12,Coldfire and ARM-Kinetis Devices.&lt;/A&gt; to help identify or alternatively since it is a commercial version can you provide a link to a web page?&lt;/LI&gt;&lt;LI&gt;What operating system&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 Sep 2014 00:04:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329737#M2847</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-09-21T00:04:21Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to program MC9S08PT60 using USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329738#M2848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for reply me. That is my first time to use USBDM. So I got several problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I set the stand-alone HCS08 programmer as shown in Fig.1 and 2 &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46176i4B3E1C9AAF46334C/image-size/large?v=v2&amp;amp;px=999" title="programmer setting 1.png" alt="programmer setting 1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Fig.1&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46178i22E6E9165D904111/image-size/large?v=v2&amp;amp;px=999" title="programmer setting 2.png" alt="programmer setting 2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Fig.2&lt;/P&gt;&lt;P&gt;When I tried to detect the chip ID, it started to give errors in following figures:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46179i80845FE8E8FAFA12/image-size/large?v=v2&amp;amp;px=999" title="programmer detect ID error.png" alt="programmer detect ID error.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46180i182112B6B47805AC/image-size/large?v=v2&amp;amp;px=999" title="programmer detect ID error2.png" alt="programmer detect ID error2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I also tried to load the Hex file: HCS08-PTxx-flash-program.abs.s19. The programmers gave such following errors:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46181i5E4785634C76686B/image-size/large?v=v2&amp;amp;px=999" title="programmer example error.png" alt="programmer example error.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46185i085790F0B026A8EC/image-size/large?v=v2&amp;amp;px=999" title="programmer example error2.png" alt="programmer example error2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The USBDM I used based on JS16. The website is &lt;A href="http://www.myhcs08.com/show.php?contentid=367" title="http://www.myhcs08.com/show.php?contentid=367"&gt;USBDM_JS16仿真下载器-售价40元_开发工具_北京飞锐泰克科技有限公司&lt;/A&gt;. The system I used is windows 7 32bit system.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Sep 2014 01:27:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329738#M2848</guid>
      <dc:creator>shuchengzhu</dc:creator>
      <dc:date>2014-09-22T01:27:06Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to program MC9S08PT60 using USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329739#M2849</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MCU I used is M9S8PT60VLH. I tried with debug version as well, but I could not find any log file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Shucheng Zhu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Sep 2014 01:40:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329739#M2849</guid>
      <dc:creator>shuchengzhu</dc:creator>
      <dc:date>2014-09-22T01:40:26Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to program MC9S08PT60 using USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329740#M2850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shucheng,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The log file are in &lt;EM&gt;&lt;STRONG&gt;%appdata%/usbdm&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;The useful files would be &lt;EM&gt;&lt;STRONG&gt;FlashProgrammer_HCS08.log&lt;/STRONG&gt;&lt;/EM&gt; and &lt;EM&gt;&lt;STRONG&gt;usbdm.log&lt;/STRONG&gt;&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I assume you did try cycling the power when the dialogue pops up?&amp;nbsp; Some devices can't be connected to unless the power is cycled while the BKGD signal is held low.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Sep 2014 07:32:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329740#M2850</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-09-22T07:32:07Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to program MC9S08PT60 using USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329741#M2851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes I cycled power to the board. Yesterday I measured waveforms of BKGD and reset pin and found the BKGD pin voltage level is not correct, I changed the pull-up resistor from 10k ohms to 2kohms. Now the programmer start to detect ID of MCU. However it detected the PT to PA series. I will find out the log and attach them here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Shucheng Zhu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Sep 2014 23:24:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329741#M2851</guid>
      <dc:creator>shuchengzhu</dc:creator>
      <dc:date>2014-09-22T23:24:03Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to program MC9S08PT60 using USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329742#M2852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shucheng,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will have a look at the logs tonight,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the meantime you could try &lt;EM&gt;&lt;STRONG&gt;manually&lt;/STRONG&gt;&lt;/EM&gt; selecting the device as I think there is some error in the handling of the SDIDs for aliased devices which was introduced in the latest version. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would have thought that a pull-up of 10K would be fine for the BKGD signal.&amp;nbsp; I'm surprised that a change to 2K would be necessary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Sep 2014 07:44:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329742#M2852</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-09-23T07:44:38Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to program MC9S08PT60 using USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329743#M2853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to use the manual selection of MCU, it seems not work as well. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Shucheng Zhu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Sep 2014 02:17:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Fail-to-program-MC9S08PT60-using-USBDM/m-p/329743#M2853</guid>
      <dc:creator>shuchengzhu</dc:creator>
      <dc:date>2014-09-29T02:17:20Z</dc:date>
    </item>
  </channel>
</rss>