<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックRe: Re: Re: USBDM can´t program PA16</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-can-t-program-PA16/m-p/325002#M2807</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tested and it works perfectly!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you pgo !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Jul 2014 14:33:02 GMT</pubDate>
    <dc:creator>lucianonicolau</dc:creator>
    <dc:date>2014-07-28T14:33:02Z</dc:date>
    <item>
      <title>USBDM can´t program PA16</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-can-t-program-PA16/m-p/324998#M2803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using 4.10.6.140 I have MC9S08PA16 on my board and it only can be programmed if selected as PT16.&lt;/P&gt;&lt;P&gt;If selected the right device "PA16" it cause this error:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="usbdm_problem.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45286i1B9634919FD4F77F/image-size/large?v=v2&amp;amp;px=999" role="button" title="usbdm_problem.jpg" alt="usbdm_problem.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Tell me how to fix it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jul 2014 13:23:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-can-t-program-PA16/m-p/324998#M2803</guid>
      <dc:creator>lucianonicolau</dc:creator>
      <dc:date>2014-07-25T13:23:21Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM can´t program PA16</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-can-t-program-PA16/m-p/324999#M2804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Luciano,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've attached an updated &lt;STRONG&gt;hcs08_devices.xml&lt;/STRONG&gt; file.&amp;nbsp; Can you replace this file in the USBDM installation and check if it works correctly with your devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Place in directory &lt;STRONG&gt;&lt;EM&gt;C:\Program Files (x86)\pgo\USBDM 4.10.6.170\DeviceData&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this doesn't work correctly could you provide the ID number that the programmer detects?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Jul 2014 07:00:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-can-t-program-PA16/m-p/324999#M2804</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-07-26T07:00:10Z</dc:date>
    </item>
    <item>
      <title>Re: Re: USBDM can´t program PA16</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-can-t-program-PA16/m-p/325000#M2805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First test it stop working for PT16 too, then I changed the SDID and it works fine!&lt;/P&gt;&lt;P&gt;The SDID for PA8 and PA16 is 1042 (tested for both), I edited your new hcs_device.xml, now it can detect chip for PA8 and PA16.&lt;/P&gt;&lt;P&gt;See file attached with new SDIDs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you have time, please, insert my website on USBDM website as manufacturer: &lt;A href="http://www.usbdm.com.br/"&gt;www.usbdm.com.br&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks a lot,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jul 2014 12:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-can-t-program-PA16/m-p/325000#M2805</guid>
      <dc:creator>lucianonicolau</dc:creator>
      <dc:date>2014-07-28T12:39:25Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Re: USBDM can´t program PA16</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-can-t-program-PA16/m-p/325001#M2806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Luciano,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The manual for the chip indicates that the SDID is 0x0042 so it looks like the first digit is the mask revision.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've changed the SDIDmask in the attached file which should have the same effect as the changes you made but also work with the version given in the manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would appreciate it you could test this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have previously added your site to the list on:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://usbdm.sourceforge.net/" title="http://usbdm.sourceforge.net/"&gt;http://usbdm.sourceforge.net/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jul 2014 13:51:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-can-t-program-PA16/m-p/325001#M2806</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-07-28T13:51:35Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Re: USBDM can´t program PA16</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-can-t-program-PA16/m-p/325002#M2807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tested and it works perfectly!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you pgo !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jul 2014 14:33:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-can-t-program-PA16/m-p/325002#M2807</guid>
      <dc:creator>lucianonicolau</dc:creator>
      <dc:date>2014-07-28T14:33:02Z</dc:date>
    </item>
  </channel>
</rss>