<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem USB BDM (HCS08/HCS12/CFV1) with MCF51EM in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Problem-USB-BDM-HCS08-HCS12-CFV1-with-MCF51EM/m-p/257585#M2552</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sezgin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately the only guaranteed way to get a a MCF51 into BKGD mode is through a power-cycle with the BKGD pin low.&amp;nbsp; This is described in the device manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Often it is not necessary - but in many cases for&amp;nbsp; blank device it will be.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is independent of the programmer used.&amp;nbsp; Some programmers provide the ability to cycle the power when required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 May 2013 12:26:18 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2013-05-27T12:26:18Z</dc:date>
    <item>
      <title>Problem USB BDM (HCS08/HCS12/CFV1) with MCF51EM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Problem-USB-BDM-HCS08-HCS12-CFV1-with-MCF51EM/m-p/257584#M2551</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with programming the CFV1 Controller MCF51EM. In my testapplication for programming the controller in our production a new or unprogrammend controller needs an Power down/off of the controller. As this is not realised in the testapplication I want to ask if someone know if there is a posibility in the settings to solve this that no power down/off is needed?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119420i3CA730F9141D3E77/image-size/large?v=v2&amp;amp;px=999" title="PROGCFZ1_1.JPG" alt="PROGCFZ1_1.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best regard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sezgin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2013 07:39:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Problem-USB-BDM-HCS08-HCS12-CFV1-with-MCF51EM/m-p/257584#M2551</guid>
      <dc:creator>Montelo</dc:creator>
      <dc:date>2013-05-27T07:39:44Z</dc:date>
    </item>
    <item>
      <title>Re: Problem USB BDM (HCS08/HCS12/CFV1) with MCF51EM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Problem-USB-BDM-HCS08-HCS12-CFV1-with-MCF51EM/m-p/257585#M2552</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sezgin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately the only guaranteed way to get a a MCF51 into BKGD mode is through a power-cycle with the BKGD pin low.&amp;nbsp; This is described in the device manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Often it is not necessary - but in many cases for&amp;nbsp; blank device it will be.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is independent of the programmer used.&amp;nbsp; Some programmers provide the ability to cycle the power when required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2013 12:26:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Problem-USB-BDM-HCS08-HCS12-CFV1-with-MCF51EM/m-p/257585#M2552</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2013-05-27T12:26:18Z</dc:date>
    </item>
  </channel>
</rss>