<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HCS08 Programmer security setting issue in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/HCS08-Programmer-security-setting-issue/m-p/238924#M2474</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Antonie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have just done some tests under windows and it doesn't have any problems that I can see.&amp;nbsp; I will have a look at Ubuntu eventually but at the moment I don't have a stable build to test with.&amp;nbsp; It may be some kind of timing issue.&amp;nbsp; The USB on Linux is considerably faster than Windows on some things.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this problem occur with any test file e.g. an empty file or only with a specific file.&amp;nbsp; I would appreciate if you could re-test with the two example test files please.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also which specific USBDM hardware are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Update&lt;/P&gt;&lt;P&gt;-------------------&lt;/P&gt;&lt;P&gt;Tried the attached files with Mint Linux 32 &amp;amp; 64-bit (which is a Ubuntu derivative) and they both programmed multiple times without problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 01 Feb 2014 03:59:35 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2014-02-01T03:59:35Z</dc:date>
    <item>
      <title>HCS08 Programmer security setting issue</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/HCS08-Programmer-security-setting-issue/m-p/238923#M2473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Firstly, thank you very much for the tool, it is great. I have noticed an issue running on Ubuntu 13.10 64bit. Running the HCS08 Flash Programmer (4.6.10) and programming a&amp;nbsp; MC9S08GT16A, i can program the device multiple times using "Image" Security setting, but as soon as I select either "Secure", "Unsecure" or "Smart", I can only program the device once. The next time, the programming will succeed, but it appears as though the device never comes out of reset. It just hangs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2014 11:30:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/HCS08-Programmer-security-setting-issue/m-p/238923#M2473</guid>
      <dc:creator>tonesrsa</dc:creator>
      <dc:date>2014-01-16T11:30:47Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 Programmer security setting issue</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/HCS08-Programmer-security-setting-issue/m-p/238924#M2474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Antonie,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have just done some tests under windows and it doesn't have any problems that I can see.&amp;nbsp; I will have a look at Ubuntu eventually but at the moment I don't have a stable build to test with.&amp;nbsp; It may be some kind of timing issue.&amp;nbsp; The USB on Linux is considerably faster than Windows on some things.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this problem occur with any test file e.g. an empty file or only with a specific file.&amp;nbsp; I would appreciate if you could re-test with the two example test files please.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also which specific USBDM hardware are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Update&lt;/P&gt;&lt;P&gt;-------------------&lt;/P&gt;&lt;P&gt;Tried the attached files with Mint Linux 32 &amp;amp; 64-bit (which is a Ubuntu derivative) and they both programmed multiple times without problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Feb 2014 03:59:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/HCS08-Programmer-security-setting-issue/m-p/238924#M2474</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-02-01T03:59:35Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 Programmer security setting issue</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/HCS08-Programmer-security-setting-issue/m-p/238925#M2475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the late reply. I only got around today to test your images. In the process I have discovered that it only ever happens with a special image that we create to be flashed, which combines a two binaries. The issue probably stems from our custom file. A normal .s19 file as compiled from a Codewarrior project does not seem to do this, so for now it is not a major problem for us. We use the USBDM-JM60-SER-0001, firmware version V4.9.5, DLL Ver 4.10.6.0&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2014 14:27:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/HCS08-Programmer-security-setting-issue/m-p/238925#M2475</guid>
      <dc:creator>tonesrsa</dc:creator>
      <dc:date>2014-02-17T14:27:49Z</dc:date>
    </item>
  </channel>
</rss>