<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USBDM HCS12_FlashProgrammer in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-HCS12-FlashProgrammer/m-p/223270#M2345</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;nice tools pgo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've got a special usage where I only need to issue a 'run', wait a couple of sec, then a 'halt'&lt;/P&gt;&lt;P&gt;to a HCS12.&amp;nbsp; it looks like it would be pretty simple to add to the CLI interface of&lt;/P&gt;&lt;P&gt;HCS12_flashprogrammer (unless there's a better way to do that or some other utility,&lt;/P&gt;&lt;P&gt;opensource or not).&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't use the entire codewarrior package in this environment to do this function and&lt;/P&gt;&lt;P&gt;would be happy to make the modifications myself if the source is available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for considering&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Jan 2014 01:12:42 GMT</pubDate>
    <dc:creator>vette</dc:creator>
    <dc:date>2014-01-09T01:12:42Z</dc:date>
    <item>
      <title>USBDM HCS12_FlashProgrammer</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-HCS12-FlashProgrammer/m-p/223270#M2345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;nice tools pgo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've got a special usage where I only need to issue a 'run', wait a couple of sec, then a 'halt'&lt;/P&gt;&lt;P&gt;to a HCS12.&amp;nbsp; it looks like it would be pretty simple to add to the CLI interface of&lt;/P&gt;&lt;P&gt;HCS12_flashprogrammer (unless there's a better way to do that or some other utility,&lt;/P&gt;&lt;P&gt;opensource or not).&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't use the entire codewarrior package in this environment to do this function and&lt;/P&gt;&lt;P&gt;would be happy to make the modifications myself if the source is available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for considering&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jan 2014 01:12:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-HCS12-FlashProgrammer/m-p/223270#M2345</guid>
      <dc:creator>vette</dc:creator>
      <dc:date>2014-01-09T01:12:42Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM HCS12_FlashProgrammer</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-HCS12-FlashProgrammer/m-p/223271#M2346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi vette,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It you don't need top program the target then you could look at the USBDM API example program as a starting point for writing a simple program to do what you need..&amp;nbsp; It shows simple usage&amp;nbsp; of the USBDM interface DLL to interact with a target,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See:&lt;/P&gt;&lt;P&gt;&lt;A href="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_JS16/html/usbdm_programming.html" title="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_JS16/html/usbdm_programming.html"&gt;USBDM: Programming with the USBDM API&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jan 2014 00:37:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-HCS12-FlashProgrammer/m-p/223271#M2346</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2014-01-11T00:37:06Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM HCS12_FlashProgrammer</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-HCS12-FlashProgrammer/m-p/223272#M2347</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;wow, I guess I really should have clicked on that related pages tab.&amp;nbsp; will give it a go, thx pgo!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 11 Jan 2014 20:29:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-HCS12-FlashProgrammer/m-p/223272#M2347</guid>
      <dc:creator>vette</dc:creator>
      <dc:date>2014-01-11T20:29:29Z</dc:date>
    </item>
  </channel>
</rss>