<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Code Warrior in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217342#M2256</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Grant,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you install the USBDM software then you would be able to program target micros using the utilities included.&amp;nbsp; This does not require Codewarrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Programming a completely blank JS16 micro (on a USBDM) is possible using the JS16 bootloader included in the USBDM software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It&amp;nbsp; would be difficult to build a BDM cheaper than buying the Wytec one I would think?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Dec 2012 15:36:57 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2012-12-26T15:36:57Z</dc:date>
    <item>
      <title>Code Warrior</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217341#M2255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking at perhaps getting the Wytec USBDM which already comes with V4.9 firmware installed according to the web page. If I want to use this purely for loading StickOS onto a MCF51JM128EVLK, do I need Code Warrior or can I get away without it? I won't be doing anything other than loading StickOS, so presumably I won't need to compile anything, as StickOS already has the Hex files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I decided to make my own USBDM JS16 minimal MC9S08JS16CWJ.(for use with the above processor) instead of buying one, would I need Code Warrior to load the firmware into the USBDM?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Dec 2012 02:10:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217341#M2255</guid>
      <dc:creator>grantm</dc:creator>
      <dc:date>2012-12-26T02:10:07Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217342#M2256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Grant,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you install the USBDM software then you would be able to program target micros using the utilities included.&amp;nbsp; This does not require Codewarrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Programming a completely blank JS16 micro (on a USBDM) is possible using the JS16 bootloader included in the USBDM software.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It&amp;nbsp; would be difficult to build a BDM cheaper than buying the Wytec one I would think?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Dec 2012 15:36:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217342#M2256</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2012-12-26T15:36:57Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217343#M2257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the fast response PGO, especially over the Christmas period. That sounds good that I can use the USBDM software. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes the Wytec is very cheap, though postage is likely the killer to get it around the other side of the globe - plus a 3-4 week wait. I already have all the bits handy in through-hole form, except the micro (have an SMD-DIP adaptor to suit) and 74LV125 which can be obtained in DIP, so still tossing it around. I assume I can use 74ACT125 etc. so long as Target is always 5V like MCF51JM128EVLK?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for sharing your work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Dec 2012 17:47:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217343#M2257</guid>
      <dc:creator>grantm</dc:creator>
      <dc:date>2012-12-26T17:47:30Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217344#M2258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Grant,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are correct about the 74ACT125 or similar - providing you are using 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Dec 2012 03:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217344#M2258</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2012-12-27T03:28:17Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217345#M2259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does the BL pin have to be pulled low to initially load program the BDM chip? I'm not quite clear on this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Feb 2013 08:30:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217345#M2259</guid>
      <dc:creator>grantm</dc:creator>
      <dc:date>2013-02-22T08:30:55Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217346#M2260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi grant,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For a JS16 chip I presume?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To load the initial software you hold BL low while plugging in the BDM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To update the firmware this is not necessary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_JS16/html/construction_page.html" title="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_JS16/html/construction_page.html"&gt;USBDM: BDM Construction and Firmware&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Mar 2013 02:38:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217346#M2260</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2013-03-01T02:38:48Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217347#M2261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks pgo, you've been really helpful, I'll have to RTFM a bit better I think!&lt;/P&gt;&lt;P&gt;Yes a JS16&amp;nbsp; :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Mar 2013 11:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Code-Warrior/m-p/217347#M2261</guid>
      <dc:creator>grantm</dc:creator>
      <dc:date>2013-03-01T11:04:00Z</dc:date>
    </item>
  </channel>
</rss>