<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックRe: USBDM - Version 4.7 (JB16/JS16/JMxx Hardware Versions)</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213411#M2156</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;pgo wrote:&lt;BR /&gt;&lt;P&gt;Dear Bill,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've done some simple tests with Codewarrior Eclipse &amp;amp; Legacy but I've been unable to get it to misbehave in the fashion indicated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would expect the Serial port to lose characters occasionally as there is no flow control and the buffers are very modest (16 bytes!).&amp;nbsp; This is affected by some small portions of code that need to run with interrupts disabled.&amp;nbsp; In the present case this might be occurring when the BDM is trying to connect, but this is a guess.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does the problem occur if the serial port is not being used?&amp;nbsp; I suspect its unrelated to the serial port use but it would be useful to check.&lt;/P&gt;&lt;P&gt;If you can provide a small testcase it would be good but as yout said problems like this are hard to reproduce.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I will try to rig it w/o the serial port and see what happens.&lt;/P&gt;&lt;P&gt;It is very random and infrequent.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 14 Nov 2011 21:06:31 GMT</pubDate>
    <dc:creator>wrljet</dc:creator>
    <dc:date>2011-11-14T21:06:31Z</dc:date>
    <item>
      <title>USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213311#M2056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;USBDM has been updated to V4.6.&amp;nbsp; This version adds support for Kinetis devices but please be aware that this has had minimal testing due to lack of devices to test with &lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" id="smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please post any queries on this version in this thread,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Information available at:&amp;nbsp; &lt;A href="http://usbdm.sourceforge.net/" rel="nofollow" target="_blank"&gt;http://usbdm.sourceforge.net/&lt;/A&gt;﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Notes&lt;/P&gt;&lt;P&gt;Please note that these design are different from the &lt;STRONG&gt;Freescale OSBDM-JM60&lt;/STRONG&gt; design which was proceeding independently while I was doing the above designs&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;V4.6 (June 2011) -&lt;UL&gt;&lt;LI&gt;Support for Kinetis Targets in Codewarrior V10.1 (Eclipse, USBDM/CF only)&lt;/LI&gt;&lt;LI&gt;Added Kinetis programmer (and CFVx but only two devices!)&lt;/LI&gt;&lt;LI&gt;Improvements to USB error checking (JMxx/JS16 only)&lt;/LI&gt;&lt;LI&gt;TCL scripting&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;V4.5 (February 2011) -&lt;UL&gt;&lt;LI&gt;Support for Codesourcery Lite - Coldfire Vx&lt;/LI&gt;&lt;LI&gt;Support for Coldfire Flasher (CFFlasher) Coldfire V2,3,4 only&lt;/LI&gt;&lt;LI&gt;Support for Codewarrior Eclipse 10.1&lt;/LI&gt;&lt;LI&gt;Flash buffer is now dynamically sized in Flash programmers&lt;/LI&gt;&lt;LI&gt;Added fix for Legacy Codewarrior tools missing TBDML/OSBDM targets&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;V4.4 (January 2011) -&lt;UL&gt;&lt;LI&gt;Less intrusive auto speed detection for targets without sync&lt;/LI&gt;&lt;LI&gt;Unlocking improved for targets using slow external clocks&lt;/LI&gt;&lt;LI&gt;Codewarrior V10 New Project Wizard now includes USBDM&lt;/LI&gt;&lt;LI&gt;Programming support for HCS12/HCS08 targets with EEPROM&lt;/LI&gt;&lt;LI&gt;Programming support for CFV1 target with multiple Flash (Dual Flash)&lt;/LI&gt;&lt;LI&gt;Use of XML based device files (needed for above two items)&lt;/LI&gt;&lt;LI&gt;Automatic unsecure for Legacy HCS12 targets&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;V4.3 (December 2010) -&lt;UL&gt;&lt;LI&gt;Bug fixes (DSC Speed)&lt;/LI&gt;&lt;LI&gt;Improved Codewarrior V10 integration&lt;/LI&gt;&lt;LI&gt;Serial interface on JS16 versions (supported in JMxx but no example implementation)&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;V4.0 (September 2010) - &lt;STRONG&gt;Significant changes in some areas - Please read carefully&lt;/STRONG&gt;&lt;UL&gt;&lt;LI&gt;Support for Linux (Eclipse version of Codewarrior only)&lt;BR /&gt;Installation is still somewhat of a challenge!&lt;/LI&gt;&lt;LI&gt;Support for Linux and Windows7 64-bit (Eclipse version of Codewarrior only)&lt;BR /&gt;To support the 64-bit version of Windows it has been necessary to update to using libusb-V1 drivers. For consistency this is also done on Linux. As part of this process the VID/PID for the hardware (BDM) has been changed. This will allow the co-existence of Freescale's OSBDM-JM60 hardware while using a new driver for USBDM. Formerly both these BDMs used the same VID/PID and changes to the driver would not be possible.&lt;/LI&gt;&lt;LI&gt;Programming utilities for RS08, HCS08 and CFV1 are now (officially) included.&lt;/LI&gt;&lt;LI&gt;Support for MC56F800x (digital signal controllers) added. This is only available on USBDM_CF BDMs and the Axiom MC56F8006 Demoboard.&lt;/LI&gt;&lt;LI&gt;Minor bug fixes (installation script)&lt;/LI&gt;&lt;LI&gt;The addition of DSC support has pushed the firmware size to greater than 16K on the USBDM_JMxx-CF version. This means that MC9S08JM32/60 chip must be used.&lt;/LI&gt;&lt;LI&gt;Changed to wxWidgets for common GUI code on Windows and Linux&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;V4.6 (June 2011) -&lt;UL&gt;&lt;LI&gt;Support for Kinetis Targets in Codewarrior V10.1 (Eclipse, USBDM/CF only)&lt;/LI&gt;&lt;LI&gt;Improvements to USB error checking (JMxx/JS16 only)&lt;/LI&gt;&lt;LI&gt;TCL scripting&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;V4.5 (February 2011) -&lt;UL&gt;&lt;LI&gt;Support for Codesourcery Lite - Coldfire Vx&lt;/LI&gt;&lt;LI&gt;Support for Coldfire Flasher (CFFlasher) Coldfire V2,3,4 only&lt;/LI&gt;&lt;LI&gt;Support for Codewarrior Eclipse 10.1&lt;/LI&gt;&lt;LI&gt;Flash buffer is now dynamically sized in Flash programmers&lt;/LI&gt;&lt;LI&gt;Added fix for Legacy Codewarrior tools missing TBDML/OSBDM targets&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;V4.4 (January 2011) -&lt;UL&gt;&lt;LI&gt;Less intrusive auto speed detection for targets without sync&lt;/LI&gt;&lt;LI&gt;Unlocking improved for targets using slow external clocks&lt;/LI&gt;&lt;LI&gt;Codewarrior V10 New Project Wizard now includes USBDM&lt;/LI&gt;&lt;LI&gt;Programming support for HCS12/HCS08 targets with EEPROM&lt;/LI&gt;&lt;LI&gt;Programming support for CFV1 target with multiple Flash (Dual Flash)&lt;/LI&gt;&lt;LI&gt;Use of XML based device files (needed for above two items)&lt;/LI&gt;&lt;LI&gt;Automatic unsecure for Legacy HCS12 targets&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;V4.3 (December 2010) -&lt;UL&gt;&lt;LI&gt;Bug fixes (DSC Speed)&lt;/LI&gt;&lt;LI&gt;Improved Codewarrior V10 integration&lt;/LI&gt;&lt;LI&gt;Serial interface on JS16 versions (supported in JMxx but no example implementation)&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;V4.0 (September 2010) - &lt;STRONG&gt;Significant changes in some areas - Please read carefully&lt;/STRONG&gt;&lt;UL&gt;&lt;LI&gt;Support for Linux (Eclipse version of Codewarrior only)&lt;BR /&gt;Installation is still somewhat of a challenge!&lt;/LI&gt;&lt;LI&gt;Support for Linux and Windows7 64-bit (Eclipse version of Codewarrior only)&lt;BR /&gt;To support the 64-bit version of Windows it has been necessary to update to using libusb-V1 drivers. For consistency this is also done on Linux. As part of this process the VID/PID for the hardware (BDM) has been changed. This will allow the co-existence of Freescale's OSBDM-JM60 hardware while using a new driver for USBDM. Formerly both these BDMs used the same VID/PID and changes to the driver would not be possible.&lt;/LI&gt;&lt;LI&gt;Programming utilities for RS08, HCS08 and CFV1 are now (officially) included.&lt;/LI&gt;&lt;LI&gt;Support for MC56F800x (digital signal controllers) added. This is only available on USBDM_CF BDMs and the Axiom MC56F8006 Demoboard.&lt;/LI&gt;&lt;LI&gt;Minor bug fixes (installation script)&lt;/LI&gt;&lt;LI&gt;The addition of DSC support has pushed the firmware size to greater than 16K on the USBDM_JMxx-CF version. This means that MC9S08JM32/60 chip must be used.&lt;/LI&gt;&lt;LI&gt;Changed to wxWidgets for common GUI code on Windows and Linux&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;﻿&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jun 2011 10:54:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213311#M2056</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2011-06-07T10:54:25Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213312#M2057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!!!, Thanks for the help for use Freescale﻿&amp;nbsp;microcontroller.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I like know about a guide for the installation or step to step for installing﻿.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank for you help!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jun 2011 21:38:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213312#M2057</guid>
      <dc:creator>Vncnt</dc:creator>
      <dc:date>2011-06-08T21:38:26Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213313#M2058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First of all I'd like to thank you for the great work on USBDM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I managed to get USBDM 4.5 working on an ubuntu&amp;nbsp;8.04﻿&amp;nbsp; (32-bit) by remanimg a few of the dlls.&lt;/P&gt;&lt;P&gt;The same 4.5 failed to install on a debian stable 64-bit.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was not able to install V4.6 in either of the system mentioned above.&lt;/P&gt;&lt;P&gt;Both ubuntu 32-bit and debian 64-bit are missing several libraries (or have an incompatible version),&lt;/P&gt;&lt;P&gt;I believe most of the problem can be easily solved by recompiling the software on the target machine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I downloaded the source distribution but I cannot figure out how to build it.&lt;/P&gt;&lt;P&gt;Do you have any documentation?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2011 13:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213313#M2058</guid>
      <dc:creator>ggorlik</dc:creator>
      <dc:date>2011-07-07T13:41:29Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213314#M2059</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Gorlick,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The source code for the libraries etc are an export of the projects from Eclipse.&amp;nbsp; It's not set up for a stand-alone make mainly because I have no idea how to do it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You should be able to import them into an Eclipse installation to re-create the projects.&amp;nbsp; The build targets and settings are part of the Eclipse projects.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2011 18:14:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213314#M2059</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2011-07-07T18:14:36Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213315#M2060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks for your reply.&lt;/P&gt;&lt;P&gt;I tried to import the project using the archive importer and a few other ways without success.&lt;/P&gt;&lt;P&gt;Regardless of how I try to do the import I can't find a way to create a native build (i.e. not a microcontroller)&lt;BR /&gt;﻿I am sure it's my fault (I really don't understand how eclipse projects work).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you using CW eclipse or a different flavor?&lt;/P&gt;&lt;P&gt;Could you give me a few more hints?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks again,&lt;/P&gt;&lt;P&gt;GG&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jul 2011 01:59:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213315#M2060</guid>
      <dc:creator>ggorlik</dc:creator>
      <dc:date>2011-07-09T01:59:33Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213316#M2061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can at least partly answer that one. If it is a native build, it is not CW eclipse, it is Eclipse CDT.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jul 2011 02:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213316#M2061</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2011-07-09T02:02:15Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213317#M2062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear gorlick,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Wot Jim said!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry I was unclear.&amp;nbsp; The Libraries etc are built using a standard Eclipse CDT (C development)&amp;nbsp; version of Eclipse downloaded from &lt;A href="http://www.eclipse.org/cdt/" rel="nofollow" target="_blank"&gt;http://www.eclipse.org/cdt/&lt;/A&gt;﻿.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You may also need:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Tcl/Tk - &lt;A href="http://www.tcl.tk/software/tcltk/8.5.html" rel="nofollow" target="_blank"&gt;http://www.tcl.tk/software/tcltk/8.5.html&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;WxWidgets Cross Platform Library has been used for the GUI - &lt;A href="http://www.wxwidgets.org/" rel="nofollow" target="_blank"&gt;http://www.wxwidgets.org/&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;Xerces XML parser - &lt;A href="http://xerces.apache.org/xerces-c" rel="nofollow" target="_blank"&gt;http://xerces.apache.org/xerces-c&lt;/A&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;﻿&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Jul 2011 07:25:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213317#M2062</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2011-07-09T07:25:43Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213318#M2063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Jim and pgo!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With your help and some project settings change I managed to build a 64-b version of the V4.5 shared library and the GDI.&lt;/P&gt;&lt;P&gt;I am still having some issues with the standalone flasher and the CW plugins though.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was able to build the flasher with a hand made makefile.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'll keep you updated on the progress&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks again&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Jul 2011 07:47:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213318#M2063</guid>
      <dc:creator>ggorlik</dc:creator>
      <dc:date>2011-07-16T07:47:01Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213319#M2064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi pgo!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to program MC13213 with standalone programmer "HCS08_FlashProgrammer.exe" with JS16 hardware and v.4.6.&lt;/P&gt;&lt;P&gt;This is not possible.&lt;/P&gt;&lt;P&gt;I got "Programming Error: Programming of target flash failed! Reason: Failed to read from target"&lt;/P&gt;&lt;P&gt;In&amp;nbsp;this time programming with HiWave and same hardware&amp;nbsp;is without problems.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After I downgrade to the version 4.5 All is OK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have any idea about this situation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And another question: It is possible to read flash and save S19 file with standalone programmer&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;10x for great work on USBDM.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bendjy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jul 2011 16:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213319#M2064</guid>
      <dc:creator>bendjy</dc:creator>
      <dc:date>2011-07-19T16:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213320#M2065</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Benjy,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried programming a small project to a MC13213 chip using a JS16 USBDM (V4.6) and didn't have any problems.&amp;nbsp; If it's working OK with V4.5 for you then stick with that for the moment.&amp;nbsp; I would you appreciate checking again when the next version is available and letting know if the problem persists and I will spend more time investigating it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jul 2011 13:11:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213320#M2065</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2011-07-22T13:11:54Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213321#M2066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear PGO,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a couple of USBDM and I changed recently of computer. Now, I have an Windows 7 (home edition) - 64 bits AMD Phenom II PC. Previously, I had a Win XP 32 bits computer.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have USBDM with the 4.5 and 4.6 version, and I have the following problems with Windows&amp;nbsp; 7:&lt;/P&gt;&lt;P&gt;- Both Bootloader.exe&amp;nbsp; versions (4.5 and 4.6) fail to run.&lt;/P&gt;&lt;P&gt;- The CFV1_FlashProgrammer version 4.5 runs OK, but the CFV1_FlashProgrammer﻿ version 4.6 fails (see figure attached)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I carefully avoided to mix the dll of different versions and ran the programmes with the following compatibility options : "run in XP SP3 mode" and "Run as Administrator".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use CodeSourcery&amp;nbsp; for CFV1 and both versions and dll runs OK.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Do you have an idea what is going wrong?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thierry&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 24 Jul 2011 19:21:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213321#M2066</guid>
      <dc:creator>thm59</dc:creator>
      <dc:date>2011-07-24T19:21:27Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213322#M2067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I finally managed to compile everything (except the java stuff which still does not compile properly) on debian.&lt;/P&gt;&lt;P&gt;I can run the standalone flashers without any issues.&lt;/P&gt;&lt;P&gt;CW still refuses to work though. When I attempt to launch I get a generic error without any explanation.&lt;/P&gt;&lt;P&gt;How do I debug what is wrong?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I run ldd on the gdi.so to make sure there are no issues with the shared libraries but beside that I really have no idea what ewlse to try.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2011 05:02:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213322#M2067</guid>
      <dc:creator>ggorlik</dc:creator>
      <dc:date>2011-07-28T05:02:00Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213323#M2068</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Thierry,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bit much idea really.&amp;nbsp; The Codewarrior DLLs and the corresponding standalone programmers both use the same code for programming so I would expect errors in both or neither!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Bootloader poses some special issues since it involves 'suprise'&amp;nbsp; USB removals when changing between modes which does seem to upset some computers.&amp;nbsp; I don't see how I can investigate this as I didn't have real problems with Windows 64-bit on intel boxes and possibly the problems is with the AMD machines (or the non-intel USB interfaces).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Incidently, when you say "fails to run" do you mean the programs don't execute at all, crash or don't function correctly?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Aug 2011 16:50:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213323#M2068</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2011-08-01T16:50:51Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213324#M2069</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Gorlik,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm not sure how you can run the GDI part without having the Java plugin working - or are you using the supplied versions?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you compile the DLLs with logging enabled you should have messages from when the DLL is loaded.&amp;nbsp; If the loading is failing check the exported symbols from the GDI DLLs to see if&amp;nbsp; they are correct against the provided DLLs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Aug 2011 16:55:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213324#M2069</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2011-08-01T16:55:40Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213325#M2070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, PGO&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It seems that my problem is similar to the one mentionned by BENDJY (page 1 of this post).&lt;BR /&gt;&lt;BR /&gt;Regarding the problem of the bootloader, attached the error message.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In both cases, it seems that the programming problem occurs just before the verifying phase.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thierry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Aug 2011 21:24:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213325#M2070</guid>
      <dc:creator>thm59</dc:creator>
      <dc:date>2011-08-03T21:24:10Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213326#M2071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the JM60 version.&amp;nbsp; I updated today from 4.3 to 4.6.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now the "Leave target powered on exit" seems to no longer work.&lt;/P&gt;&lt;P&gt;When I exit the debugger, the USBDM turns off power to my target board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Aug 2011 04:42:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213326#M2071</guid>
      <dc:creator>wrljet</dc:creator>
      <dc:date>2011-08-06T04:42:04Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213327#M2072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello PGO,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I just tried your version 4.6 with Codewarrior 10.1 on a clean install of Ubuntu 11.04 (32 bit).&lt;/P&gt;&lt;P&gt;In case it helps anyone else trying this, it required adding the following libraries with the Synaptic Package Manager:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;tcl8.5&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;libwxgtk2.8-0&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;libwxgtk2.8-dbg&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;libstdc++5&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;libxerces-c3.1﻿&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then it seems to run fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks and best regards!&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Aug 2011 13:11:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213327#M2072</guid>
      <dc:creator>joncas</dc:creator>
      <dc:date>2011-08-06T13:11:12Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213328#M2073</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE&gt;I reran with the 4.6 Debug build.&amp;nbsp; The log file is attached.&amp;nbsp; (I snipped out the bulk of the middle)&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;It shows intentionally turning off the target power at the end.&amp;nbsp; I looked at that part of the code and it doesn't appear to be sensitive to &amp;nbsp;bdmOptions.leaveTargetPowered﻿. &amp;nbsp;&lt;/BLOCKQUOTE&gt;&lt;BLOCKQUOTE&gt;&lt;HR /&gt;&lt;BLOCKQUOTE&gt;wrljet wrote:&lt;/BLOCKQUOTE&gt;&lt;P&gt;I'm using the JM60 version.&amp;nbsp; I updated today from 4.3 to 4.6.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now the "Leave target powered on exit" seems to no longer work.&lt;/P&gt;&lt;P&gt;When I exit the debugger, the USBDM turns off power to my target board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Aug 2011 21:49:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213328#M2073</guid>
      <dc:creator>wrljet</dc:creator>
      <dc:date>2011-08-06T21:49:16Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213329#M2074</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Bill,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The leave target power on option is broken in 4.6 (as you realise).&amp;nbsp; It's a know bug and is fixed in my current working version and so should re-appear in the next version.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It came about in that the Vdd control is now done by the USBDM.dll on the PC rather than by the BDM only.&amp;nbsp; This allows better control when doing power-on resets etc.&amp;nbsp; The less target-specific code in the BDM the better.&amp;nbsp; I overlooked this option when doing the changes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Aug 2011 12:01:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213329#M2074</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2011-08-07T12:01:28Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM - Version 4.6 (JB16/JS16/JMxx Hardware Versions)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213330#M2075</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the update. I didn't realize Leave Power was a known issue in 4.6, and was just trying to help track&lt;/P&gt;&lt;P&gt;it down.&amp;nbsp;&amp;nbsp; Is there a place with an active list of known bugs?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the connection/optons dialog, Use Reset option is described in the doc:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;lt;&amp;lt;&amp;lt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Use RESET signal -&lt;/STRONG&gt; Many of the target microcontrollers do not have a dedicated reset signal. This is not a problem as it is possible to reset the target using the BKGD mode commands through the BDM interface. However, the RESET signal on the BDM interface will often still be connected to the Reset signal of the processor. This option allows the BDM to monitor and control the RESET signal when appropriate.&lt;BR /&gt;﻿&amp;gt;&amp;gt;&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you explain that a bit more?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bill&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Aug 2011 21:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-Version-4-6-JB16-JS16-JMxx-Hardware-Versions/m-p/213330#M2075</guid>
      <dc:creator>wrljet</dc:creator>
      <dc:date>2011-08-07T21:38:24Z</dc:date>
    </item>
  </channel>
</rss>