<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDML中的主题 Port to different processor</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Port-to-different-processor/m-p/212571#M2052</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the not too distant future I want to be able to create projects using the Kinetis line of processors.&amp;nbsp; This means that I will need to build a new BDM as the first one I built lacks the requisite connector.&amp;nbsp; I wondered if, while I'm at it, I would port the BDM processor to, say, the MCF51JM60(pin compatible) and replace the USB stack with one of the freebie stacks from Freescale.&amp;nbsp; I wondered, however, if that is really a good choice since the SPI on the V1 processors supports only 8 bit transfers and it seems 9 bit would be better.&amp;nbsp; BUT, all the V2 processors seem to have only 1 SPI and the BDM appears to need 2.&amp;nbsp; Is there a Coldfire processor that has 2 SPI with variable data format that I didn't see?&amp;nbsp; Is the whole concept really worth the trouble?&amp;nbsp; Thanks for the feedback.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 04 Mar 2012 22:30:31 GMT</pubDate>
    <dc:creator>leb</dc:creator>
    <dc:date>2012-03-04T22:30:31Z</dc:date>
    <item>
      <title>Port to different processor</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Port-to-different-processor/m-p/212571#M2052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the not too distant future I want to be able to create projects using the Kinetis line of processors.&amp;nbsp; This means that I will need to build a new BDM as the first one I built lacks the requisite connector.&amp;nbsp; I wondered if, while I'm at it, I would port the BDM processor to, say, the MCF51JM60(pin compatible) and replace the USB stack with one of the freebie stacks from Freescale.&amp;nbsp; I wondered, however, if that is really a good choice since the SPI on the V1 processors supports only 8 bit transfers and it seems 9 bit would be better.&amp;nbsp; BUT, all the V2 processors seem to have only 1 SPI and the BDM appears to need 2.&amp;nbsp; Is there a Coldfire processor that has 2 SPI with variable data format that I didn't see?&amp;nbsp; Is the whole concept really worth the trouble?&amp;nbsp; Thanks for the feedback.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Mar 2012 22:30:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Port-to-different-processor/m-p/212571#M2052</guid>
      <dc:creator>leb</dc:creator>
      <dc:date>2012-03-04T22:30:31Z</dc:date>
    </item>
  </channel>
</rss>