<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックRe: JS16 OSBDM</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/JS16-OSBDM/m-p/212349#M2051</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Michael,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The connections are correct.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The two pins are used as outputs to control the buffer at different times with the other pin 3-state.&amp;nbsp; Neither is actually used as an input.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This allows for faster manipulation of multiple port pins on a shared port but also allows independent control using a separate pin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Jul 2010 19:02:34 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2010-07-13T19:02:34Z</dc:date>
    <item>
      <title>JS16 OSBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/JS16-OSBDM/m-p/212348#M2050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hallo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;refering to USBDM_SOIC_JS16(Minimal):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it right that BKGD_DRV is connected to input- and output pins on MC9S08JS16CWJ. ﻿﻿BKGD_DRV drives only an input pin on U1B (74LV125AD)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jul 2010 21:03:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/JS16-OSBDM/m-p/212348#M2050</guid>
      <dc:creator>Michael_Theisse</dc:creator>
      <dc:date>2010-07-12T21:03:46Z</dc:date>
    </item>
    <item>
      <title>Re: JS16 OSBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/JS16-OSBDM/m-p/212349#M2051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Michael,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The connections are correct.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The two pins are used as outputs to control the buffer at different times with the other pin 3-state.&amp;nbsp; Neither is actually used as an input.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This allows for faster manipulation of multiple port pins on a shared port but also allows independent control using a separate pin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jul 2010 19:02:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/JS16-OSBDM/m-p/212349#M2051</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2010-07-13T19:02:34Z</dc:date>
    </item>
  </channel>
</rss>