<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックRe: Help Building PC executables (dll and test programs)</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Help-Building-PC-executables-dll-and-test-programs/m-p/210810#M2030</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear osoraku,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The DLL for USBDM were built with eclipse &amp;amp; MINGW.&amp;nbsp;&amp;nbsp; It should be possible to to build them with VC++ but there are some environment variables that should be set for the different targets.&amp;nbsp; This is done as part of the eclipse setup and would be automatically done if the eclipse packages were imported into Eclipse.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Aug 2009 21:08:56 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2009-08-26T21:08:56Z</dc:date>
    <item>
      <title>Help Building PC executables (dll and test programs)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Help-Building-PC-executables-dll-and-test-programs/m-p/210809#M2029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;First, let me offer huge praises to pgo and all other contributers who have done this fantastic work. Thanks so very much!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to build the PC-side programs of USBDM, namely the dll and test program. What do I need for this? I am guessing Eclipse and cygwin ... is this correct? Has anybody built them with VC++? Any advice to help a stranded newbie is much appreciated!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2009 12:19:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Help-Building-PC-executables-dll-and-test-programs/m-p/210809#M2029</guid>
      <dc:creator>osorakunakamori</dc:creator>
      <dc:date>2009-08-26T12:19:39Z</dc:date>
    </item>
    <item>
      <title>Re: Help Building PC executables (dll and test programs)</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Help-Building-PC-executables-dll-and-test-programs/m-p/210810#M2030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear osoraku,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The DLL for USBDM were built with eclipse &amp;amp; MINGW.&amp;nbsp;&amp;nbsp; It should be possible to to build them with VC++ but there are some environment variables that should be set for the different targets.&amp;nbsp; This is done as part of the eclipse setup and would be automatically done if the eclipse packages were imported into Eclipse.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2009 21:08:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Help-Building-PC-executables-dll-and-test-programs/m-p/210810#M2030</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2009-08-26T21:08:56Z</dc:date>
    </item>
  </channel>
</rss>