<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックOSJTAG debugger Hangs up</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/OSJTAG-debugger-Hangs-up/m-p/208045#M1994</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I am using TWR-K60 board for code development and OSJTAG Debugger for debugging&lt;BR /&gt;the code.I am using Keil IDE for software development.&amp;nbsp; I have a working&lt;BR /&gt;version of code and I am adding more functionality to it. Under normal&lt;BR /&gt;circumstances I can load and debug the code.&lt;BR /&gt;&lt;BR /&gt;When I added few more functions to my file and tried to debug the code using&lt;BR /&gt;OSJTAG, the IDE just gets hanged and I am not able to do anything except kill&lt;BR /&gt;the IDE process. I tried to burn the same code to board flash and it runs just&lt;BR /&gt;fine under normal running condition.&lt;BR /&gt;&lt;BR /&gt;Secondly, if I add more functionality to the same file, I am again able to&lt;BR /&gt;debug the code with the section of code (with which i was not able to debug)&lt;BR /&gt;included.&lt;BR /&gt;&lt;BR /&gt;If I disable the newly added code, I am again able to debug using OSJTAG.&lt;BR /&gt;&lt;BR /&gt;I see, my code is working just fine, but some how when I try to debug OSJTAG&lt;BR /&gt;gets hanged (for Flash based or RAM based target project).&lt;BR /&gt;&lt;BR /&gt;I am at a situation where I am not able to debug my code anymore for further&lt;BR /&gt;development.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The OSJTAG version as specified by P&amp;amp;E Micro's Firmware information Utility is "Firmware Build 29".&lt;BR /&gt;&lt;BR /&gt;Is there any code size limit associated with OSJTAG? Is there a bug in OSJTAG?&lt;BR /&gt;What I need to do/take care to avoid this situation?&lt;BR /&gt;&lt;BR /&gt;Warm Regards,&lt;BR /&gt;Dhaval Shah&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 May 2011 11:34:09 GMT</pubDate>
    <dc:creator>d_shah</dc:creator>
    <dc:date>2011-05-21T11:34:09Z</dc:date>
    <item>
      <title>OSJTAG debugger Hangs up</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/OSJTAG-debugger-Hangs-up/m-p/208045#M1994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I am using TWR-K60 board for code development and OSJTAG Debugger for debugging&lt;BR /&gt;the code.I am using Keil IDE for software development.&amp;nbsp; I have a working&lt;BR /&gt;version of code and I am adding more functionality to it. Under normal&lt;BR /&gt;circumstances I can load and debug the code.&lt;BR /&gt;&lt;BR /&gt;When I added few more functions to my file and tried to debug the code using&lt;BR /&gt;OSJTAG, the IDE just gets hanged and I am not able to do anything except kill&lt;BR /&gt;the IDE process. I tried to burn the same code to board flash and it runs just&lt;BR /&gt;fine under normal running condition.&lt;BR /&gt;&lt;BR /&gt;Secondly, if I add more functionality to the same file, I am again able to&lt;BR /&gt;debug the code with the section of code (with which i was not able to debug)&lt;BR /&gt;included.&lt;BR /&gt;&lt;BR /&gt;If I disable the newly added code, I am again able to debug using OSJTAG.&lt;BR /&gt;&lt;BR /&gt;I see, my code is working just fine, but some how when I try to debug OSJTAG&lt;BR /&gt;gets hanged (for Flash based or RAM based target project).&lt;BR /&gt;&lt;BR /&gt;I am at a situation where I am not able to debug my code anymore for further&lt;BR /&gt;development.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The OSJTAG version as specified by P&amp;amp;E Micro's Firmware information Utility is "Firmware Build 29".&lt;BR /&gt;&lt;BR /&gt;Is there any code size limit associated with OSJTAG? Is there a bug in OSJTAG?&lt;BR /&gt;What I need to do/take care to avoid this situation?&lt;BR /&gt;&lt;BR /&gt;Warm Regards,&lt;BR /&gt;Dhaval Shah&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 May 2011 11:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/OSJTAG-debugger-Hangs-up/m-p/208045#M1994</guid>
      <dc:creator>d_shah</dc:creator>
      <dc:date>2011-05-21T11:34:09Z</dc:date>
    </item>
  </channel>
</rss>