<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic The BCM91250A in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/The-BCM91250A/m-p/207938#M1993</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Product Overview&lt;/STRONG&gt;&lt;BR /&gt;The BCM91250A is an evaluation board for the SiByteTM&lt;BR /&gt;BCM1250&lt;BR /&gt;dual-processor SOC (System On a Chip) and is implemented in the&lt;BR /&gt;standard ATX form factor. The board uses all the interfaces of the&lt;BR /&gt;BCM1250. To provide examples for both hardware and software&lt;BR /&gt;designers, configurable interfaces are used in all their modes wherever&lt;BR /&gt;possible.&lt;BR /&gt;The board comes complete with an ATX 2.0 compliant case and power&lt;BR /&gt;supply.&amp;nbsp; Common off-the-shelf peripherals can be added, such as PCI&lt;BR /&gt;graphics adapters, USB keyboards and mice, and ATA hard disks.&amp;nbsp; In&lt;BR /&gt;addition, the board has provisions for a few specialized applications&lt;BR /&gt;including PCMCIA and HyperTransport&lt;BR /&gt;TM (HT) peripherals.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;STRONG&gt;Operating System Support&lt;/STRONG&gt;&lt;BR /&gt;Two operating systems are provided for the BCM91250A.&lt;BR /&gt;? VxWorks? version 5.4 with 64-bit support for data. VxMPTM, a&lt;BR /&gt;VxWorks? kernel running independently on each core, is an available&lt;BR /&gt;option.&amp;nbsp; Users will need to use the Tornado? tools version 2.1 for 64-&lt;BR /&gt;bit or VxMPTM support. The BSP for the SWARM board is supported&lt;BR /&gt;by Wind River Systems.&lt;BR /&gt;? Linux? version 2.4 running in 32-bit or 64-bit mode with full SMP&lt;BR /&gt;support. Full source code is available.&lt;BR /&gt;Device drivers are provided as examples of how the many modes of the&lt;BR /&gt;BCM1250 interfaces are used.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Resource&lt;/STRONG&gt;:&lt;A href="http://www.seekic.com" rel="nofollow" target="_self"&gt;http://www.seekic.com&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 May 2011 13:57:20 GMT</pubDate>
    <dc:creator>silence</dc:creator>
    <dc:date>2011-05-20T13:57:20Z</dc:date>
    <item>
      <title>The BCM91250A</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/The-BCM91250A/m-p/207938#M1993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Product Overview&lt;/STRONG&gt;&lt;BR /&gt;The BCM91250A is an evaluation board for the SiByteTM&lt;BR /&gt;BCM1250&lt;BR /&gt;dual-processor SOC (System On a Chip) and is implemented in the&lt;BR /&gt;standard ATX form factor. The board uses all the interfaces of the&lt;BR /&gt;BCM1250. To provide examples for both hardware and software&lt;BR /&gt;designers, configurable interfaces are used in all their modes wherever&lt;BR /&gt;possible.&lt;BR /&gt;The board comes complete with an ATX 2.0 compliant case and power&lt;BR /&gt;supply.&amp;nbsp; Common off-the-shelf peripherals can be added, such as PCI&lt;BR /&gt;graphics adapters, USB keyboards and mice, and ATA hard disks.&amp;nbsp; In&lt;BR /&gt;addition, the board has provisions for a few specialized applications&lt;BR /&gt;including PCMCIA and HyperTransport&lt;BR /&gt;TM (HT) peripherals.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;STRONG&gt;Operating System Support&lt;/STRONG&gt;&lt;BR /&gt;Two operating systems are provided for the BCM91250A.&lt;BR /&gt;? VxWorks? version 5.4 with 64-bit support for data. VxMPTM, a&lt;BR /&gt;VxWorks? kernel running independently on each core, is an available&lt;BR /&gt;option.&amp;nbsp; Users will need to use the Tornado? tools version 2.1 for 64-&lt;BR /&gt;bit or VxMPTM support. The BSP for the SWARM board is supported&lt;BR /&gt;by Wind River Systems.&lt;BR /&gt;? Linux? version 2.4 running in 32-bit or 64-bit mode with full SMP&lt;BR /&gt;support. Full source code is available.&lt;BR /&gt;Device drivers are provided as examples of how the many modes of the&lt;BR /&gt;BCM1250 interfaces are used.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Resource&lt;/STRONG&gt;:&lt;A href="http://www.seekic.com" rel="nofollow" target="_self"&gt;http://www.seekic.com&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 May 2011 13:57:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/The-BCM91250A/m-p/207938#M1993</guid>
      <dc:creator>silence</dc:creator>
      <dc:date>2011-05-20T13:57:20Z</dc:date>
    </item>
  </channel>
</rss>