<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックRe: Error message for coldfire v2 using USBDM</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Error-message-for-coldfire-v2-using-USBDM/m-p/204897#M1870</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear raghu123,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you check that you have enabled the BDM interface on the board (link present on BDM_EN).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If this has no effect (or you are already doing this!) could you do the following:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Install the debug version of the USBDM software.&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;Try your example again&lt;/LI&gt;&lt;LI&gt;Go to the %APPDATA%\usbdm directory - (type %APPDATA%\usbdm in the address bar of a Windows Explorer window)&lt;/LI&gt;&lt;LI&gt;Zip up the file:&amp;nbsp; usbdm.log &amp;amp; post&amp;nbsp; it here&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Jun 2010 12:57:44 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2010-06-04T12:57:44Z</dc:date>
    <item>
      <title>Error message for coldfire v2 using USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Error-message-for-coldfire-v2-using-USBDM/m-p/204896#M1869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have rigged up the circuit&amp;nbsp; for &lt;STRONG&gt;USBDM_CF_JMXX_CLD&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I have programmed the board using &lt;STRONG&gt;USBDM_JMxx_v2 firmware.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; For testing pupose i am using &lt;STRONG&gt;M52233DEMO board&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i followed all the instructions&amp;nbsp; given in &lt;STRONG&gt;USBDM_CF_JMxx.chm&lt;/STRONG&gt; and accordingly configured &lt;STRONG&gt;codewarrior v7.1&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; when i try to debug the code in RAM, I could continue up to progess bar which shows the downloading no of&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; bytes to target, after that i get a error message saying:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "&lt;STRONG&gt;ColdFire GDI Protocol Adapter: An invalid preference was passed to the ColdFire GDI protocol&lt;/STRONG&gt; "&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; i tried with the &lt;STRONG&gt;CF_unlocke&lt;/STRONG&gt;r and was successful in detecting the target and erasing it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; one more thing, while installing USB driver&amp;nbsp; i get the identification of device as &lt;STRONG&gt;JB16JMxx USBDM(OSBDM mode&lt;/STRONG&gt;),&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; but in the manual the images show the USB device recognized as &lt;STRONG&gt;JMxx USBDM(TBCLF mode)&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp; is it because of this the error message is occuring?.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please help me in identifying the problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jun 2010 20:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Error-message-for-coldfire-v2-using-USBDM/m-p/204896#M1869</guid>
      <dc:creator>raghu123</dc:creator>
      <dc:date>2010-06-03T20:01:51Z</dc:date>
    </item>
    <item>
      <title>Re: Error message for coldfire v2 using USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Error-message-for-coldfire-v2-using-USBDM/m-p/204897#M1870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear raghu123,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you check that you have enabled the BDM interface on the board (link present on BDM_EN).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If this has no effect (or you are already doing this!) could you do the following:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;Install the debug version of the USBDM software.&lt;/STRONG&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;UL&gt;&lt;LI&gt;Try your example again&lt;/LI&gt;&lt;LI&gt;Go to the %APPDATA%\usbdm directory - (type %APPDATA%\usbdm in the address bar of a Windows Explorer window)&lt;/LI&gt;&lt;LI&gt;Zip up the file:&amp;nbsp; usbdm.log &amp;amp; post&amp;nbsp; it here&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jun 2010 12:57:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Error-message-for-coldfire-v2-using-USBDM/m-p/204897#M1870</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2010-06-04T12:57:44Z</dc:date>
    </item>
    <item>
      <title>Re: Error message for coldfire v2 using USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Error-message-for-coldfire-v2-using-USBDM/m-p/204898#M1871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear pgo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for the reply&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I had enabled the BDM interface on the board and have confirmed it , because if i remove the BDM enable jumper&lt;/P&gt;&lt;P&gt;&amp;nbsp;i get the error messsage very early and i cannot even see the dowloading progress bar.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Then i installed the &lt;STRONG&gt;DEBUG&amp;nbsp; VERSION of USBDM&lt;/STRONG&gt;( by double click on &lt;STRONG&gt;Install Codewarrior Debug Files.cmd&lt;/STRONG&gt;),&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the command window i could see the&amp;nbsp; installation messages&lt;/P&gt;&lt;P&gt;3 files copied for for&amp;nbsp; code warrior&amp;nbsp; for ColdFire V2,V3 &amp;amp;V4,&lt;/P&gt;&lt;P&gt;1 file copied for code warrior&amp;nbsp; for RS08/HCS08/Coldfire v1,&lt;/P&gt;&lt;P&gt;1 file copied for code warrior&amp;nbsp; for HCS12&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then i tried downloading the code into the RAM and&amp;nbsp; i got the same error message:&lt;/P&gt;&lt;P&gt;"&lt;STRONG&gt;ColdFire GDI Protocol Adapter: An invalid preference was passed to the ColdFire GDI protocol&lt;/STRONG&gt; "&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Then i typed &lt;STRONG&gt;%APPDATA%\usbdm&lt;/STRONG&gt; in the address bar of a Windows Explorer, but windows couldn't find that folder.&lt;/P&gt;&lt;P&gt;Even i went to application data folder and checked, but there was no usbdm folder.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then i gave search in windows for *.log and i could locate one file in &lt;STRONG&gt;C:\&lt;/STRONG&gt; by name &lt;STRONG&gt;usbdm_dll.log&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am attaching this file, please check whether this is correct file and any error can be located in the log file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jun 2010 19:55:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Error-message-for-coldfire-v2-using-USBDM/m-p/204898#M1871</guid>
      <dc:creator>raghu123</dc:creator>
      <dc:date>2010-06-04T19:55:30Z</dc:date>
    </item>
    <item>
      <title>Re: Error message for coldfire v2 using USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Error-message-for-coldfire-v2-using-USBDM/m-p/204899#M1872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Raghu,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm sorry I gave you the wrong location for the log file (as you discovered)&amp;nbsp; The V3 software moved this.&amp;nbsp; The log file you provided is the intended one.&amp;nbsp; It indicates a problem with the target recognizing a command.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There was a timing problem in the V2 USBDM for coldfire that affected some targets.&amp;nbsp; I would suggest trying the V3 software to see if this improves the situation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="lia-message-read"&gt;&lt;A href="http://forums.freescale.com/../OSBDM-JM60-Open-Source-BDM-for/USBDM-Version-3-JB16-JS16-JMxx-Hardware-Versions/td-p/55789" rel="nofollow" target="_blank"&gt;USBDM - Version 3 (JB16/JS16&lt;SPAN class="wbr"&gt;&amp;nbsp;&lt;/SPAN&gt;/JMxx Hardware&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you install this version you will be prompted to update the BDM firmware on the first use.&amp;nbsp; I expect that this will fix the problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jun 2010 22:04:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Error-message-for-coldfire-v2-using-USBDM/m-p/204899#M1872</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2010-06-04T22:04:31Z</dc:date>
    </item>
    <item>
      <title>Re: Error message for coldfire v2 using USBDM</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Error-message-for-coldfire-v2-using-USBDM/m-p/204900#M1873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear pgo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i have installed USBDM V3 and also updated the firmware .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; it worked perfectly fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i tried downloading code both in RAM and FLASH, both worked fine.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for the support in helping me to fix the problem&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Bye.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Jun 2010 19:21:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Error-message-for-coldfire-v2-using-USBDM/m-p/204900#M1873</guid>
      <dc:creator>raghu123</dc:creator>
      <dc:date>2010-06-05T19:21:46Z</dc:date>
    </item>
  </channel>
</rss>