<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDML中的主题 Unable to detect microcontroller in CodeWarrior</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Unable-to-detect-microcontroller-in-CodeWarrior/m-p/203909#M1747</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KITMMA955XLEVM"&gt;KITMMA955XLEVM: Sensor Toolbox for Xtrinsic Smart Sensing Platform&lt;/A&gt;, and using CodeWarrior 10.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to create a custom program and load it on to the microcontroller. However, I am unable to connect or even find the microcontroller when attempting to enter debug mode.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/118879iB4B2D4362DD3B022/image-size/large?v=v2&amp;amp;px=999" title="osbdm.jpg" alt="osbdm.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running a Bareboard Project with Open Source BDM. The board is connected to the computer through a single USB cable. I am able to use Sensor Toolbox to read the data from the board. The CPU type on the board is MCF51QE64CLH.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running on Windows 7 Home Premium 64-bit. I've tried re-installing the drivers from &lt;A href="http://www.pemicro.com/osbdm" title="http://www.pemicro.com/osbdm"&gt;PEMicro.com&lt;/A&gt;, but nothing shows up in Device Manager.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/118880iEFDA6FF11C056B1D/image-size/large?v=v2&amp;amp;px=999" title="osbdm2.jpg.png" alt="osbdm2.jpg.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any help or advice would be greatly appreciated. Cheers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Sep 2012 12:49:58 GMT</pubDate>
    <dc:creator>kpro3</dc:creator>
    <dc:date>2012-09-28T12:49:58Z</dc:date>
    <item>
      <title>Unable to detect microcontroller in CodeWarrior</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Unable-to-detect-microcontroller-in-CodeWarrior/m-p/203909#M1747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KITMMA955XLEVM"&gt;KITMMA955XLEVM: Sensor Toolbox for Xtrinsic Smart Sensing Platform&lt;/A&gt;, and using CodeWarrior 10.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to create a custom program and load it on to the microcontroller. However, I am unable to connect or even find the microcontroller when attempting to enter debug mode.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/118879iB4B2D4362DD3B022/image-size/large?v=v2&amp;amp;px=999" title="osbdm.jpg" alt="osbdm.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm running a Bareboard Project with Open Source BDM. The board is connected to the computer through a single USB cable. I am able to use Sensor Toolbox to read the data from the board. The CPU type on the board is MCF51QE64CLH.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running on Windows 7 Home Premium 64-bit. I've tried re-installing the drivers from &lt;A href="http://www.pemicro.com/osbdm" title="http://www.pemicro.com/osbdm"&gt;PEMicro.com&lt;/A&gt;, but nothing shows up in Device Manager.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/118880iEFDA6FF11C056B1D/image-size/large?v=v2&amp;amp;px=999" title="osbdm2.jpg.png" alt="osbdm2.jpg.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any help or advice would be greatly appreciated. Cheers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Sep 2012 12:49:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Unable-to-detect-microcontroller-in-CodeWarrior/m-p/203909#M1747</guid>
      <dc:creator>kpro3</dc:creator>
      <dc:date>2012-09-28T12:49:58Z</dc:date>
    </item>
  </channel>
</rss>