<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USBDM 4.7 Device Not Responding in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193731#M1609</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PGO,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am talking to my micro now.&amp;nbsp; Thanks for all the guidance and patience.&amp;nbsp; I'm still having problems with what appears to be freescale's serial monitor code but I beleive I am past any of problems with the pod.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Jan 2012 09:41:31 GMT</pubDate>
    <dc:creator>DoneBrokeIt</dc:creator>
    <dc:date>2012-01-11T09:41:31Z</dc:date>
    <item>
      <title>USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193719#M1597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need a some help.&amp;nbsp; I am using USBDM version 4.7 and codewarrior version 5.9.&amp;nbsp; I am attempting to load serial monitor into a HCS12DG128.&amp;nbsp; All I get is device not responding when I attempt to debug the standard Freescale Serial Monitor code.&amp;nbsp; The first thing I would like to do is just verify that all my connections are correct.&amp;nbsp; I have attached a copy of my schematic.&amp;nbsp; Can anyone veryify pin out?&amp;nbsp; If this is all OK maybe we can dig into the settings and what nots.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jan 2012 10:40:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193719#M1597</guid>
      <dc:creator>DoneBrokeIt</dc:creator>
      <dc:date>2012-01-03T10:40:16Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193720#M1598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear James,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After a quick glance (and from memory!)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;XCLKS is active low and you have it active.&amp;nbsp; Doesn't this mean an external clock source rather than a XTAL?&lt;/P&gt;&lt;P&gt;R16 seems very low.&amp;nbsp; I would have expected about 1M?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jan 2012 12:20:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193720#M1598</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2012-01-03T12:20:46Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193721#M1599</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PGO,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Per the data sheet XCLKS is low for an external clock or the Pierce configuration.&amp;nbsp; It is only high for the Colpitts oscilator.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The schematic I attached earlier is also has an error.&amp;nbsp; modb and moda are tied low to enable Normal Single Chip mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jan 2012 09:35:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193721#M1599</guid>
      <dc:creator>DoneBrokeIt</dc:creator>
      <dc:date>2012-01-04T09:35:18Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193722#M1600</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear james,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just shows you how good my memory is!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For reference I've attached a design I did previously for a DP256. This board works fine with a DG128 without any changes.&amp;nbsp; It uses the Pierce OSC.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I assume you can check the BDM with another board/chip so you know it's working?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Things to check (which you probably have already done if you have a CRO):&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Check for oscillator activity on XTAL/EXTAL&lt;/LI&gt;&lt;LI&gt;Check ECLK activity&lt;/LI&gt;&lt;LI&gt;The RESET signal should go low when the BDM is initially attempting to connect.&lt;/LI&gt;&lt;LI&gt;The BKGD signal should have activity when connecting.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I can provide more detail on the RESET/BKGD signal connect sequence if useful.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jan 2012 08:21:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193722#M1600</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2012-01-05T08:21:36Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193723#M1601</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the example.&amp;nbsp; Looking at it, the hardware should be good.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I looked at the RESET and BKGD pins on the scope there is no activity.&amp;nbsp; I did have some difficulties installing the drivers originally but beleive they may be correct as my computer does recognize the pod.&amp;nbsp; I do not have another board to test the operation of the pod.&amp;nbsp; I did have a micro fail when the pod was connected but appears to be functioning correctly after replacing it.&amp;nbsp; It is possible that it damaged the pod as well but I was having the same connection problems prior to this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a method for testing the pod as a stand alone device to verify operation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jan 2012 11:25:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193723#M1601</guid>
      <dc:creator>DoneBrokeIt</dc:creator>
      <dc:date>2012-01-05T11:25:47Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193724#M1602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear James,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is TCL command interpreter supplied with the later version of usbdm.&amp;nbsp; In V4.7 &amp;amp; 4.8 this is available in the start menu.&lt;/P&gt;&lt;P&gt;Type ? to get a list of commands.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can do a basic output pin static test with the following commands:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;;# Simple BDM test openbdmsettarget hcs12

pinSet rst=LpinSet rst=3 pinSet bkgd=L pinSet bkgd=3&lt;/PRE&gt;&lt;P&gt;You would need to supplied power to the BDM connector for this to affect the pins if you are using an unpowered BDM.&amp;nbsp; This should be done without the target connected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The following provides a repeating loop for testing with a CRO:&lt;/P&gt;&lt;PRE&gt;;# Simple BDM test loopopenbdmsettarget hcs12proc test {} {   for { set i 1 } { $i &amp;lt;= 100 } { incr i } {     pinSet rst=L  ; after 10;     pinSet rst=3  ; after 10;     pinSet bkgd=L ; after 10;     pinSet bkgd=3 ; after 10;     pinSet bkgd=H ; after 10;     pinSet bkgd=3 ; after 10;   }}&lt;/PRE&gt;&lt;P&gt;Save it to a file (say testbdm.tcl)&amp;nbsp; in the same directory as the USBDM files and then use:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;source testbdm.tcltest&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;to load script and execute the test procedure.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:47:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193724#M1602</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2020-10-29T09:47:56Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193725#M1603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Before I installed USBDM V4.8, I read one of these threads that was talking about errors when using virtual machines.&amp;nbsp; As I only have windows 7 64 and codewarrior 5.9, I had to run it in XP mode.&amp;nbsp; I downloaded CW 5.1 and installed on windows 7.&amp;nbsp; I also installed USBDM 4.8.&amp;nbsp; Windows would not recognize the pod.&amp;nbsp; I used the zadig app from the 4.6 download and then windows was happy.&amp;nbsp; When the pod is plugged into a USB port, the red LED is lit continuously.&amp;nbsp; When I use TBDML as the connection the red LED momentarily turns off after starting debugging and then immediately back on.&amp;nbsp; The command window says no link to target.&amp;nbsp; If I select P&amp;amp;E Multilink/Cyclone Pro as the connection, the LED is always red and the command window says unable to load PEOSBDMV1.DLL.&amp;nbsp; In any case there is still no activity on the BCKG or RESET lines.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jan 2012 10:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193725#M1603</guid>
      <dc:creator>DoneBrokeIt</dc:creator>
      <dc:date>2012-01-09T10:08:37Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193726#M1604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So I went to play with the TCL interpretor and when using the openbdm command the response is found 1 device and then failed to open device 0 and then USB transfer error.&amp;nbsp; At this point all I can think is there is stil something missing from my installation.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jan 2012 10:30:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193726#M1604</guid>
      <dc:creator>DoneBrokeIt</dc:creator>
      <dc:date>2012-01-09T10:30:37Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193727#M1605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is important to use the same BDM firmware version as the PC software.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I suggest you try the stand-alone HCS12 programmer.&amp;nbsp; It reports the BDM firmware version and DLL version on the the first tab.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If they are not the same then you should update the BDM firmware using the USBDM Bootloader.&amp;nbsp; The firmware files are provided in the installation directory.&amp;nbsp; There is a link on the start menu to the folder.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note that one firmware file was incorrect and a newer version was uploaded to sourceforge separately.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The procedure is given part way down this page:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="4"&gt;&lt;STRONG&gt;Update of BDM Firmware and changing serial number.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://usbdm.sourceforge.net/USBDM_V4.8/USBDM_JS16/html/installation_page.html" rel="nofollow" target="_blank"&gt;http://usbdm.sourceforge.net/USBDM_V4.8/USBDM_JS16/html/installation_page.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This is for a JS16 BDM but is similar for other versions,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Jan 2012 14:28:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193727#M1605</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2012-01-09T14:28:09Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193728#M1606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It appears as though you have already addressed this issue in another post but the firmware in the 4.8 folder is for the Kinetis board.&amp;nbsp; I was going to load the 4.7 firmware as you suggested but it does not appear to be available anymore on sourceforge.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jan 2012 11:57:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193728#M1606</guid>
      <dc:creator>DoneBrokeIt</dc:creator>
      <dc:date>2012-01-10T11:57:09Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193729#M1607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Firmware files have been included in the .msi installs.&amp;nbsp; both for V4.7 &amp;amp; V4.8 but the image for one hardware (USBDM_JMxxCLD_V4.sx) was built incorrectly in the latter and has been uploaded separately on Sourceforge,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any changes in the firmware for V4.7 was rolled into the final posted version (USBDM_4_7_0i_Win.msi).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would suggest installing V4.8 and downloading the separate flash image if necessary.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm sorry - This seems to have been a lot of stuffing about!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you advise what hardware you are using if you still have problems?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jan 2012 13:22:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193729#M1607</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2012-01-10T13:22:24Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193730#M1608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The programming pod I am using is this one:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.technologicalarts.ca/catalog/product_info.php?products_id=572" rel="nofollow" target="_blank"&gt;http://www.technologicalarts.ca/catalog/product_info.php?products_id=572&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My micro is a MC9S12DG128.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I will check for the other firmware files later this evening.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2012 00:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193730#M1608</guid>
      <dc:creator>DoneBrokeIt</dc:creator>
      <dc:date>2012-01-11T00:06:11Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193731#M1609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PGO,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am talking to my micro now.&amp;nbsp; Thanks for all the guidance and patience.&amp;nbsp; I'm still having problems with what appears to be freescale's serial monitor code but I beleive I am past any of problems with the pod.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;James&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2012 09:41:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193731#M1609</guid>
      <dc:creator>DoneBrokeIt</dc:creator>
      <dc:date>2012-01-11T09:41:31Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.7 Device Not Responding</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193732#M1610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What made it work:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I installed CW 5.1 on windows 7.&amp;nbsp; Installed USBDM 4.8.&amp;nbsp; Flashed the pod to the 4.8 firmware.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am now able to program my micro.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2012 23:00:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-7-Device-Not-Responding/m-p/193732#M1610</guid>
      <dc:creator>DoneBrokeIt</dc:creator>
      <dc:date>2012-01-11T23:00:48Z</dc:date>
    </item>
  </channel>
</rss>