<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USBDM 4.9.5 / Flash Programmer HCS08 / Erase the Flash Memory without Reprogramming? in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-9-5-Flash-Programmer-HCS08-Erase-the-Flash-Memory/m-p/189365#M1402</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Florian,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The programmers don't allow programming unless a file has been loaded.&amp;nbsp; This was the intended operation previously but I may have overlooked some condition.&amp;nbsp; It was intended that you could trim or secure a device without a file but this would not serve your requirement. This was just me being careful.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You will have to load an empty S19 file such as that attached and use the Mass Erase option.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Aug 2012 14:42:12 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2012-08-16T14:42:12Z</dc:date>
    <item>
      <title>USBDM 4.9.5 / Flash Programmer HCS08 / Erase the Flash Memory without Reprogramming?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-9-5-Flash-Programmer-HCS08-Erase-the-Flash-Memory/m-p/189364#M1401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;in the past I was using the Flash Programmer for the HCS08 microcontroller with success.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No I want to erase the whole flash memory of the micorocontroller to make some investigations with an unprogrammed system (safe state of I/O lines, etc.).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately it seems not to possible to erase the device without reprogramming it immediately.&lt;/P&gt;&lt;P&gt;Have I overlooked something?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards, Florian&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Aug 2012 22:41:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-9-5-Flash-Programmer-HCS08-Erase-the-Flash-Memory/m-p/189364#M1401</guid>
      <dc:creator>florianton</dc:creator>
      <dc:date>2012-08-15T22:41:01Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.9.5 / Flash Programmer HCS08 / Erase the Flash Memory without Reprogramming?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-9-5-Flash-Programmer-HCS08-Erase-the-Flash-Memory/m-p/189365#M1402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Florian,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The programmers don't allow programming unless a file has been loaded.&amp;nbsp; This was the intended operation previously but I may have overlooked some condition.&amp;nbsp; It was intended that you could trim or secure a device without a file but this would not serve your requirement. This was just me being careful.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You will have to load an empty S19 file such as that attached and use the Mass Erase option.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2012 14:42:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-9-5-Flash-Programmer-HCS08-Erase-the-Flash-Memory/m-p/189365#M1402</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2012-08-16T14:42:12Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM 4.9.5 / Flash Programmer HCS08 / Erase the Flash Memory without Reprogramming?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-9-5-Flash-Programmer-HCS08-Erase-the-Flash-Memory/m-p/189366#M1403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello pgo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tested your suggestion to use an empty S19 file to erase the flash of the microcontroller.&lt;/P&gt;&lt;P&gt;It has worked very well in my case - thank you very much!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I still think it would not be a bad idea to add an extra button for mass erase without programming the microcontroller to the flash programming tool.&lt;/P&gt;&lt;P&gt;Example: with the "STM32 ST-Link Utility" for the STM32 microcontroller I can choose if I only want to "erase", "erase &amp;amp; program" or "erase &amp;amp; program &amp;amp; verify" the chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But don't get me wrong.&lt;/P&gt;&lt;P&gt;I'm very happy that this tool exists and I only want to give you a feedback for improvement!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Florian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Aug 2012 13:56:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/USBDM-4-9-5-Flash-Programmer-HCS08-Erase-the-Flash-Memory/m-p/189366#M1403</guid>
      <dc:creator>florianton</dc:creator>
      <dc:date>2012-08-17T13:56:34Z</dc:date>
    </item>
  </channel>
</rss>