<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How can I use MON08Interface to debug HC08JB16? in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-can-I-use-MON08Interface-to-debug-HC08JB16/m-p/187916#M1355</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Dear syf,&lt;BR /&gt;&lt;BR /&gt;A few things to check:&lt;BR /&gt;&lt;BR /&gt;Have you set up the chip to boot into&amp;nbsp; Monitor mode - see chapter 9 of the JB16 documentation.&lt;BR /&gt;&lt;BR /&gt;I normally use "Ignore security" .&amp;nbsp; The only disadvantage is that it will erase the chip before programming.&lt;BR /&gt;&lt;BR /&gt;I have found the MON08 interface a pain to use and rather unreliable.&lt;BR /&gt;&lt;BR /&gt;Also:&lt;BR /&gt;The JB16 uses a different clock frequency to the original JB08 so a different version of the TBDML code is needed.&amp;nbsp; I would suggest you look at this thread &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=TBDML&amp;amp;thread.id=240" target="test_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=TBDML&amp;amp;thread.id=240&lt;/A&gt;.&lt;BR /&gt;&lt;BR /&gt;The JB16 supports one time INITIAL programming using the USB interface.&amp;nbsp; This is much easier method of programming the hardware but you only get once chance to get it correct!&amp;nbsp; Once programmed this option is not available unless special steps are taken in the programmed code.&amp;nbsp; See app note:AN2399 for details.&lt;BR /&gt;&lt;BR /&gt;I hope the above helps.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Sep 2008 10:08:45 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2008-09-25T10:08:45Z</dc:date>
    <item>
      <title>How can I use MON08Interface to debug HC08JB16?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-can-I-use-MON08Interface-to-debug-HC08JB16/m-p/187915#M1354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi,&lt;BR /&gt;I'm a flesh to TBDML.I want to development a TBDML with JB16.When i use prog08sz.exe to programming the device,i have some problems.Details as bellow.&lt;BR /&gt;&lt;BR /&gt;1.My target board scheme is just use the JB16 instead of JB8.&lt;BR /&gt;2.The oscillate is 12MHz.&lt;BR /&gt;3.Connect to PC via the MON08Interface.And my configuration are&lt;IMG alt=":smileysad:" class="emoticon emoticon-smileysad" id="smileysad" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-sad.gif" title="Smiley Sad" /&gt;1),Class iii,port com4,baud 19200;(2),attempt FF-FF-FF-FF-FF-FF-FF-FF{From security.ini}{Recent}.&lt;BR /&gt;&lt;BR /&gt;But i can not link to the target via the configuration as up.When i'm trying ,i got the picture as bellow.&lt;BR /&gt;Then,if i choose the to "ignore security failure and enter monitor mode",in this case,the pc can link to the target,but cann't programming the JB16.&lt;BR /&gt;&lt;BR /&gt;So,i'm here to find some help.Can anybody give me some advise or you expreaence.&lt;BR /&gt;Thanks a lot.&lt;BR /&gt;&lt;BR /&gt;syf&lt;BR /&gt;2008.9.24&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Sep 2008 11:47:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/How-can-I-use-MON08Interface-to-debug-HC08JB16/m-p/187915#M1354</guid>
      <dc:creator>syf</dc:creator>
      <dc:date>2008-09-24T11:47:35Z</dc:date>
    </item>
    <item>
      <title>Re: How can I use MON08Interface to debug HC08JB16?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-can-I-use-MON08Interface-to-debug-HC08JB16/m-p/187916#M1355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Dear syf,&lt;BR /&gt;&lt;BR /&gt;A few things to check:&lt;BR /&gt;&lt;BR /&gt;Have you set up the chip to boot into&amp;nbsp; Monitor mode - see chapter 9 of the JB16 documentation.&lt;BR /&gt;&lt;BR /&gt;I normally use "Ignore security" .&amp;nbsp; The only disadvantage is that it will erase the chip before programming.&lt;BR /&gt;&lt;BR /&gt;I have found the MON08 interface a pain to use and rather unreliable.&lt;BR /&gt;&lt;BR /&gt;Also:&lt;BR /&gt;The JB16 uses a different clock frequency to the original JB08 so a different version of the TBDML code is needed.&amp;nbsp; I would suggest you look at this thread &lt;A href="http://forums.freescale.com/freescale/board/message?board.id=TBDML&amp;amp;thread.id=240" target="test_blank"&gt;http://forums.freescale.com/freescale/board/message?board.id=TBDML&amp;amp;thread.id=240&lt;/A&gt;.&lt;BR /&gt;&lt;BR /&gt;The JB16 supports one time INITIAL programming using the USB interface.&amp;nbsp; This is much easier method of programming the hardware but you only get once chance to get it correct!&amp;nbsp; Once programmed this option is not available unless special steps are taken in the programmed code.&amp;nbsp; See app note:AN2399 for details.&lt;BR /&gt;&lt;BR /&gt;I hope the above helps.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2008 10:08:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/How-can-I-use-MON08Interface-to-debug-HC08JB16/m-p/187916#M1355</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2008-09-25T10:08:45Z</dc:date>
    </item>
    <item>
      <title>Re: How can I use MON08Interface to debug HC08JB16?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-can-I-use-MON08Interface-to-debug-HC08JB16/m-p/187917#M1356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;thanks!&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Sep 2008 11:54:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/How-can-I-use-MON08Interface-to-debug-HC08JB16/m-p/187917#M1356</guid>
      <dc:creator>syf</dc:creator>
      <dc:date>2008-09-25T11:54:05Z</dc:date>
    </item>
    <item>
      <title>Re: How can I use MON08Interface to debug HC08JB16?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-can-I-use-MON08Interface-to-debug-HC08JB16/m-p/187918#M1357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Thanks for the guys who helped me.I'm here agian to declear that my TBDML is now working perfect!&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2008 21:04:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/How-can-I-use-MON08Interface-to-debug-HC08JB16/m-p/187918#M1357</guid>
      <dc:creator>syf</dc:creator>
      <dc:date>2008-09-26T21:04:00Z</dc:date>
    </item>
  </channel>
</rss>