<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックSupport for OSBDM using Code Warrior 10</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Support-for-OSBDM-using-Code-Warrior-10/m-p/183886#M1303</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to get a project based on a MCF52259 working using the Open Source BDM module. I am using CodeWarrior 10 and when I try to program the application into the ColdFire I get the following error message -&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P align="left"&gt;fl::target -lc "HelloWorld_twrmcf52259_Ext_MRAM_Debug_OSBDM"&lt;/P&gt;&lt;P align="left"&gt;fl::target -b 0x20000000 0xffff&lt;/P&gt;&lt;P align="left"&gt;fl::target -v off -l off -ie on -i "C:/Users/Owner/Documents/Freescale MQX 3.6/lib/twrmcf52259.cw10/mqx/dbg/twrmcf52259.cfg" -p MCF52259&lt;/P&gt;&lt;P align="left"&gt;cmdwin::fl::device -d "CFM_MCF5225X_512" -o "256Kx16x1" -a 0x0 0x7ffff&lt;/P&gt;&lt;P align="left"&gt;cmdwin::fl::image -f "W:\\CodeWarrior10\\HelloWorld\\twrmcf52259_Int_Flash_Debug\\HelloWorld.elf" -t "Auto Detect" -re off -oe off&lt;/P&gt;&lt;P align="left"&gt;cmdwin::fl::erase image&lt;/P&gt;&lt;P&gt;&lt;FONT color="#ff0000" size="2"&gt;&lt;FONT color="#ff0000" size="2"&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;Error: Connect Failed.&lt;/P&gt;&lt;P align="left"&gt;Can't connect. Can't load GDI dll - System error:The specified module could not be found.&lt;/P&gt;&lt;P&gt;. (ColdFire GDI Protocol Adapter)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;Is this because I have not added the GDI DLL plug-in? If so how do I go about adding this in?&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;DIV&gt;ebee&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Feb 2011 23:48:30 GMT</pubDate>
    <dc:creator>ebee</dc:creator>
    <dc:date>2011-02-16T23:48:30Z</dc:date>
    <item>
      <title>Support for OSBDM using Code Warrior 10</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Support-for-OSBDM-using-Code-Warrior-10/m-p/183886#M1303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to get a project based on a MCF52259 working using the Open Source BDM module. I am using CodeWarrior 10 and when I try to program the application into the ColdFire I get the following error message -&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P align="left"&gt;fl::target -lc "HelloWorld_twrmcf52259_Ext_MRAM_Debug_OSBDM"&lt;/P&gt;&lt;P align="left"&gt;fl::target -b 0x20000000 0xffff&lt;/P&gt;&lt;P align="left"&gt;fl::target -v off -l off -ie on -i "C:/Users/Owner/Documents/Freescale MQX 3.6/lib/twrmcf52259.cw10/mqx/dbg/twrmcf52259.cfg" -p MCF52259&lt;/P&gt;&lt;P align="left"&gt;cmdwin::fl::device -d "CFM_MCF5225X_512" -o "256Kx16x1" -a 0x0 0x7ffff&lt;/P&gt;&lt;P align="left"&gt;cmdwin::fl::image -f "W:\\CodeWarrior10\\HelloWorld\\twrmcf52259_Int_Flash_Debug\\HelloWorld.elf" -t "Auto Detect" -re off -oe off&lt;/P&gt;&lt;P align="left"&gt;cmdwin::fl::erase image&lt;/P&gt;&lt;P&gt;&lt;FONT color="#ff0000" size="2"&gt;&lt;FONT color="#ff0000" size="2"&gt;&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P align="left"&gt;Error: Connect Failed.&lt;/P&gt;&lt;P align="left"&gt;Can't connect. Can't load GDI dll - System error:The specified module could not be found.&lt;/P&gt;&lt;P&gt;. (ColdFire GDI Protocol Adapter)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;Is this because I have not added the GDI DLL plug-in? If so how do I go about adding this in?&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;DIV&gt;ebee&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Feb 2011 23:48:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Support-for-OSBDM-using-Code-Warrior-10/m-p/183886#M1303</guid>
      <dc:creator>ebee</dc:creator>
      <dc:date>2011-02-16T23:48:30Z</dc:date>
    </item>
  </channel>
</rss>