<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックRe: Need help: install + identify USBDM pcb hardware revision</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Need-help-install-identify-USBDM-pcb-hardware-revision/m-p/180941#M1243</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Found the original drivers and installed them (after uninstalling and removing my generated driver). It works fine now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The reason why I missed it. I did not notice the separate USBDM_Drivers_1_0_1_Win_x64.msi in the sourceforge, as I just installed the package at &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://sourceforge.net/projects/usbdm"&gt;http://sourceforge.net/projects/usbdm&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The 4.9 USB driver page had more detailed instructions but the latest version does not mention the need to install the MSI above. &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_CF_JMxx/html/driver_page.html"&gt;http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_CF_JMxx/html/driver_page.html&lt;/A&gt;&lt;SPAN&gt; - you might want to edit this page to mention this extra file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One more (dumb) question: would this board support ARM-SWD or only JTAG? My targets would be Kinetis devices&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Nov 2012 07:07:51 GMT</pubDate>
    <dc:creator>adioltean</dc:creator>
    <dc:date>2012-11-21T07:07:51Z</dc:date>
    <item>
      <title>Need help: install + identify USBDM pcb hardware revision</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Need-help-install-identify-USBDM-pcb-hardware-revision/m-p/180937#M1239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First, a big thanks to the creators of USBDM - pretty amazing stuff! &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I acquired this device over eBay in the hope of starting off quickly, but I have trouble identifying the actual version of the device and using the software. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Questions&lt;/P&gt;&lt;P&gt;- What USBDM revision does this correspond to? Looks like an older version (V2.0) of the PCB not the latest 3.0 version. &lt;/P&gt;&lt;P&gt;- What software version should I use? &lt;/P&gt;&lt;P&gt;- Any recommended firmware updates? &lt;/P&gt;&lt;P&gt;- What OS should I install the software on? (I use Windows 7 64-bit) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is a high-res picture of the board &lt;A href="http://img02.taobaocdn.com/imgextra/i2/37306034/T2VBWpXb4bXXXXXXXX_!!37306034.jpg" title="http://img02.taobaocdn.com/imgextra/i2/37306034/T2VBWpXb4bXXXXXXXX_!!37306034.jpg"&gt;http://img02.taobaocdn.com/imgextra/i2/37306034/T2VBWpXb4bXXXXXXXX_!!37306034.jpg&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/118984iB6049C187667AD90/image-size/large?v=v2&amp;amp;px=999" title="T2VBWpXb4bXXXXXXXX_!!37306034.jpg" alt="T2VBWpXb4bXXXXXXXX_!!37306034.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This seems somewhat similar with the latest V3 of the USBDM/CF JMxx v4.10.3 but without the Kinetis adapters. &lt;A href="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_CF_JMxx/html/USBDM_CF_SER.jpg" title="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_CF_JMxx/html/USBDM_CF_SER.jpg"&gt;http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_CF_JMxx/html/USBDM_CF_SER.jpg&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Details:&lt;/P&gt;&lt;P&gt;1) The board processor is JM60 (MCS9S08JM60CLD)&lt;/P&gt;&lt;P&gt;2) The board "version" states Freescale_BDM&amp;nbsp;&amp;nbsp; V2.0&amp;nbsp;&amp;nbsp; 2011-03-01 &lt;/P&gt;&lt;P&gt;3) The USB device is not recognized by the latest USBDM 4.10 software. Its hardware ID is USB\VID_16D0&amp;amp;PID_0567&amp;amp;REV_0410 and the instance path is USB\VID_16D0&amp;amp;PID_0567\USBDM-JMXX-CF-0001&amp;nbsp; (the REV0410 seems to suggest the 4.10 firmware or something like this?)&lt;/P&gt;&lt;P&gt;4) The board has three adapters: 26-pin JTAG, 14-pin JTAG and the well-known 6-pin BDM adapter.&lt;/P&gt;&lt;P&gt;5) The USBDM software installation completed fine with the default options&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Granted, I installed USBDM 4.10 on a 64-bit version of Windows 7, so it might be a driver installation issue. Or maybe the device is toasted. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone help? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks, Adi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2012 06:43:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Need-help-install-identify-USBDM-pcb-hardware-revision/m-p/180937#M1239</guid>
      <dc:creator>adioltean</dc:creator>
      <dc:date>2012-11-20T06:43:20Z</dc:date>
    </item>
    <item>
      <title>Re: Need help: install + identify USBDM pcb hardware revision</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Need-help-install-identify-USBDM-pcb-hardware-revision/m-p/180938#M1240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys, problem solved (so far!). The drivers were missing. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Digging in the USBDM help, I found this page in an older version (4.9). &lt;A href="http://usbdm.sourceforge.net/USBDM_V4.9/USBDM_JMxx/html/driver_page.html" title="http://usbdm.sourceforge.net/USBDM_V4.9/USBDM_JMxx/html/driver_page.html"&gt;USBDM (JMxx Version): USB Driver Installation &lt;/A&gt;(Interestingly enough this was missing from 4.10 - editing problem?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried first the &lt;A href="http://sourceforge.net/apps/trac/libusb-win32/wiki" title="http://sourceforge.net/apps/trac/libusb-win32/wiki"&gt; libusb-win32 &lt;/A&gt;which also contains a INF generator program. By using the proper PID/VID I was able to make it work somehow (the driver installation was 100% succesful) but then the USBDM tools wouldn't recognize the new device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Digging in the same USBDM 4.9 page I found another tool called Zadig (the tool has since moved to GitHub here: &lt;A href="https://github.com/pbatard/libwdi/wiki" title="https://github.com/pbatard/libwdi/wiki"&gt;Home · pbatard/libwdi Wiki · GitHub&lt;/A&gt; (or, see &lt;A href="http://sourceforge.net/projects/libwdi/files/zadig/" title="http://sourceforge.net/projects/libwdi/files/zadig/"&gt;libwdi - Browse /zadig at SourceForge.net&lt;/A&gt; for the direct download location), With Zadig, I was able to reinstall properly the device. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After this, the "openbdm" command in the TCL interpreter worked. Yes! &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;% openbdm&lt;/P&gt;&lt;P&gt;Found 1 devices&lt;/P&gt;&lt;P&gt;USBDM DLL Version = 4.10.3&lt;/P&gt;&lt;P&gt;BDM Version = HW=8C, SW=49&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2012 09:02:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Need-help-install-identify-USBDM-pcb-hardware-revision/m-p/180938#M1240</guid>
      <dc:creator>adioltean</dc:creator>
      <dc:date>2012-11-20T09:02:49Z</dc:date>
    </item>
    <item>
      <title>Re: Need help: install + identify USBDM pcb hardware revision</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Need-help-install-identify-USBDM-pcb-hardware-revision/m-p/180939#M1241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;(Just replying with the list of remaining questions)&lt;/P&gt;&lt;P&gt;- Based on the information above, what would be the PCB version? Are there some PCB design schematics on sourceforge for this particular version? &lt;/P&gt;&lt;P&gt;- What is the exact firmware version on the device? &lt;/P&gt;&lt;P&gt;- Can I safely upgrade the firmware to the latest version? I installed USBDM 4.10.3. Just wanted to make sure I don't brick the device ... &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2012 09:22:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Need-help-install-identify-USBDM-pcb-hardware-revision/m-p/180939#M1241</guid>
      <dc:creator>adioltean</dc:creator>
      <dc:date>2012-11-20T09:22:23Z</dc:date>
    </item>
    <item>
      <title>Re: Need help: install + identify USBDM pcb hardware revision</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Need-help-install-identify-USBDM-pcb-hardware-revision/m-p/180940#M1242</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board does not correspond directly with any of the "official" example PCBs that I published.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From its appearance it is approximately equivalent to the USBDM-V2 which is similar to V3 but with the following changes omissions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;V3 vs V2&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Serial interface may not be buffered&lt;/LI&gt;&lt;LI&gt;Kinetis connector absent (requires an adapter from coldfire connector or similar).&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On your board specifically:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Has an extra LED&lt;/LI&gt;&lt;LI&gt;RS08 power is not populated&lt;/LI&gt;&lt;LI&gt;Has some jumpers - I don't know what for.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All the USBDM-JM60 deluxe boards use the same firmware so I would suggest updating to the latest version.&amp;nbsp; The firmware updater will identify the correct firmware providing the existing firmware is standard.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The driver installation should have also been straight forward using the drivers provided with V4.10.3. Note these are a separate download!&amp;nbsp; The use of zadig is no longer recommended - did you install the drivers with V4.10.3?&amp;nbsp; If so, I'm puzzled by the difficulty unless the firmware was very old (using the earlier bootloader).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Message was edited by: Peter O Donoghue Corrected version numbers!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2012 02:39:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Need-help-install-identify-USBDM-pcb-hardware-revision/m-p/180940#M1242</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2012-11-21T02:39:33Z</dc:date>
    </item>
    <item>
      <title>Re: Need help: install + identify USBDM pcb hardware revision</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Need-help-install-identify-USBDM-pcb-hardware-revision/m-p/180941#M1243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Found the original drivers and installed them (after uninstalling and removing my generated driver). It works fine now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The reason why I missed it. I did not notice the separate USBDM_Drivers_1_0_1_Win_x64.msi in the sourceforge, as I just installed the package at &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://sourceforge.net/projects/usbdm"&gt;http://sourceforge.net/projects/usbdm&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The 4.9 USB driver page had more detailed instructions but the latest version does not mention the need to install the MSI above. &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_CF_JMxx/html/driver_page.html"&gt;http://usbdm.sourceforge.net/USBDM_V4.10/USBDM_CF_JMxx/html/driver_page.html&lt;/A&gt;&lt;SPAN&gt; - you might want to edit this page to mention this extra file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One more (dumb) question: would this board support ARM-SWD or only JTAG? My targets would be Kinetis devices&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2012 07:07:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Need-help-install-identify-USBDM-pcb-hardware-revision/m-p/180941#M1243</guid>
      <dc:creator>adioltean</dc:creator>
      <dc:date>2012-11-21T07:07:51Z</dc:date>
    </item>
    <item>
      <title>Re: Need help: install + identify USBDM pcb hardware revision</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Need-help-install-identify-USBDM-pcb-hardware-revision/m-p/180942#M1244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the page you linked, the section:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;H2&gt;Installation of USBDM USB drivers for Windows&lt;/H2&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;was meant to explain the change to separate driver installation but (obviously) it could do with some improvement!:smileysilly:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board will only support the ARM-JTAG interface unfortunately.&amp;nbsp; There is a table on this page that summarises this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://usbdm.sourceforge.net/" title="http://usbdm.sourceforge.net/"&gt;USBDM: USBDM Debugger interface for Freescale RS08,HCS08,HCS12,Coldfire and ARM-Kinetis Devices.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2012 07:33:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Need-help-install-identify-USBDM-pcb-hardware-revision/m-p/180942#M1244</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2012-11-21T07:33:34Z</dc:date>
    </item>
  </channel>
</rss>