<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDML中的主题 Re: TBDML Error</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/TBDML-Error/m-p/176405#M1158</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Spencer,&lt;BR /&gt;&lt;BR /&gt;The TBDML has no trouble with S12 and does not use a different list of PARTID from the other tool.&lt;BR /&gt;I see two choices for you:&lt;BR /&gt;&lt;BR /&gt;- Check your communications parameters and see if 0x0033 is the right PARTID for the DT/DG256.&lt;BR /&gt;- Ask support from FSL direct because you are a partner...&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Jan 2008 03:06:51 GMT</pubDate>
    <dc:creator>Nabla69</dc:creator>
    <dc:date>2008-01-09T03:06:51Z</dc:date>
    <item>
      <title>TBDML Error</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/TBDML-Error/m-p/176404#M1157</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I implemented a TBDML BDM on a DT256 target board aimed at the Educational arena.&amp;nbsp; However, when I attempt to use CW for HCS12, V4.6 I get the following error:&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;"Unknown Device: The connected device PARTID/SDID (0x0033 is not registered in the debugger core file.&amp;nbsp; Do you want to select the device from a list?)&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;I&amp;nbsp;click okay, pick from the list and it works..but it will prompt me again next time.&amp;nbsp; I can erase and program the target using a P&amp;amp;E Multilink and the P&amp;amp;E tools.&amp;nbsp; The program runs as expected.&amp;nbsp; Howver, when I attempt to program the device using CW and the Multilink cable programming fails.&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Since the part can be programmed using the P&amp;amp;E tools and the P&amp;amp;E cable I have to assume the board design is OK.&amp;nbsp; I believe this is a CW problem either with the setup or with program functionality but I don't know where to look.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Any thoughts?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2008 05:13:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/TBDML-Error/m-p/176404#M1157</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2008-01-04T05:13:11Z</dc:date>
    </item>
    <item>
      <title>Re: TBDML Error</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/TBDML-Error/m-p/176405#M1158</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello Spencer,&lt;BR /&gt;&lt;BR /&gt;The TBDML has no trouble with S12 and does not use a different list of PARTID from the other tool.&lt;BR /&gt;I see two choices for you:&lt;BR /&gt;&lt;BR /&gt;- Check your communications parameters and see if 0x0033 is the right PARTID for the DT/DG256.&lt;BR /&gt;- Ask support from FSL direct because you are a partner...&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Alban.&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Jan 2008 03:06:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/TBDML-Error/m-p/176405#M1158</guid>
      <dc:creator>Nabla69</dc:creator>
      <dc:date>2008-01-09T03:06:51Z</dc:date>
    </item>
  </channel>
</rss>