<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic OSBDM malfuncitions on MCF5482 using CodeWarrior 7.1 in OSBDM and TBDML</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/OSBDM-malfuncitions-on-MCF5482-using-CodeWarrior-7-1/m-p/171263#M1080</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;BR /&gt;&lt;BR /&gt;I met some problems debugging MCF5482 using OSBDM.&lt;BR /&gt;&lt;BR /&gt;My OSBDM works well on both MCF5213 and MCF5228 boards, with functions such as debug, step, breakpoints and download to flash. But when I tried to connect with 5482, the debugger seems run out of control. When I click "step", the PC cursor points to the instruction right above the current instruction, and stepped "back" one instruction at a time. Also, the only way I can enter this debug mode is to select "Stop on...Program Entry Point" on "Debugger Setting" page. Any other settings would lead to no stop on downloading to SRAM.&lt;BR /&gt;&lt;BR /&gt;It's a strange phenomenon and I don't know how to fix it....&lt;BR /&gt;&lt;BR /&gt;The target is built to run in SRAM (the simplest way I think);&lt;/P&gt;&lt;P&gt;the firmware is just a simple program generated from "New Project Wizard";&lt;/P&gt;&lt;P&gt;the CodeWarrior IDE is 7.1.2, with service patch installed;&lt;/P&gt;&lt;P&gt;the firmware version in OSBDM is Build20.1(2009-09-30).(Except that I correct some mistakes on target power monitor and oscillator initialization.)&lt;BR /&gt;&lt;BR /&gt;Does anybody have any suggestions?&lt;BR /&gt;Thank you very much and expecting your reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Li Lei&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 Dec 2010 17:48:03 GMT</pubDate>
    <dc:creator>Stones</dc:creator>
    <dc:date>2010-12-21T17:48:03Z</dc:date>
    <item>
      <title>OSBDM malfuncitions on MCF5482 using CodeWarrior 7.1</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/OSBDM-malfuncitions-on-MCF5482-using-CodeWarrior-7-1/m-p/171263#M1080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All&lt;BR /&gt;&lt;BR /&gt;I met some problems debugging MCF5482 using OSBDM.&lt;BR /&gt;&lt;BR /&gt;My OSBDM works well on both MCF5213 and MCF5228 boards, with functions such as debug, step, breakpoints and download to flash. But when I tried to connect with 5482, the debugger seems run out of control. When I click "step", the PC cursor points to the instruction right above the current instruction, and stepped "back" one instruction at a time. Also, the only way I can enter this debug mode is to select "Stop on...Program Entry Point" on "Debugger Setting" page. Any other settings would lead to no stop on downloading to SRAM.&lt;BR /&gt;&lt;BR /&gt;It's a strange phenomenon and I don't know how to fix it....&lt;BR /&gt;&lt;BR /&gt;The target is built to run in SRAM (the simplest way I think);&lt;/P&gt;&lt;P&gt;the firmware is just a simple program generated from "New Project Wizard";&lt;/P&gt;&lt;P&gt;the CodeWarrior IDE is 7.1.2, with service patch installed;&lt;/P&gt;&lt;P&gt;the firmware version in OSBDM is Build20.1(2009-09-30).(Except that I correct some mistakes on target power monitor and oscillator initialization.)&lt;BR /&gt;&lt;BR /&gt;Does anybody have any suggestions?&lt;BR /&gt;Thank you very much and expecting your reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Li Lei&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Dec 2010 17:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/OSBDM-malfuncitions-on-MCF5482-using-CodeWarrior-7-1/m-p/171263#M1080</guid>
      <dc:creator>Stones</dc:creator>
      <dc:date>2010-12-21T17:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: OSBDM malfuncitions on MCF5482 using CodeWarrior 7.1</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/OSBDM-malfuncitions-on-MCF5482-using-CodeWarrior-7-1/m-p/171264#M1081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No one replies?&lt;/P&gt;&lt;P&gt;Does any body know this problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jan 2011 12:05:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/OSBDM-malfuncitions-on-MCF5482-using-CodeWarrior-7-1/m-p/171264#M1081</guid>
      <dc:creator>Stones</dc:creator>
      <dc:date>2011-01-05T12:05:06Z</dc:date>
    </item>
  </channel>
</rss>