<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックRe: PULL UP missing on the OSBDM ?</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/PULL-UP-missing-on-the-OSBDM/m-p/170229#M1049</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear naej_gz,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Most of the OSBDMs would be programmed using the USB ICP feature that does not require A.1 to be any particular level.&amp;nbsp; As you indicated, the floating pins might interfere with the MON08 interface but this would only be needed if being de-bugged.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by pgo on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-04-08&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;02:24 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Apr 2009 11:22:54 GMT</pubDate>
    <dc:creator>pgo</dc:creator>
    <dc:date>2009-04-08T11:22:54Z</dc:date>
    <item>
      <title>PULL UP missing on the OSBDM ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/PULL-UP-missing-on-the-OSBDM/m-p/170228#M1048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After a reset, the state of PTC1 is unknown. if PTC1 is low, the direction of 1T45 is B to A.&lt;/P&gt;&lt;P&gt;Therefore, the pull up resistor on PTA1 has no effect an the state of PTA1 is unknown.&lt;/P&gt;&lt;P&gt;The chip may be difficult to program using the mon08 connector because of this unknown state of PTA1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;any body has an idea about this ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye Jean&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2009 18:02:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/PULL-UP-missing-on-the-OSBDM/m-p/170228#M1048</guid>
      <dc:creator>naej_gz</dc:creator>
      <dc:date>2009-04-07T18:02:32Z</dc:date>
    </item>
    <item>
      <title>Re: PULL UP missing on the OSBDM ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/PULL-UP-missing-on-the-OSBDM/m-p/170229#M1049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear naej_gz,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Most of the OSBDMs would be programmed using the USB ICP feature that does not require A.1 to be any particular level.&amp;nbsp; As you indicated, the floating pins might interfere with the MON08 interface but this would only be needed if being de-bugged.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV class="message-edit-history"&gt;&lt;SPAN class="edit-author"&gt;Message Edited by pgo on&lt;/SPAN&gt; &lt;SPAN class="local-date"&gt;2009-04-08&lt;/SPAN&gt; &lt;SPAN class="local-time"&gt;02:24 PM&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Apr 2009 11:22:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/PULL-UP-missing-on-the-OSBDM/m-p/170229#M1049</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2009-04-08T11:22:54Z</dc:date>
    </item>
    <item>
      <title>Re: PULL UP missing on the OSBDM ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/PULL-UP-missing-on-the-OSBDM/m-p/170230#M1050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In addition most well designed MON08 adapters would include a pullup within the adapter.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Apr 2009 11:47:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/PULL-UP-missing-on-the-OSBDM/m-p/170230#M1050</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-04-08T11:47:26Z</dc:date>
    </item>
    <item>
      <title>Re: PULL UP missing on the OSBDM ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/PULL-UP-missing-on-the-OSBDM/m-p/170231#M1051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Peg,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The missing pull-up is on C.1 which isn't on the MON08 interface so naej_gz still has a point I think.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Apr 2009 14:15:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/PULL-UP-missing-on-the-OSBDM/m-p/170231#M1051</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2009-04-08T14:15:19Z</dc:date>
    </item>
    <item>
      <title>Re: PULL UP missing on the OSBDM ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/PULL-UP-missing-on-the-OSBDM/m-p/170232#M1052</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yeah, knew I should have looked at the circuit first. (C1 is in a lot of other MON08 interfaces)&lt;/P&gt;&lt;P&gt;Also A1 is a don't care when blank so you can get the initial code in the first time at either level.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I guess things must tend to favour the OK levels here to get it to work.&lt;/P&gt;&lt;P&gt;I know I have re-programmed and debugged many times ( a long time ago) without any issues over the MON08 interface as well as USB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Apr 2009 14:46:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/PULL-UP-missing-on-the-OSBDM/m-p/170232#M1052</guid>
      <dc:creator>peg</dc:creator>
      <dc:date>2009-04-08T14:46:41Z</dc:date>
    </item>
    <item>
      <title>Re: PULL UP missing on the OSBDM ?</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/PULL-UP-missing-on-the-OSBDM/m-p/170233#M1053</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hy&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you accept same probability for every floating input state&amp;nbsp; (i'm not sure of that)&lt;/P&gt;&lt;P&gt;the chance is 1/2 for wrong direction of translator chip (otherwise the pull up on PTA1 works fine), then 1/2 for wrong state of translator input.&lt;/P&gt;&lt;P&gt;therefore the chance is only 1/4 to get a trouble (not entering monitor state)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;may that explain the problem was not seen ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&amp;nbsp;&lt;/P&gt;&lt;P&gt;and thanks for your answers&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Apr 2009 16:13:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/PULL-UP-missing-on-the-OSBDM/m-p/170233#M1053</guid>
      <dc:creator>naej_gz</dc:creator>
      <dc:date>2009-04-08T16:13:36Z</dc:date>
    </item>
  </channel>
</rss>