<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDML中的主题 How do I verify, that the connection to the controller is established</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167161#M1011</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a MC9S12C64CFAE&amp;nbsp;(48 pin package) that i need to program with a .s19 file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a Turbo BDM Light USB debugger.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use Hiwave to program the chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When i press "load application" i the file menu and afterwarts run (F5) i doesn´t get any errors, but if i try to program the chip without i BDM cable connected i doesn´t get any errors aswell.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I verify, that the connection to the controller is established??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can it be a syncronization problem? how should i set my speed in the TBDML menu?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;my chip runs at 8.00MHz and the debugger runs at 12.00MHz, shouldn´t the right ratio&amp;nbsp;be 0.67 ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Martin&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jan 2010 15:31:27 GMT</pubDate>
    <dc:creator>Carmedia</dc:creator>
    <dc:date>2010-01-14T15:31:27Z</dc:date>
    <item>
      <title>How do I verify, that the connection to the controller is established</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167161#M1011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a MC9S12C64CFAE&amp;nbsp;(48 pin package) that i need to program with a .s19 file.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a Turbo BDM Light USB debugger.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I use Hiwave to program the chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When i press "load application" i the file menu and afterwarts run (F5) i doesn´t get any errors, but if i try to program the chip without i BDM cable connected i doesn´t get any errors aswell.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I verify, that the connection to the controller is established??&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can it be a syncronization problem? how should i set my speed in the TBDML menu?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;my chip runs at 8.00MHz and the debugger runs at 12.00MHz, shouldn´t the right ratio&amp;nbsp;be 0.67 ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Martin&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jan 2010 15:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167161#M1011</guid>
      <dc:creator>Carmedia</dc:creator>
      <dc:date>2010-01-14T15:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: How do I verify, that the connection to the controller is established</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167162#M1012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Carmedia,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;That's a bit strange!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the TBDML_HCS12 menu if you select Connect... you should get the "TBDML Setup"&amp;nbsp; dialogue box.&amp;nbsp; It should show a list of (usually one) TBDML device to connect to.&amp;nbsp; If empty it didn't find any TBDMLs.&amp;nbsp; If you don't have the menu it means you need to change the connection (Component-&amp;gt;Set Connection...).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have to admit it doesn't make much of a fan fair if it doesn't connect when there is no BDM.&amp;nbsp; Check the Command Window (usually at bottom right of the screen).&amp;nbsp; It will have a message "No link to target" if it fails to connect.&amp;nbsp; It shouldn't let you debug without a connection!&amp;nbsp; Stepping will result in messages in the same window.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the TBDML fails to connect to the target device there would be multiple error dialogue windows alerting you to the fact.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possilble that you are using the simulator connection i.e. simulating the operation&amp;nbsp; of the device?&amp;nbsp; There aren't many visible differences between this and the hardware debugger i.e. BDM operation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2010 08:35:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167162#M1012</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2010-01-15T08:35:21Z</dc:date>
    </item>
    <item>
      <title>Re: How do I verify, that the connection to the controller is established</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167163#M1013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I doesn´t have a "connect" option im my TBDML menu, but i have a "setup" option, it is set to "TBDML #1" witch is my only option whether the bdm cable is connected or not.&lt;/P&gt;&lt;P&gt;In set connection i have selected "HC12" in processor and "TBDML" in connection.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;when i connect to my debugger i get an error in the command window&amp;nbsp;&lt;/P&gt;&lt;P&gt;Micro Name: MC9S12C64&lt;BR /&gt;GDI:&amp;nbsp;&amp;nbsp; DiDirectCommand(GETNVMFREQUENCY)==&amp;gt; DI_OK&lt;BR /&gt;GDI:&amp;nbsp;&amp;nbsp; DiDirectReadNoWait()==&amp;gt; DI_OK&lt;/P&gt;&lt;P&gt;&lt;FONT color="#00ff00"&gt;FP: Bus speed detection skipped. Now using predefined frequency of 4002779 Hz&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What dos that tell you?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jan 2010 15:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167163#M1013</guid>
      <dc:creator>Carmedia</dc:creator>
      <dc:date>2010-01-15T15:09:12Z</dc:date>
    </item>
    <item>
      <title>Re: How do I verify, that the connection to the controller is established</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167164#M1014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Carmedia,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't believe any of those messages are errors.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The last is just informing you that you have set the 'bus speed' to ~4MHz rather than allowing the BDM to auto-detect the speed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What messages appear when you step through your code?&amp;nbsp; With or without the TBDML connected?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you using hiwave directly or using it with the Codewarrior IDE i.e. creating a project and then starting the debugger (hiwave) from within the IDE?&amp;nbsp; If you&amp;nbsp; are using it directly then I suggest you create a simple project with codewarrior and then use it to test you hardware debugging connection.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Jan 2010 12:50:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167164#M1014</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2010-01-16T12:50:03Z</dc:date>
    </item>
    <item>
      <title>Re: How do I verify, that the connection to the controller is established</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167165#M1015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes i´m using hiwave directly.&lt;/P&gt;&lt;P&gt;If i use hiwave through IDE i get an error&amp;nbsp;saying "Error while loading diagnostics algorithm to target system" then hiwave starts.&lt;/P&gt;&lt;P&gt;I get the same error if i press "flash" in the TBDML menu.&lt;/P&gt;&lt;P&gt;I´ll check if there´s difference between the massages in the commend window&amp;nbsp;with and&amp;nbsp;without the cable connected.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Jan 2010 17:08:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167165#M1015</guid>
      <dc:creator>Carmedia</dc:creator>
      <dc:date>2010-01-16T17:08:45Z</dc:date>
    </item>
    <item>
      <title>Re: How do I verify, that the connection to the controller is established</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167166#M1016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now i have checked if there´s a difference between the command window with and without the cable&amp;nbsp;connected.&lt;/P&gt;&lt;P&gt;There´s not difference at all.&lt;/P&gt;&lt;P&gt;I have attached&amp;nbsp;a copy of the text from the command window.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2010 17:22:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167166#M1016</guid>
      <dc:creator>Carmedia</dc:creator>
      <dc:date>2010-01-18T17:22:51Z</dc:date>
    </item>
    <item>
      <title>Re: How do I verify, that the connection to the controller is established</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167167#M1017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Martin,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Every read of a register or memory is returning zero so it looks like there is no connection.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have you tried unsecuring the chip?&amp;nbsp; This shouldn't be necessary since it is a new chip but worth a try.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Other than that can you check you BDM hardware and connection to the target chip?&amp;nbsp; Do you have a circuit of the BDM? &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some things to check:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Activity on the RESET and BKGD pins on the target.&lt;/P&gt;&lt;P&gt;Activity on the corresponding pins of the JB16 chip in the BDM - both the driver and receiver side.&amp;nbsp; Without a circuit I can't suggest more specific checks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;bye&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Jan 2010 09:53:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167167#M1017</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2010-01-22T09:53:40Z</dc:date>
    </item>
    <item>
      <title>Re: How do I verify, that the connection to the controller is established</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167168#M1018</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have come to the solution that the debugger isn´t working.. and the store where we bourght it isn´t answering you mails... :smileysad:&lt;/P&gt;&lt;P&gt;The solution was that we bought a P&amp;amp;E multilink. And now everything is working :smileyhappy:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2010 21:29:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/How-do-I-verify-that-the-connection-to-the-controller-is/m-p/167168#M1018</guid>
      <dc:creator>Carmedia</dc:creator>
      <dc:date>2010-02-04T21:29:50Z</dc:date>
    </item>
  </channel>
</rss>