<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>OSBDM and TBDMLのトピックConnection problem with CW10.0</title>
    <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Connection-problem-with-CW10-0/m-p/167029#M1006</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have made a hardware implementing jm60OSBDM for HCS08 and CFV1.&lt;/P&gt;&lt;P&gt;With HCS08 It works for CW6.3 but It doesn't work with CW10.0.&lt;/P&gt;&lt;P&gt;I can't download the code to the MCU.&lt;/P&gt;&lt;P&gt;If I set a project to work with both P&amp;amp;E BDM and OSBDM, and at first I use P&amp;amp;E BDM and then OSBDM it works.&lt;/P&gt;&lt;P&gt;But with OSBDM only I can't make it work. I've tried with different firmware and drivers versions.&lt;/P&gt;&lt;P&gt;Has someone had a similar problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Gabriel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 04 Dec 2010 05:33:56 GMT</pubDate>
    <dc:creator>gos_arg</dc:creator>
    <dc:date>2010-12-04T05:33:56Z</dc:date>
    <item>
      <title>Connection problem with CW10.0</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Connection-problem-with-CW10-0/m-p/167029#M1006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have made a hardware implementing jm60OSBDM for HCS08 and CFV1.&lt;/P&gt;&lt;P&gt;With HCS08 It works for CW6.3 but It doesn't work with CW10.0.&lt;/P&gt;&lt;P&gt;I can't download the code to the MCU.&lt;/P&gt;&lt;P&gt;If I set a project to work with both P&amp;amp;E BDM and OSBDM, and at first I use P&amp;amp;E BDM and then OSBDM it works.&lt;/P&gt;&lt;P&gt;But with OSBDM only I can't make it work. I've tried with different firmware and drivers versions.&lt;/P&gt;&lt;P&gt;Has someone had a similar problem?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Gabriel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Dec 2010 05:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Connection-problem-with-CW10-0/m-p/167029#M1006</guid>
      <dc:creator>gos_arg</dc:creator>
      <dc:date>2010-12-04T05:33:56Z</dc:date>
    </item>
    <item>
      <title>Re: Connection problem with CW10.0</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Connection-problem-with-CW10-0/m-p/167030#M1007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Gabriel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I haven't a OSBDM so the following is speculation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The OSBDM requires you to set up a flash programming task to program the chip before debugging or as an auto run task as part of the debugging launch.&amp;nbsp; This is differenty from the P&amp;amp;E BDM or USBDM which do the programming themselves.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it possible that you haven't done this?&amp;nbsp; It would usually be done for you if you made a project targetting OSBDM but you may have set up your project for the P&amp;amp;E BDM initially.&amp;nbsp; This would account for it working AFTER having used the P&amp;amp;E BDM as it would have programmed the chip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bye&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Dec 2010 12:32:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Connection-problem-with-CW10-0/m-p/167030#M1007</guid>
      <dc:creator>pgo</dc:creator>
      <dc:date>2010-12-10T12:32:46Z</dc:date>
    </item>
    <item>
      <title>Re: Connection problem with CW10.0</title>
      <link>https://community.nxp.com/t5/OSBDM-and-TBDML/Connection-problem-with-CW10-0/m-p/167031#M1008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pgo,&lt;/P&gt;&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;When you make a new project for S08 double clicking on ttf file the flash task is set.&lt;/P&gt;&lt;P&gt;After some testing I can say that there is an error message show by the software but the MCU is programmed and debugging could be done.&lt;/P&gt;&lt;P&gt;The situation is not the same for CFV1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Gabriel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Jan 2011 21:37:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/OSBDM-and-TBDML/Connection-problem-with-CW10-0/m-p/167031#M1008</guid>
      <dc:creator>gos_arg</dc:creator>
      <dc:date>2011-01-29T21:37:43Z</dc:date>
    </item>
  </channel>
</rss>