<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>AUTOSAR SW-C中的主题 hw triggering using eMIOS BCTU ADC configuration is not in sync with generad pwm/ timer</title>
    <link>https://community.nxp.com/t5/AUTOSAR-SW-C/hw-triggering-using-eMIOS-BCTU-ADC-configuration-is-not-in-sync/m-p/2295519#M58</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am trying to route the eMIOS_CH_3 -&amp;gt; BCTU -&amp;gt; ADC1 to convert 3 channels P0, P2 and P4 using a CL.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The EMIOS0_CH3 is operating at a frequency of 65kHz, in PWMCB_leaing edge mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Once a trigger is generated the ADC conversion takes around 3 us for completion, however the next trigger to the ADC is initiated after 25us. This does not match the period of the PWM signal which is triggering the ADC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have measured the adc conversion from the trigger enable notification and last conversion notification which comes to around 3us. This is acceptable. However, the BCTU trigger is missing for the next cycle.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Can someone provide any hints on above topic? (I also tried the PWM in OPWMT but the&amp;nbsp; resultss is the same. The frequency of PWM and trigger donot match).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thankyou,&lt;/P&gt;&lt;P&gt;Aditya&lt;/P&gt;</description>
    <pubDate>Sun, 18 Jan 2026 17:34:34 GMT</pubDate>
    <dc:creator>aditya_barve</dc:creator>
    <dc:date>2026-01-18T17:34:34Z</dc:date>
    <item>
      <title>hw triggering using eMIOS BCTU ADC configuration is not in sync with generad pwm/ timer</title>
      <link>https://community.nxp.com/t5/AUTOSAR-SW-C/hw-triggering-using-eMIOS-BCTU-ADC-configuration-is-not-in-sync/m-p/2295519#M58</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am trying to route the eMIOS_CH_3 -&amp;gt; BCTU -&amp;gt; ADC1 to convert 3 channels P0, P2 and P4 using a CL.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The EMIOS0_CH3 is operating at a frequency of 65kHz, in PWMCB_leaing edge mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Once a trigger is generated the ADC conversion takes around 3 us for completion, however the next trigger to the ADC is initiated after 25us. This does not match the period of the PWM signal which is triggering the ADC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have measured the adc conversion from the trigger enable notification and last conversion notification which comes to around 3us. This is acceptable. However, the BCTU trigger is missing for the next cycle.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Can someone provide any hints on above topic? (I also tried the PWM in OPWMT but the&amp;nbsp; resultss is the same. The frequency of PWM and trigger donot match).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thankyou,&lt;/P&gt;&lt;P&gt;Aditya&lt;/P&gt;</description>
      <pubDate>Sun, 18 Jan 2026 17:34:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/AUTOSAR-SW-C/hw-triggering-using-eMIOS-BCTU-ADC-configuration-is-not-in-sync/m-p/2295519#M58</guid>
      <dc:creator>aditya_barve</dc:creator>
      <dc:date>2026-01-18T17:34:34Z</dc:date>
    </item>
  </channel>
</rss>