<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Powertrain and Electrification Analog DriversのトピックMC33816 programming</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33816-programming/m-p/478883#M80</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently working on a project to use the MC33816 driver to control the solenoids of an AMT. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the meantime, I'm trying to establish a simple connection with an Arduino Uno board just to learn about its SPI communication and check its basic functions. However, when I try to check the driver's responses to the write commands I'm sending, or even when I try to read the contents of any address I previously recorded with a specific value, the result is 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The driver's connections I'm using are the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4 SPI pins connected straight to the Arduino SPI.&lt;/P&gt;&lt;P&gt;ResetB pin connected to the 3V3 pin of the Arduino&lt;/P&gt;&lt;P&gt;VCC5 pin connected to the 5V pin of the Arduino&lt;/P&gt;&lt;P&gt;AGND and DGND pins connected together to the Arduino GND pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did not connect the VBATT and the exposed pad pins, because I believe they are not necessary at this phase of my experiments. Also, I do not have an external clock linked to the driver. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please help me finding out what may be the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Feb 2016 00:09:19 GMT</pubDate>
    <dc:creator>ricardovaz</dc:creator>
    <dc:date>2016-02-01T00:09:19Z</dc:date>
    <item>
      <title>MC33816 programming</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33816-programming/m-p/478883#M80</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently working on a project to use the MC33816 driver to control the solenoids of an AMT. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the meantime, I'm trying to establish a simple connection with an Arduino Uno board just to learn about its SPI communication and check its basic functions. However, when I try to check the driver's responses to the write commands I'm sending, or even when I try to read the contents of any address I previously recorded with a specific value, the result is 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The driver's connections I'm using are the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4 SPI pins connected straight to the Arduino SPI.&lt;/P&gt;&lt;P&gt;ResetB pin connected to the 3V3 pin of the Arduino&lt;/P&gt;&lt;P&gt;VCC5 pin connected to the 5V pin of the Arduino&lt;/P&gt;&lt;P&gt;AGND and DGND pins connected together to the Arduino GND pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did not connect the VBATT and the exposed pad pins, because I believe they are not necessary at this phase of my experiments. Also, I do not have an external clock linked to the driver. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please help me finding out what may be the problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Feb 2016 00:09:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33816-programming/m-p/478883#M80</guid>
      <dc:creator>ricardovaz</dc:creator>
      <dc:date>2016-02-01T00:09:19Z</dc:date>
    </item>
  </channel>
</rss>