<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Merging 2 different sdk samples in Powertrain and Electrification Analog Drivers</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/Merging-2-different-sdk-samples/m-p/2132493#M738</link>
    <description>&lt;P&gt;Im doing a PMSM control and im using a&amp;nbsp;&lt;STRONG&gt;&lt;EM&gt;FRDM-MCXN947&lt;SPAN&gt;&amp;nbsp; ,&amp;nbsp;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/STRONG&gt;&lt;SPAN&gt;so im willing to do the motoro control with AI but i have the motor control sample and ai sample. I dont have idea if i can merge two different sdk samples in the same project and make it work in the card as the same project. Also about the PSMS sdk example the FreeMASTER programm is capable of create a database to train the AI ML model.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 11 Jul 2025 11:18:09 GMT</pubDate>
    <dc:creator>Asimoes</dc:creator>
    <dc:date>2025-07-11T11:18:09Z</dc:date>
    <item>
      <title>Merging 2 different sdk samples</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/Merging-2-different-sdk-samples/m-p/2132493#M738</link>
      <description>&lt;P&gt;Im doing a PMSM control and im using a&amp;nbsp;&lt;STRONG&gt;&lt;EM&gt;FRDM-MCXN947&lt;SPAN&gt;&amp;nbsp; ,&amp;nbsp;&lt;/SPAN&gt;&lt;/EM&gt;&lt;/STRONG&gt;&lt;SPAN&gt;so im willing to do the motoro control with AI but i have the motor control sample and ai sample. I dont have idea if i can merge two different sdk samples in the same project and make it work in the card as the same project. Also about the PSMS sdk example the FreeMASTER programm is capable of create a database to train the AI ML model.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jul 2025 11:18:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/Merging-2-different-sdk-samples/m-p/2132493#M738</guid>
      <dc:creator>Asimoes</dc:creator>
      <dc:date>2025-07-11T11:18:09Z</dc:date>
    </item>
    <item>
      <title>Re: Merging 2 different sdk samples</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/Merging-2-different-sdk-samples/m-p/2132715#M739</link>
      <description>&lt;P&gt;Hello Asimoes&lt;/P&gt;
&lt;P&gt;In this part of the community we provide support to other PNs, I recommend that you go to &lt;A href="https://community.nxp.com/t5/MCX-Microcontrollers/bd-p/MCX" target="_blank"&gt;MCX Microcontrollers&lt;/A&gt;, so that my colleagues can see your case and help you.&lt;/P&gt;
&lt;P&gt;Enjoy your weekend&lt;/P&gt;
&lt;P&gt;Have a great day and best of luck.&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jul 2025 23:14:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/Merging-2-different-sdk-samples/m-p/2132715#M739</guid>
      <dc:creator>RafaR</dc:creator>
      <dc:date>2025-07-11T23:14:52Z</dc:date>
    </item>
  </channel>
</rss>