<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Sample code for gate driver MC33GD3100 in Powertrain and Electrification Analog Drivers</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/Sample-code-for-gate-driver-MC33GD3100/m-p/2086656#M711</link>
    <description>&lt;P&gt;We are considering the use of gate driver &lt;LI-PRODUCT title="GD3100" id="GD3100"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;with the S32K3 for automotive application. I searched for a sample code of the firmware driver for the GD3100, but could not find it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please link to me any sample code for the same? preferably on the s32k but if not available then on other MCU is also ok.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Thu, 24 Apr 2025 13:42:04 GMT</pubDate>
    <dc:creator>punekar</dc:creator>
    <dc:date>2025-04-24T13:42:04Z</dc:date>
    <item>
      <title>Sample code for gate driver MC33GD3100</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/Sample-code-for-gate-driver-MC33GD3100/m-p/2086656#M711</link>
      <description>&lt;P&gt;We are considering the use of gate driver &lt;LI-PRODUCT title="GD3100" id="GD3100"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;with the S32K3 for automotive application. I searched for a sample code of the firmware driver for the GD3100, but could not find it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please link to me any sample code for the same? preferably on the s32k but if not available then on other MCU is also ok.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 24 Apr 2025 13:42:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/Sample-code-for-gate-driver-MC33GD3100/m-p/2086656#M711</guid>
      <dc:creator>punekar</dc:creator>
      <dc:date>2025-04-24T13:42:04Z</dc:date>
    </item>
    <item>
      <title>Re: Sample code for gate driver MC33GD3100</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/Sample-code-for-gate-driver-MC33GD3100/m-p/2086681#M712</link>
      <description>&lt;P&gt;Hi Sanket,&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;What we can provide is the&amp;nbsp;GD31xx Driver Example Code, you can download it from the GD3160 website:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://www.nxp.com/products/GD3160" target="_blank"&gt;https://www.nxp.com/products/GD3160&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2025-04-24 162454.png" style="width: 928px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/334767iE5519E0E8ED7BA74/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot 2025-04-24 162454.png" alt="Screenshot 2025-04-24 162454.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot 2025-04-24 162454.png&lt;/span&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The GD31xx.c file&amp;nbsp;contains the GD31xx device driver functions.&amp;nbsp;They consist of SPI access, initialization and register configuration functions. There is also a sample interrupt service routine for&amp;nbsp;monitoring the INTB signal from the GD31xx.&amp;nbsp;All low-level SPI transmit and receive functions are written for the MCP5777C MCU. These functions will have to be changed if you are using a different MCU from the S32K3 family.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BRs, Tomas&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Apr 2025 14:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/Sample-code-for-gate-driver-MC33GD3100/m-p/2086681#M712</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2025-04-24T14:32:04Z</dc:date>
    </item>
  </channel>
</rss>