<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Powertrain and Electrification Analog Drivers中的主题 BATTERY MANAGEMENT SYSTEM</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/BATTERY-MANAGEMENT-SYSTEM/m-p/2074264#M699</link>
    <description>&lt;P&gt;i am working on making a bms for fsae electrical vehicle&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i require 13 gpio pins in the cell monitoring unit for temperature monitoring&amp;nbsp; but in MC33774 only 8 GPIOs pins are present so is there a way to increase number of&amp;nbsp; GPIO pins by using some ic or by using two MC33774 ics together also if i use a centralized thermistor expansion module would it be able to communicate with s32k3 or will there be any problem&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 04 Apr 2025 12:29:52 GMT</pubDate>
    <dc:creator>rj2025</dc:creator>
    <dc:date>2025-04-04T12:29:52Z</dc:date>
    <item>
      <title>BATTERY MANAGEMENT SYSTEM</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/BATTERY-MANAGEMENT-SYSTEM/m-p/2074264#M699</link>
      <description>&lt;P&gt;i am working on making a bms for fsae electrical vehicle&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i require 13 gpio pins in the cell monitoring unit for temperature monitoring&amp;nbsp; but in MC33774 only 8 GPIOs pins are present so is there a way to increase number of&amp;nbsp; GPIO pins by using some ic or by using two MC33774 ics together also if i use a centralized thermistor expansion module would it be able to communicate with s32k3 or will there be any problem&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Apr 2025 12:29:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/BATTERY-MANAGEMENT-SYSTEM/m-p/2074264#M699</guid>
      <dc:creator>rj2025</dc:creator>
      <dc:date>2025-04-04T12:29:52Z</dc:date>
    </item>
    <item>
      <title>Re: BATTERY MANAGEMENT SYSTEM</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/BATTERY-MANAGEMENT-SYSTEM/m-p/2076438#M700</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes, you can use multiple MC33774 ICs in the same BMS chain or you can check our GPIO Expanders:&amp;nbsp;&lt;A href="https://www.nxp.com/products/interfaces/ic-spi-i3c-interface-devices/general-purpose-i-o-gpio:MC_41850" target="_blank"&gt;https://www.nxp.com/products/interfaces/ic-spi-i3c-interface-devices/general-purpose-i-o-gpio:MC_41850&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Apr 2025 19:02:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/BATTERY-MANAGEMENT-SYSTEM/m-p/2076438#M700</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2025-04-08T19:02:01Z</dc:date>
    </item>
  </channel>
</rss>