<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Powertrain and Electrification Analog Drivers中的主题 Re: About MC33PT2000 not use self DC-DC boost voltage functionality</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/About-MC33PT2000-not-use-self-DC-DC-boost-voltage-functionality/m-p/2054415#M685</link>
    <description>Thanks very much!!</description>
    <pubDate>Mon, 03 Mar 2025 06:13:32 GMT</pubDate>
    <dc:creator>Borden</dc:creator>
    <dc:date>2025-03-03T06:13:32Z</dc:date>
    <item>
      <title>About MC33PT2000 not use self DC-DC boost voltage functionality</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/About-MC33PT2000-not-use-self-DC-DC-boost-voltage-functionality/m-p/2050552#M681</link>
      <description>&lt;P&gt;Dear NXP team:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;SPAN&gt;For the 3-cylinder injection, if the DC-DC Vboost voltage (65V) is generated using an external circuit instead of the built-in functionality of this chip, how should the registers and code be set?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Feb 2025 06:39:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/About-MC33PT2000-not-use-self-DC-DC-boost-voltage-functionality/m-p/2050552#M681</guid>
      <dc:creator>Borden</dc:creator>
      <dc:date>2025-02-25T06:39:31Z</dc:date>
    </item>
    <item>
      <title>Re: About MC33PT2000 not use self DC-DC boost voltage functionality</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/About-MC33PT2000-not-use-self-DC-DC-boost-voltage-functionality/m-p/2052644#M684</link>
      <description>&lt;P&gt;HI Borden&lt;/P&gt;
&lt;P&gt;You can refer to below datasheet page38:&lt;/P&gt;
&lt;P&gt;Application without boost voltage&lt;BR /&gt;For this purpose, it is possible to change the internal voltage divider ratio from 1/32 to 1/4 by setting the signal boost_mon_en high. To &lt;BR /&gt;detect undervoltage and use the signal uv_vboost to disable the pre-drivers, the uv_vboost bit needs to be set to “1” (refer to Table 162, &lt;BR /&gt;driver_status (1B2h)). The uv_vboost signal goes high as soon as the voltage at the VBOOST pin is below the threshold, if the VBOOST&lt;BR /&gt;UV monitor is enabled (Vboost_disable_en = 1).&lt;BR /&gt;The same digital filter used for the VBOOST voltage measurement is also used for the VBOOST UV monitoring mode. The DAC set point &lt;BR /&gt;value in this mode has to be chosen to fulfill two requirements:&lt;BR /&gt;• The pre-drivers must not be disabled at a battery voltage above 5.0 V &lt;BR /&gt;• The device internal charge pump only works properly down to a battery voltage of 4.7 V&lt;BR /&gt;The VBOOST UV threshold can be calculated using the following formula. &lt;BR /&gt;• VBOOST = (DAC_VALUE * 39.1 mV)&lt;/P&gt;</description>
      <pubDate>Thu, 27 Feb 2025 06:56:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/About-MC33PT2000-not-use-self-DC-DC-boost-voltage-functionality/m-p/2052644#M684</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2025-02-27T06:56:23Z</dc:date>
    </item>
    <item>
      <title>Re: About MC33PT2000 not use self DC-DC boost voltage functionality</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/About-MC33PT2000-not-use-self-DC-DC-boost-voltage-functionality/m-p/2054415#M685</link>
      <description>Thanks very much!!</description>
      <pubDate>Mon, 03 Mar 2025 06:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/About-MC33PT2000-not-use-self-DC-DC-boost-voltage-functionality/m-p/2054415#M685</guid>
      <dc:creator>Borden</dc:creator>
      <dc:date>2025-03-03T06:13:32Z</dc:date>
    </item>
  </channel>
</rss>