<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Powertrain and Electrification Analog DriversのトピックRe: PCA9450 Absolute Maximum Ratings</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/PCA9450-Absolute-Maximum-Ratings/m-p/1968210#M604</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am very sorry, but I made a mistake with the item number listed on the datasheet, so please let me check again.&lt;BR /&gt;The limit value of "LX4, LX5" Max = "INB45 + 0.5V" listed in Table 70 of the PCA9450 datasheet applies only under normal operating conditions (VSYS = INB45 = 2.7 to 5.5V), so is it correct to think that it is invalid when the input voltage transitions from ON to OFF?&lt;BR /&gt;This is because I believe that this is unavoidable, as residual voltage will remain on the output pins "LX4, LX5" due to the load capacitor even when the input voltage is turned OFF.&lt;/P&gt;&lt;P&gt;Best Regard.&lt;/P&gt;</description>
    <pubDate>Mon, 07 Oct 2024 23:11:05 GMT</pubDate>
    <dc:creator>kouichinakahash</dc:creator>
    <dc:date>2024-10-07T23:11:05Z</dc:date>
    <item>
      <title>PCA9450 Absolute Maximum Ratings</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/PCA9450-Absolute-Maximum-Ratings/m-p/1967857#M600</link>
      <description>&lt;P&gt;The LX5 pin MAX in PCA9450AA datasheet 7.1 Absolute Maximum Ratings states "INB45 + 0.5V", but this may be exceeded due to the voltage charged in the external capacitor, such as when the power is turned from ON to OFF. Is it correct to assume that this regulation applies only when the Input voltage is normal (VSYS=INB45=2.7 to 5.5V)?&lt;/P&gt;</description>
      <pubDate>Mon, 07 Oct 2024 11:41:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/PCA9450-Absolute-Maximum-Ratings/m-p/1967857#M600</guid>
      <dc:creator>kouichinakahash</dc:creator>
      <dc:date>2024-10-07T11:41:51Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9450 Absolute Maximum Ratings</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/PCA9450-Absolute-Maximum-Ratings/m-p/1967871#M601</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;P&gt;Hello,&lt;BR /&gt;Yes, the “INB45 + 0.5V” regulation for the LX5 pin in the PCA9450AA datasheet applies under normal operating conditions (VSYS=INB45=2.7 to 5.5V). Exceeding this limit due to external capacitor voltage during power transitions could potentially damage the device12. Ensure proper design to avoid such scenarios.&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Gary Byers&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Mon, 07 Oct 2024 12:15:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/PCA9450-Absolute-Maximum-Ratings/m-p/1967871#M601</guid>
      <dc:creator>gary598byers</dc:creator>
      <dc:date>2024-10-07T12:15:07Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9450 Absolute Maximum Ratings</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/PCA9450-Absolute-Maximum-Ratings/m-p/1968210#M604</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am very sorry, but I made a mistake with the item number listed on the datasheet, so please let me check again.&lt;BR /&gt;The limit value of "LX4, LX5" Max = "INB45 + 0.5V" listed in Table 70 of the PCA9450 datasheet applies only under normal operating conditions (VSYS = INB45 = 2.7 to 5.5V), so is it correct to think that it is invalid when the input voltage transitions from ON to OFF?&lt;BR /&gt;This is because I believe that this is unavoidable, as residual voltage will remain on the output pins "LX4, LX5" due to the load capacitor even when the input voltage is turned OFF.&lt;/P&gt;&lt;P&gt;Best Regard.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Oct 2024 23:11:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/PCA9450-Absolute-Maximum-Ratings/m-p/1968210#M604</guid>
      <dc:creator>kouichinakahash</dc:creator>
      <dc:date>2024-10-07T23:11:05Z</dc:date>
    </item>
  </channel>
</rss>