<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PT200xHM measurement function, no voltage in Powertrain and Electrification Analog Drivers</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/PT200xHM-measurement-function-no-voltage/m-p/1909905#M536</link>
    <description>&lt;P&gt;With OA feature, I can not setup for voltage setting.&lt;/P&gt;&lt;P&gt;I write to:&lt;/P&gt;&lt;P&gt;1AAh = 426d&lt;BR /&gt;b6=oa1_g1 b5-3= oa_sel1 b2-1=oa1_gain b0=oa1_en&lt;BR /&gt;0000 000 0001 0001 0x0011&lt;BR /&gt;'000': output from current measurement block 1&lt;BR /&gt;'001': output from current measurement block 3&lt;BR /&gt;'010': OA_Meas1: output from measurement function, unprocessed signal&lt;BR /&gt;'011': OA_Meas2: output from measurement function, low-pass + high-pass filtering&lt;BR /&gt;'100': OA_Meas3: output from measurement function, LP + two times HP filtering&lt;BR /&gt;'101': 2.5 Volt&lt;BR /&gt;'110': OA_Meas4: output from measurement function, low-pass filtering&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;meas_func1 register (1ACh)&lt;BR /&gt;reserved b12-9= dac_fb_sel b8=cur_volt0, b7-5 =d_ls_sel b4-2=s_hs_sel b1-0 oa_cur&lt;BR /&gt;000 0000 0 001/.010 0.01 00 = 0044h HS2 - LS1&lt;/P&gt;&lt;P&gt;meas_func2 register (1ADh)&lt;BR /&gt;b15=offset_hp2_sel, b14=offset_hp1_sel, b13-10=fc_hp2_sel, b9-7=gain_hp1_sel b6-3=fcut_hp1_sel b2-1=volt_att&lt;BR /&gt;xxxx xxxx xxxx x000=0 Unfiltered div by 30&lt;/P&gt;&lt;P&gt;Scope shows flat line at 0V&lt;/P&gt;&lt;P&gt;Yes it has M in part name.&lt;/P&gt;&lt;P&gt;What have I missed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 16 Jul 2024 16:43:54 GMT</pubDate>
    <dc:creator>Fast</dc:creator>
    <dc:date>2024-07-16T16:43:54Z</dc:date>
    <item>
      <title>PT200xHM measurement function, no voltage</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/PT200xHM-measurement-function-no-voltage/m-p/1909905#M536</link>
      <description>&lt;P&gt;With OA feature, I can not setup for voltage setting.&lt;/P&gt;&lt;P&gt;I write to:&lt;/P&gt;&lt;P&gt;1AAh = 426d&lt;BR /&gt;b6=oa1_g1 b5-3= oa_sel1 b2-1=oa1_gain b0=oa1_en&lt;BR /&gt;0000 000 0001 0001 0x0011&lt;BR /&gt;'000': output from current measurement block 1&lt;BR /&gt;'001': output from current measurement block 3&lt;BR /&gt;'010': OA_Meas1: output from measurement function, unprocessed signal&lt;BR /&gt;'011': OA_Meas2: output from measurement function, low-pass + high-pass filtering&lt;BR /&gt;'100': OA_Meas3: output from measurement function, LP + two times HP filtering&lt;BR /&gt;'101': 2.5 Volt&lt;BR /&gt;'110': OA_Meas4: output from measurement function, low-pass filtering&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;meas_func1 register (1ACh)&lt;BR /&gt;reserved b12-9= dac_fb_sel b8=cur_volt0, b7-5 =d_ls_sel b4-2=s_hs_sel b1-0 oa_cur&lt;BR /&gt;000 0000 0 001/.010 0.01 00 = 0044h HS2 - LS1&lt;/P&gt;&lt;P&gt;meas_func2 register (1ADh)&lt;BR /&gt;b15=offset_hp2_sel, b14=offset_hp1_sel, b13-10=fc_hp2_sel, b9-7=gain_hp1_sel b6-3=fcut_hp1_sel b2-1=volt_att&lt;BR /&gt;xxxx xxxx xxxx x000=0 Unfiltered div by 30&lt;/P&gt;&lt;P&gt;Scope shows flat line at 0V&lt;/P&gt;&lt;P&gt;Yes it has M in part name.&lt;/P&gt;&lt;P&gt;What have I missed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jul 2024 16:43:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/PT200xHM-measurement-function-no-voltage/m-p/1909905#M536</guid>
      <dc:creator>Fast</dc:creator>
      <dc:date>2024-07-16T16:43:54Z</dc:date>
    </item>
    <item>
      <title>Re: PT200xHM measurement function, no voltage</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/PT200xHM-measurement-function-no-voltage/m-p/1914218#M542</link>
      <description>&lt;P&gt;Yes it does work. Nice rest over weekend.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jul 2024 14:32:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/PT200xHM-measurement-function-no-voltage/m-p/1914218#M542</guid>
      <dc:creator>Fast</dc:creator>
      <dc:date>2024-07-22T14:32:44Z</dc:date>
    </item>
  </channel>
</rss>