<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Powertrain and Electrification Analog DriversのトピックMC33HB2001 - Internal Pullups</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2001-Internal-Pullups/m-p/1622661#M370</link>
    <description>&lt;P&gt;The datasheet indicates that the MC33HB2001 has internal pullups to 5V and I am questioning if this is correct when VDDQ of 3.3V is applied:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="deckhardt_0-1679926371006.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/216424iAB25B1D4C9443E93/image-size/medium?v=v2&amp;amp;px=400" role="button" title="deckhardt_0-1679926371006.png" alt="deckhardt_0-1679926371006.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;deckhardt_0-1679926371006.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;When looking at the development board FRDM-HB2001FEVM it looks like you can connect VRDM_VDD to VDD and VDD to VDDQ.&lt;BR /&gt;&lt;BR /&gt;Could someone confirm if these internal pullups are to VDDQ or is there an internal 5V regulator?&lt;/P&gt;</description>
    <pubDate>Mon, 27 Mar 2023 14:21:02 GMT</pubDate>
    <dc:creator>deckhardt</dc:creator>
    <dc:date>2023-03-27T14:21:02Z</dc:date>
    <item>
      <title>MC33HB2001 - Internal Pullups</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2001-Internal-Pullups/m-p/1622661#M370</link>
      <description>&lt;P&gt;The datasheet indicates that the MC33HB2001 has internal pullups to 5V and I am questioning if this is correct when VDDQ of 3.3V is applied:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="deckhardt_0-1679926371006.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/216424iAB25B1D4C9443E93/image-size/medium?v=v2&amp;amp;px=400" role="button" title="deckhardt_0-1679926371006.png" alt="deckhardt_0-1679926371006.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;deckhardt_0-1679926371006.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;When looking at the development board FRDM-HB2001FEVM it looks like you can connect VRDM_VDD to VDD and VDD to VDDQ.&lt;BR /&gt;&lt;BR /&gt;Could someone confirm if these internal pullups are to VDDQ or is there an internal 5V regulator?&lt;/P&gt;</description>
      <pubDate>Mon, 27 Mar 2023 14:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2001-Internal-Pullups/m-p/1622661#M370</guid>
      <dc:creator>deckhardt</dc:creator>
      <dc:date>2023-03-27T14:21:02Z</dc:date>
    </item>
    <item>
      <title>Re: MC33HB2001 - Internal Pullups</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2001-Internal-Pullups/m-p/1623084#M372</link>
      <description>&lt;P&gt;Hi David,&lt;/P&gt;
&lt;P&gt;The pull-up level is dependent upon the voltage level applied to VDDQ. If 3.3V is applied on VDDQ, the internal pull-ups will be to 3.3V for these logic pins. I think the spec is referring to a 5.0V applied to VDDQ scenario.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Tue, 28 Mar 2023 07:01:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2001-Internal-Pullups/m-p/1623084#M372</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2023-03-28T07:01:16Z</dc:date>
    </item>
    <item>
      <title>Re: MC33HB2001 - Internal Pullups</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2001-Internal-Pullups/m-p/1636414#M377</link>
      <description>&lt;P&gt;I have laid out a development board using the&amp;nbsp;MC33HB2001FKR2. I supplied 12V to VPWR (pins 12,13,29,30) and 3.3V to VDDQ (pin 1) and CS_B (pin 32) measures to be 0V. According to the datasheet the CS_B pin should be internally pulled up. Can you confirm or deny? I confirm the same behavior on the NXP development board FRDM-HB2001FEVM.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Apr 2023 17:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2001-Internal-Pullups/m-p/1636414#M377</guid>
      <dc:creator>deckhardt</dc:creator>
      <dc:date>2023-04-19T17:18:56Z</dc:date>
    </item>
    <item>
      <title>Re: MC33HB2001 - Internal Pullups</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2001-Internal-Pullups/m-p/1637740#M378</link>
      <description>&lt;P&gt;Hi David,&lt;/P&gt;
&lt;P&gt;Yes, CS_B has an internal weak pull-up to VDDQ. The FRDM-HB2001FEVM development board drives the SPI signals at 3.3V. The MCU should not be holding the CS_B pin low while data is not being transmitted.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Fri, 21 Apr 2023 06:16:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2001-Internal-Pullups/m-p/1637740#M378</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2023-04-21T06:16:59Z</dc:date>
    </item>
  </channel>
</rss>