<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Powertrain and Electrification Analog DriversのトピックRe: MC33HB2000 SPI communication error</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2000-SPI-communication-error/m-p/1622094#M369</link>
    <description>&lt;P&gt;Dear Anderson.&lt;/P&gt;&lt;P&gt;The reason for using the damping resistor was added due to EMC CE current NG.&lt;BR /&gt;I need to use a damping resistor for the SCLK line. Is there a way to determine the application range of the damping resistor because the following problem has occurred?&lt;BR /&gt;And why does the error appear when 1kohm is applied?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Mon, 27 Mar 2023 00:26:34 GMT</pubDate>
    <dc:creator>hyjung</dc:creator>
    <dc:date>2023-03-27T00:26:34Z</dc:date>
    <item>
      <title>MC33HB2000 SPI communication error</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2000-SPI-communication-error/m-p/1621490#M367</link>
      <description>&lt;P&gt;Dear all.&lt;/P&gt;&lt;P&gt;I send detailed waveform data regarding whether or not a damping resistor 1kohm is inserted in SPI line&amp;nbsp; between the MCU and the MC33HB2000.&lt;/P&gt;&lt;P&gt;test condition)&lt;/P&gt;&lt;P&gt;When waking up from sleep, it operates for 15 seconds after initializing for 100 ms&lt;/P&gt;&lt;P&gt;SPI freq. 500 kHz, Motor current 1.5A max.&lt;/P&gt;&lt;P&gt;What is the reason for the difference caused by the presence or absence of the damping resistance of the SLK line?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Mar 2023 07:48:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2000-SPI-communication-error/m-p/1621490#M367</guid>
      <dc:creator>hyjung</dc:creator>
      <dc:date>2023-03-24T07:48:50Z</dc:date>
    </item>
    <item>
      <title>Re: MC33HB2000 SPI communication error</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2000-SPI-communication-error/m-p/1621906#M368</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Not understanding question. The want to use damping resistor on SCLK line? 1kohm seems quite large.&lt;/P&gt;
&lt;P&gt;Wayne&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Mar 2023 20:36:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2000-SPI-communication-error/m-p/1621906#M368</guid>
      <dc:creator>Wayne_Anderson</dc:creator>
      <dc:date>2023-03-24T20:36:25Z</dc:date>
    </item>
    <item>
      <title>Re: MC33HB2000 SPI communication error</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2000-SPI-communication-error/m-p/1622094#M369</link>
      <description>&lt;P&gt;Dear Anderson.&lt;/P&gt;&lt;P&gt;The reason for using the damping resistor was added due to EMC CE current NG.&lt;BR /&gt;I need to use a damping resistor for the SCLK line. Is there a way to determine the application range of the damping resistor because the following problem has occurred?&lt;BR /&gt;And why does the error appear when 1kohm is applied?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Mar 2023 00:26:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2000-SPI-communication-error/m-p/1622094#M369</guid>
      <dc:creator>hyjung</dc:creator>
      <dc:date>2023-03-27T00:26:34Z</dc:date>
    </item>
    <item>
      <title>Re: MC33HB2000 SPI communication error</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2000-SPI-communication-error/m-p/1622756#M371</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Ensure you have adequate hold time. SCLK falling edge to MOSI requires a minimum 30ns hold timing.&lt;/P&gt;</description>
      <pubDate>Mon, 27 Mar 2023 17:41:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2000-SPI-communication-error/m-p/1622756#M371</guid>
      <dc:creator>Wayne_Anderson</dc:creator>
      <dc:date>2023-03-27T17:41:11Z</dc:date>
    </item>
    <item>
      <title>Re: MC33HB2000 SPI communication error</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2000-SPI-communication-error/m-p/1626484#M373</link>
      <description>&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;If MOSI fails to reach the hold time, does MISO send an error?&lt;BR /&gt;What I do not understand is why MISO sends an error even though it is not actually an error in the motor driver.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Apr 2023 01:14:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2000-SPI-communication-error/m-p/1626484#M373</guid>
      <dc:creator>hyjung</dc:creator>
      <dc:date>2023-04-03T01:14:28Z</dc:date>
    </item>
    <item>
      <title>Re: MC33HB2000 SPI communication error</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2000-SPI-communication-error/m-p/1627027#M374</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;What is the error you are detecting in the status register? Are you getting a SPI framing error? If the number of clock pulses within CS_B low is not more than 0 and an integer multiple of 16, the current SPI communication is ignored and a framing error is recorded in the status register. Do you have inadvertent Chip Select going low?&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Apr 2023 17:33:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33HB2000-SPI-communication-error/m-p/1627027#M374</guid>
      <dc:creator>Wayne_Anderson</dc:creator>
      <dc:date>2023-04-03T17:33:52Z</dc:date>
    </item>
  </channel>
</rss>