<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Powertrain and Electrification Analog Drivers中的主题 a problem about using Labview to control MC33816</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/a-problem-about-using-Labview-to-control-MC33816/m-p/1497847#M328</link>
    <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I'm new to KIT33816. Now I want to make an upper computer on Labview to control MC33816's valve in Dram and it's injection. However there are some questions I can't solve:&lt;/P&gt;&lt;P&gt;1:When I connected the board to computer,&amp;nbsp; the&amp;nbsp;Communication port didn't response. Visa can't find the&amp;nbsp;Communication port.&lt;/P&gt;&lt;P&gt;2:How should I give the board a signal so KIT33816 can receive the data or start to inject in Labview without SPIGen?&lt;/P&gt;&lt;P&gt;3:How can I load the address of Dram in spi_add register since it only has 8 bit?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 29 Jul 2022 07:50:14 GMT</pubDate>
    <dc:creator>huuuh</dc:creator>
    <dc:date>2022-07-29T07:50:14Z</dc:date>
    <item>
      <title>a problem about using Labview to control MC33816</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/a-problem-about-using-Labview-to-control-MC33816/m-p/1497847#M328</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I'm new to KIT33816. Now I want to make an upper computer on Labview to control MC33816's valve in Dram and it's injection. However there are some questions I can't solve:&lt;/P&gt;&lt;P&gt;1:When I connected the board to computer,&amp;nbsp; the&amp;nbsp;Communication port didn't response. Visa can't find the&amp;nbsp;Communication port.&lt;/P&gt;&lt;P&gt;2:How should I give the board a signal so KIT33816 can receive the data or start to inject in Labview without SPIGen?&lt;/P&gt;&lt;P&gt;3:How can I load the address of Dram in spi_add register since it only has 8 bit?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Jul 2022 07:50:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/a-problem-about-using-Labview-to-control-MC33816/m-p/1497847#M328</guid>
      <dc:creator>huuuh</dc:creator>
      <dc:date>2022-07-29T07:50:14Z</dc:date>
    </item>
  </channel>
</rss>