<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Powertrain and Electrification Analog Drivers中的主题 Re: MC33GD3000 Power dissipation profiles</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33GD3000-Power-dissipation-profiles/m-p/1496316#M326</link>
    <description>&lt;P&gt;Hi Tom,&lt;/P&gt;
&lt;P&gt;You are right, it should be given in watts.&lt;/P&gt;
&lt;P&gt;Thank you for pointing that out, we will correct it in the next datasheet revision.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
    <pubDate>Wed, 27 Jul 2022 10:27:49 GMT</pubDate>
    <dc:creator>TomasVaverka</dc:creator>
    <dc:date>2022-07-27T10:27:49Z</dc:date>
    <item>
      <title>MC33GD3000 Power dissipation profiles</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33GD3000-Power-dissipation-profiles/m-p/1496243#M325</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a question related to the figure about the power dissipation of the MC33GD3000 shown in the datasheet:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="image.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/188026iDD569C7010BE3631/image-size/large?v=v2&amp;amp;px=999" role="button" title="image.png" alt="image.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Is it right, that the power dissipation is given in ohms or should it be given in watts?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 08:41:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33GD3000-Power-dissipation-profiles/m-p/1496243#M325</guid>
      <dc:creator>TomLightning</dc:creator>
      <dc:date>2022-07-27T08:41:20Z</dc:date>
    </item>
    <item>
      <title>Re: MC33GD3000 Power dissipation profiles</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33GD3000-Power-dissipation-profiles/m-p/1496316#M326</link>
      <description>&lt;P&gt;Hi Tom,&lt;/P&gt;
&lt;P&gt;You are right, it should be given in watts.&lt;/P&gt;
&lt;P&gt;Thank you for pointing that out, we will correct it in the next datasheet revision.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 10:27:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33GD3000-Power-dissipation-profiles/m-p/1496316#M326</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2022-07-27T10:27:49Z</dc:date>
    </item>
    <item>
      <title>Re: MC33GD3000 Power dissipation profiles</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33GD3000-Power-dissipation-profiles/m-p/1496403#M327</link>
      <description>&lt;P&gt;Okay, that makes more sense. The thermal resistance from the exposed pad to the junction (internal chip structure) is give with 3°C/W acc. datasheet. Let's assume that the ground plane which is directly connected to the exposed pad has a temperature of +125°C. Is the assumption right, that my junction temperature would only increase about approx. 3°C at 1W power dissipation? I'm trying to find out if I could get a thermal problem when operating the MC33GD3000 with the battery supply.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;</description>
      <pubDate>Wed, 27 Jul 2022 12:59:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/MC33GD3000-Power-dissipation-profiles/m-p/1496403#M327</guid>
      <dc:creator>TomLightning</dc:creator>
      <dc:date>2022-07-27T12:59:58Z</dc:date>
    </item>
  </channel>
</rss>