<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Powertrain and Electrification Analog DriversのトピックRe: Trouble with PT2001</title>
    <link>https://community.nxp.com/t5/Powertrain-and-Electrification/Trouble-with-PT2001/m-p/1484206#M315</link>
    <description>&lt;P&gt;I have now tried to build the example project in the S32-DS environment. For this I tried it with S32-DS Platform 3.4 and S32-DS ARM V 2.2 with many compiler errors. Therefore I tried it with S32DS.ARM.2018 R.1 environment and I still get these following 2 errors and can't fix them.&lt;/P&gt;&lt;P&gt;Furthermore as requested I am sending a picture of the PT2001 chip so that the manufacturing date can be seen.&lt;/P&gt;&lt;P&gt;Is there any other current example project, that fits to the new version of S32 DS?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Younes&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 04 Jul 2022 21:00:02 GMT</pubDate>
    <dc:creator>Younes</dc:creator>
    <dc:date>2022-07-04T21:00:02Z</dc:date>
    <item>
      <title>Trouble with PT2001</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/Trouble-with-PT2001/m-p/1483390#M313</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;dear community,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have taken the sample code in PT2001 Developer Studio and then uploaded it to PT2001EVB via SPI GEN software. It seems that all files are successfully uploaded. But when I connect 12 V Powersupply and give HIGH signal to STARTx pin via "Batch Command", I cannot set any current at injector output at all.&lt;/P&gt;&lt;P&gt;I read through the old posts and found a similar problem with PT2000. But there the suggested solution was to replace the IC on the board as it is an older version. But I bought the PT2001 board recently, so I almost assume that the IC is also the new version. Besides, yes I can't replace such an IC personally, that needs the appropriate machines.&lt;/P&gt;&lt;P&gt;Please help me, because I have to give this project in a short time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Jul 2022 10:07:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/Trouble-with-PT2001/m-p/1483390#M313</guid>
      <dc:creator>Younes</dc:creator>
      <dc:date>2022-07-01T10:07:46Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble with PT2001</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/Trouble-with-PT2001/m-p/1483869#M314</link>
      <description>&lt;P&gt;Dear Younes,&lt;/P&gt;
&lt;P&gt;which MCU board are you using with the PT2001 EVB? I presume you are using the FRDM-KL25Z board? In the kit should be included also the&amp;nbsp;S32K144EVB-Q100, which can be used with S32 Design Studio IDE. Please refer to the section 7 in&amp;nbsp;KTFRDMPT2001EVMUG attached. Please consider to use the PT2001 with the S32K1 MCU. There is an sample project for the S32K144 and PT2001.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/development-boards/analog-toolbox/pt2001-evaluation-board:FRDMPT2001EVM" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/development-boards/analog-toolbox/pt2001-evaluation-board:FRDMPT2001EVM&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1656917087525.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/185435iBBFDF56E005702CC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1656917087525.png" alt="JozefKozon_0-1656917087525.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The latest S32DS version can be downloaded from this link:&amp;nbsp;&lt;A href="https://www.nxp.com/design/software/development-software/s32-design-studio-ide:S32-DESIGN-STUDIO-IDE" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/software/development-software/s32-design-studio-ide:S32-DESIGN-STUDIO-IDE&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JozefKozon_0-1656917605009.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/185437i7489A27E899F7ABF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JozefKozon_0-1656917605009.png" alt="JozefKozon_0-1656917605009.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please take a picture of the top of the PT2001 chip so we can check the date of production of the PT2001. The third line should define the year and week of production.&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jul 2022 06:54:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/Trouble-with-PT2001/m-p/1483869#M314</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2022-07-04T06:54:21Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble with PT2001</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/Trouble-with-PT2001/m-p/1484206#M315</link>
      <description>&lt;P&gt;I have now tried to build the example project in the S32-DS environment. For this I tried it with S32-DS Platform 3.4 and S32-DS ARM V 2.2 with many compiler errors. Therefore I tried it with S32DS.ARM.2018 R.1 environment and I still get these following 2 errors and can't fix them.&lt;/P&gt;&lt;P&gt;Furthermore as requested I am sending a picture of the PT2001 chip so that the manufacturing date can be seen.&lt;/P&gt;&lt;P&gt;Is there any other current example project, that fits to the new version of S32 DS?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Younes&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Jul 2022 21:00:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/Trouble-with-PT2001/m-p/1484206#M315</guid>
      <dc:creator>Younes</dc:creator>
      <dc:date>2022-07-04T21:00:02Z</dc:date>
    </item>
    <item>
      <title>Re: Trouble with PT2001</title>
      <link>https://community.nxp.com/t5/Powertrain-and-Electrification/Trouble-with-PT2001/m-p/1485988#M316</link>
      <description>&lt;P&gt;Hi Younes,&lt;/P&gt;
&lt;P&gt;I have sent you a reply in the new case you have created.&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jul 2022 06:56:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Powertrain-and-Electrification/Trouble-with-PT2001/m-p/1485988#M316</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2022-07-07T06:56:13Z</dc:date>
    </item>
  </channel>
</rss>